Skip to main content

Professional technician cleaning air conditioner Summer does not care about HVAC problems. It shows up on a Tuesday in June and expects the house to be cold. When the AC is running but the house is not cooling, the clock is already ticking.

The good news: many “AC not cooling” service calls trace back to something a sharp technician, contractor, or attentive homeowner can find and fix in under an hour. Work through the list below before placing a call.

How a Central AC System Actually Cools

Understanding the basic cycle makes diagnosis faster. The refrigerant circuit works like this:

  • The indoor air handler pulls warm room air across the evaporator coil, where refrigerant absorbs heat and the air drops in temperature.
  • The blower pushes that cooled air back into the living space.
  • The now-warm refrigerant travels outside to the condenser coil, where it releases heat to the outdoor air.
  • The refrigerant cools, returns inside, and the cycle repeats.

Every common cooling failure interrupts one of those four steps.

9 Common Reasons an AC Is Not Cooling

1

Thermostat Set to Fan Instead of Cool

The fan runs continuously on the “on” or “fan” setting without running a cooling cycle, moving unconditioned air through every register. Set the thermostat to “cool,” confirm the setpoint is at least 3 to 5 degrees below room temperature, and switch fan mode to “auto.” Give the system five minutes before drawing conclusions.

2

Clogged Air Filter

A filter loaded with dust starves the evaporator coil of airflow. Less airflow means less heat transfer to the refrigerant, which means the coil drops below freezing and ices over. Pull the filter. Hold it up to a light. If almost no light passes through, replace it before doing anything else.

During peak summer months, most residential systems need a fresh filter every 30 to 60 days. Browse air filters by size and MERV rating at SupplyHouse to keep a couple on the shelf.

Related reading: How to Select the Best Air Furnace Filter covers MERV ratings and system compatibility in detail.

3

Dirty or Blocked Condenser Coils

The outdoor condenser dumps heat collected indoors back into the outdoor air. When the coils are packed with cottonwood, grass clippings, dirt, or debris, heat cannot escape efficiently. Check the outdoor unit. Clear at least 18 to 24 inches of clearance on all sides. Rinse the coil with a garden hose set to a moderate stream, spraying from inside the coil outward. Never use a pressure washer.

4

Frozen Evaporator Coil

A frozen coil blocks airflow entirely and the system blows warm air even while running. Signs include:

  • Noticeably weaker airflow from all registers
  • Ice visible on the copper refrigerant lines near the air handler
  • Water dripping or pooling beneath the indoor unit as ice melts

To thaw: shut the AC off, run the fan on “fan only” mode for two to four hours, then replace the filter and restart. If the coil refreezes within 24 hours, the underlying cause is almost certainly low refrigerant.

5

Low Refrigerant (Refrigerant Leak)

Refrigerant circulates in a closed loop. Low refrigerant means a leak. Signs include:

  • Hissing or bubbling sounds near the outdoor unit or refrigerant lines
  • Ice buildup on the refrigerant lines or coil
  • The system running constantly without reaching the setpoint

Refrigerant handling is EPA Section 608 regulated and requires certification. Do not let anyone top off a low system without locating and repairing the leak first.

6

Tripped Breaker or Blown Fuse

If the outdoor unit is not running but the air handler inside is, check the electrical panel. Reset the dedicated breaker once. If it trips again immediately, stop. Repeated tripping means an underlying electrical or compressor problem that needs a licensed technician.

7

Clogged Condensate Drain Line

AC systems pull significant moisture from the air. That condensate drains through a PVC line. When algae or mold blocks the line, the drain pan can fill, and many systems use a safety float switch that shuts the system down.

The fix: flush the drain line with a cup of white vinegar, then follow with water. For more involved drain issues, check the full guide to replacing a condensate pump or browse condensate removal pumps at SupplyHouse.

8

Undersized or Oversized System

A system that is too small runs constantly and still cannot keep up on the hottest days. A system that is too large short-cycles, shutting off before removing enough humidity. The house ends up cold and clammy or still too warm. Proper sizing requires a Manual J load calculation.

9

Failing Compressor

If the compressor fails, the system runs without actually moving refrigerant. Compressor replacement on a residential system typically costs $1,200 to $2,500 in parts alone. On systems older than 10 to 12 years, replacing the full system often pencils out better.

Quick Diagnostic Table: DIY vs. Call a Pro

Symptom Likely Cause DIY Fix Call a Pro
Fan running, no cold air Thermostat on fan mode Reset to cool If still not cooling
Weak airflow, iced lines Clogged filter / frozen coil Replace filter, thaw coil If coil refreezes
Outdoor unit not running Tripped breaker Reset once If it trips again
Hissing near outdoor unit Refrigerant leak No Yes, EPA-regulated
Water dripping from air handler Clogged condensate drain Flush with vinegar If clog persists
Runs constantly, no setpoint Undersized or dirty coil Clean coil, check filter If persists
Warm air, compressor running Failing compressor No Yes

Preventive Maintenance That Prevents Most of This

  • Replace air filters every 30 to 60 days during the cooling season
  • Clean the condenser coil each spring before first use
  • Flush the condensate drain line at the start of each season
  • Confirm all supply and return vents are open and unobstructed
  • Schedule a professional tune-up annually

For a complete spring startup walkthrough, check out How to Prepare an Air Conditioner for Spring Startup on the blog.

Frequently Asked Questions

Why is an AC running but not cooling the house?

The most common reasons are a clogged air filter, a frozen evaporator coil, dirty condenser coils, or low refrigerant from a leak. Start with the filter.

Can a dirty filter cause an AC to stop cooling entirely?

Yes. A severely clogged filter restricts airflow enough to freeze the evaporator coil, which blocks air movement completely. The system keeps running but blows warm air.

How can someone tell if the AC has a refrigerant leak?

Signs include ice on the copper lines near the outdoor unit, a hissing or bubbling sound, and a system that runs constantly without reaching the thermostat setpoint. Only a licensed HVAC technician can legally handle refrigerant.

Is it OK to run an AC with a frozen coil?

No. Running the system with a frozen coil strains the compressor and can damage it permanently. Shut the AC off, run the fan only to thaw the coil, then fix the underlying cause before restarting.

How often should an AC be serviced to prevent cooling failures?

Once per year, ideally in spring before the first hot stretch. A professional tune-up catches refrigerant level issues, dirty coils, and electrical problems before they become breakdowns.

What does short cycling mean for an AC?

Short cycling means the system turns on and off too frequently. Common causes include oversizing, airflow problems, refrigerant issues, electrical faults, or control problems.

Why does an AC run all day but never cool below 78F?

On extremely hot days, some systems struggle to overcome peak heat loads. If it is persistent, the system is either undersized, has dirty coils limiting capacity, has low refrigerant, or there are significant duct leaks.

Can closing vents in unused rooms help the AC cool better?

No. Closing vents increases static pressure in the duct system, reduces overall airflow efficiency, and can cause the evaporator coil to freeze. Keep all vents open.

What is the most common reason an AC fails right before summer?

A clogged air filter that has been sitting untouched since the previous season. Swapping it out during the spring startup prevents the most common cascade of cooling failures.

When does an AC need to be replaced vs. repaired?

When the system is more than 10 to 15 years old and a repair costs more than 30 to 50% of a replacement system’s price, replacement usually wins. Aging R-22 systems tip the math further toward replacement due to refrigerant scarcity.

Most AC cooling failures come down to five fixable things: a dirty filter, a frozen coil, a fouled condenser, a tripped breaker, or a clogged drain. Run through the list in order before calling anyone. The more expensive causes, refrigerant leaks and compressor failure, show up at the end of the diagnostic sequence for a reason. Fix the cheap things first. Browse air filters, condensate pumps, and HVAC equipment at SupplyHouse to stay ahead of summer breakdowns before they happen.