Skip to main content
Low water pressure faucet

The International Plumbing Code requires a minimum of 20 psi at any fixture outlet, but understanding how to fix low water pressure starts with knowing that most showers, dishwashers, and irrigation systems need 40 to 60 psi to function properly. A pressure drop that builds gradually over months usually points to a different root cause than one that appears overnight. The morning shower barely rinses shampoo, the kitchen faucet takes a full minute to fill a pot, and the garden hose puts out a lazy arc instead of a proper stream. Each scenario has a specific fix, and diagnosing it correctly saves both time and pipe. 

How Residential Water Pressure Works 

Municipal water pressure varies by utility, pressure zone, elevation, and demand. The service line from the street carries that pressure to the water meter, which sits at the property boundary or in the basement. From the meter, a main supply line (usually 3/4-inch or 1-inch copper, PEX, or galvanized steel) feeds the home. 

Homes with static water pressure above 80 psi require a pressure-reducing valve under the IPC. The PRV’s job is to step incoming pressure down to a safe operating range, typically preset at 50 psi from the factory. Without a PRV, high municipal pressure can stress pipes, blow out washing machine hoses, and damage water heater components. 

Inside the home, the main line branches into hot and cold distribution lines. Water pressure drops at every fitting, tee, elbow, and valve in the system. The further a fixture sits from the main, and the more fittings between them, the lower the delivered pressure. Elevation plays a role too: water loses approximately 0.43 psi for every foot of vertical rise. A second-floor bathroom sits roughly 10 feet above the basement entry point, which means about 4.3 psi of loss just from height. 

Pipe diameter matters enormously. A 3/4-inch main supply line flowing at 10 GPM loses far less pressure per foot of run than a 1/2-inch line at the same flow. When multiple fixtures run simultaneously (the shower, the dishwasher, and the washing machine), flow demand spikes and pressure at each fixture drops. In undersized systems, this simultaneous demand a common source of perceived low pressure. 

Well-fed homes work differently. A well pump pushes water into a pressure tank, which maintains system pressure between two set points (typically 40 psi on and 60 psi off). When the tank pressure drops to the lower set point, the pump kicks on and refills it. A waterlogged tank, a weak pump, or a failing pressure switch can all produce low-pressure symptoms. 

Low Water Pressure: Causes at a Glance 

Low water pressure is a symptom with multiple possible causes. The table below maps common symptoms to their likely source, scope, and the recommended first step. 

Symptom Likely Cause Scope Recommended Fix Key Product 
Low at one faucet only Clogged aerator or supply valve partially closed Single fixture Clean or replace aerator; open valve fully — 
Low at all fixtures Failing or misadjusted PRV Whole house Test pressure, adjust or replace PRV Watts LF25AUB-Z3 
Gradual decline over years Galvanized pipe interior corrosion Whole house Repipe affected sections with copper or PEX — 
Sudden drop, all fixtures Partially closed main shutoff or meter valve Whole house Open gate or ball valve to full-open position — 
Low on hot water only Sediment buildup in water heater Hot side only Flush the water heater tank — 
Low, but unable to identify source Unknown baseline; could be any of the above Whole house Test static pressure with a gauge first Zurn HGI-25 

Tools and Materials 

  • Hose-bib pressure gauge (Zurn HGI-25 or equivalent) 
  • Adjustable wrench (10-inch) 
  • Channel-lock pliers (12-inch) 
  • Pipe wrenches, 10-inch and 14-inch (for PRV replacement) 
  • White vinegar and a small bowl (for aerator soaking) 
  • Bucket 
  • Flashlight 
  • PTFE thread seal tape, 1/2-inch width 
  • Garden hose (for water heater flush, if needed) 
  • Flat-head screwdriver (for PRV adjustment bolt) 

A Zurn HGI-25 pressure gauge threads directly onto any standard hose bib and reads up to 200 psi. The built-in maximum-pressure indicator holds the peak reading, which is critical for diagnosing intermittent surges. 

Step-by-Step: How to Fix Low Water Pressure 

Step 1: Identify the Scope of the Problem 

Run every faucet, shower, and hose bib in the building one at a time. Note which fixtures have low pressure and whether it affects hot, cold, or both. If only one fixture is weak, the problem is local (aerator, angle stop, or flex supply line). If every fixture is weak, the cause is system-wide. 

Step 2: Test Static Pressure at a Hose Bib 

Shut off every water-using fixture and appliance inside the building. Thread a Zurn HGI-25 gauge onto an outdoor hose bib (or the laundry-room bib, if no outdoor bib is accessible). Open the bib fully and read the gauge. Normal residential static pressure is 40 to 80 psi. Below 40 psi confirms a system-level problem. Above 80 psi indicates the PRV may be set too high or has failed open. 

Step 3: Check the Main Shutoff Valve 

Locate the main shutoff valve, typically in the basement, crawl space, or utility closet near where the service line enters the building. If it’s a gate valve (round handle), turn it fully counterclockwise. If it’s a ball valve (lever handle), confirm the lever is parallel to the pipe. A gate valve that’s even one turn short of fully open can cut delivered pressure by 25 percent or more. 

Step 4: Check the Meter Valve 

The meter valve sits on the street side of the water meter and is technically the utility’s property. However, it’s worth verifying that it’s fully open. After a meter replacement or street-side repair, utility crews occasionally leave this valve partially closed. If it has a lever handle, it should be parallel to the pipe. Contact the water authority if it needs adjustment. 

Step 5: Inspect and Clean Aerators 

Unscrew the aerator from the tip of every affected faucet. Aerators have a tiny mesh screen that traps sediment, mineral flakes, and pipe debris. A clogged aerator can reduce a faucet’s flow to a trickle while static pressure tests perfectly normal. Soak the aerator in white vinegar for 30 minutes, scrub with an old toothbrush, rinse, and reinstall. 

Step 6: Check Showerheads for Mineral Buildup 

Remove each affected showerhead and inspect the inlet screen and nozzle openings. Hard-water deposits clog nozzle holes over time, especially in areas where water hardness exceeds 120 ppm. Soak in vinegar overnight if needed, or replace the head if the nozzles are permanently blocked. 

Step 7: Test Hot vs. Cold Separately 

At each fixture, run hot only and then cold only. If cold pressure is normal but hot is weak, the problem is between the water heater and the fixture: a partially closed heater shutoff valve, sediment buildup inside the tank, or a corroded hot-water distribution line. 

Step 8: Inspect Supply Valves Under Sinks and Behind Toilets 

Angle stops (the small shutoff valves under sinks and behind toilets) can fail partially closed due to mineral deposits on the gate or ball. Turn each valve fully open. If an angle stop is seized or visibly corroded, it needs replacement. 

Step 9: Locate and Inspect the Pressure Reducing Valve 

The PRV is typically a bell-shaped brass body installed on the main supply line just downstream of the meter. Look for it in the basement or utility closet. A standard PRV has an adjustment bolt on top (sometimes covered by a cap) and a locknut. If the PRV body shows green corrosion, weeping at the seams, or visible mineral crusting, it’s nearing the end of its service life. 

Step 10: Adjust the PRV 

Loosen the locknut on the adjustment bolt with a wrench. Turn the bolt clockwise (looking down at the top of the valve) to increase pressure. Make small adjustments, about one full turn at a time, then re-check the gauge at the hose bib. The target is 50 to 60 psi for most residential systems. Do not exceed 80 psi, the IPC maximum for static pressure. 

Step 11: Test Pressure After PRV Adjustment 

With the gauge still on the hose bib, open the bib and read the new pressure. Run a few fixtures simultaneously to check dynamic pressure under load. If the gauge reads correctly at the bib but pressure is still low at distant fixtures, the issue is in the distribution piping, not the PRV. 

Step 12: Flush the Water Heater (Hot-Side Issues) 

If low pressure affects only the hot side, sediment in the water heater tank is a likely culprit. Sediment accumulates at the bottom of the tank and can partially block the outlet.  

Step 13: Check for Galvanized Pipe Sections 

Galvanized steel pipe corrodes from the inside out. A 50-year-old 3/4-inch galvanized pipe might have an effective interior diameter of only 3/8 inch due to mineral and rust buildup on the pipe walls. Use a magnet to test exposed pipe: galvanized steel is magnetic, copper is not. If the main supply line or major branch lines are galvanized, partial or full repiping with copper or PEX is the permanent fix. 

Step 14: Rule Out Municipal Supply Issues 

If all testing points to adequate equipment but pressure is still low, the problem may be on the street side. Contact the local water authority and ask for a pressure test at the meter. Construction, main breaks, and seasonal demand peaks (summer irrigation) can all reduce supply pressure temporarily. 

Step 15: Retest All Fixtures After Repairs 

After completing any repair, whether it’s a PRV adjustment, an aerator cleaning, or a valve opening, retest every fixture in the building. Run the static gauge test again at the hose bib with all fixtures off, then run multiple fixtures simultaneously and re-check. The goal is 40 to 60 psi static, with adequate pressure at the fixtures under normal simultaneous demand. 

Diagnosing Pressure Loss by Fixture vs. Whole House 

The single most important diagnostic question is whether low pressure shows up at one fixture or all of them. That answer splits the troubleshooting path in two completely different directions. 

Single-fixture problems are almost always local. The aerator is clogged, the angle stop under the sink is partially closed, the flex supply line is kinked, or the cartridge inside the faucet or shower valve is fouled. These are quick fixes. Clean the aerator, open the valve, replace the supply line, or swap the cartridge. 

Whole-house problems point upstream: a failing PRV, a partially closed main valve, corroded galvanized pipes, or a municipal supply issue. These take more investigation but always start with a static pressure reading at the hose bib. That single number tells the story: if static pressure is normal (40+ psi) but dynamic pressure drops sharply when fixtures run, the pipes can’t carry enough volume. If static pressure itself is low, the restriction is at or before the PRV. 

A third scenario: pressure is fine everywhere except one bathroom or one floor. That usually means a partially closed branch valve, a corroded section of pipe feeding that zone, or a long run of undersized 1/2-inch pipe that creates excessive friction loss. 

Galvanized Pipe Corrosion: The Hidden Pressure Killer 

Galvanized steel pipe was the standard for residential water distribution from the 1930s through the 1960s. The zinc coating that gives galvanized pipe its corrosion resistance breaks down over decades, and the steel underneath rusts from the inside out. The rust creates a rough, narrowing interior surface that progressively chokes flow. 

A new 3/4-inch galvanized pipe has an interior diameter of about 0.824 inches. After 40 to 60 years, that interior can narrow to 0.4 inches or less, cutting the cross-sectional flow area by more than 75 percent. The pressure loss through that corroded section is dramatic, and it gets worse every year. 

Galvanized corrosion is also uneven. Horizontal runs corrode faster at the bottom of the pipe. Elbows and tees corrode faster than straight runs because turbulence accelerates material loss. The result is unpredictable, with some sections still flowing reasonably well while others are nearly sealed shut. 

There’s no way to clean out the interior of an in-wall galvanized pipe. Partial repiping (replacing the most corroded sections with copper or PEX) provides immediate improvement. Full repiping is the permanent solution and adds meaningful value to older properties. 

Adjusting and Replacing a Pressure Reducing Valve 

Pressure reducing valves have a typical service life of 7 to 12 years, depending on water quality and incoming pressure. A failing PRV might stick in a partially closed position (low pressure), fail open (dangerously high pressure), or fluctuate erratically. 

Adjustment is the first step. Loosen the locknut, turn the bolt clockwise to raise pressure or counterclockwise to lower it, re-check with the gauge, and re-tighten the locknut when the target is reached. If adjustment doesn’t hold, or if the valve body shows corrosion and weeping, replacement is the right call. The Watts LF25AUB-Z3 is a 3/4-inch lead-free PRV with a threaded female-union inlet and NPT female outlet, which simplifies installation on standard residential supply lines. 

For a complete guide to PRV installation, including pipe prep, orientation, and initial adjustment, see How to Install and Set a Pressure Reducing Valve. 

When replacing a PRV, always install a pressure gauge downstream for real-time verification. Set the new valve to 50 psi, run fixtures, and fine-tune from there. Lock the nut when satisfied. 

Well Pump Systems and Pressure Tanks 

Homes on private wells don’t have municipal supply pressure. Instead, a submersible or jet pump draws water from the well and pushes it into a pressure tank. The tank contains an air bladder that maintains system pressure between two set points, commonly 30/50 or 40/60 psi (cut-in/cut-out). 

When the pressure tank’s air bladder loses its charge, the tank becomes waterlogged. Without the air cushion, the pump cycles rapidly (short-cycling), and pressure swings wildly between high and low with every fixture use. Check the tank’s air charge with a tire pressure gauge on the Schrader valve at the top of the tank. The pre-charge should be 2 psi below the pump’s cut-in pressure (e.g., 38 psi for a 40/60 system). 

A weak well pump delivers low pressure even when the tank is properly charged. Pump capacity degrades over time as impellers wear and motor windings deteriorate. If the pump runs continuously but can’t maintain the cut-out pressure, it needs service or replacement. 

The pressure switch, mounted on the supply pipe near the tank, can also fail. Corroded contact points prevent the switch from closing the pump circuit at the correct pressure. Replacing a pressure switch is a fraction of the cost of a new pump and solves the problem when the pump itself is still strong. 

Stocking Recommendations for Plumbers 

  • Zurn HGI-25 Hose Bibb Pressure Gauge with Maximum Pressure Indicator (SKU: HGI-25). Reads up to 200 psi with a lazy-hand maximum indicator. Threads onto any standard 3/4-inch hose bib for quick static and dynamic pressure testing. Essential diagnostic tool for every service call involving pressure complaints. 
  • Watts LF25AUB-Z3 3/4″ Pressure Reducing Valve (SKU: 0009257). Lead-free brass PRV with threaded female-union inlet and NPT female outlet. Factory preset at 50 psi, adjustable from 25 to 75 psi. Standard replacement for most residential 3/4-inch main lines. 

Frequently Asked Questions 

Q: What is normal residential water pressure? 

Normal residential static water pressure falls between 40 and 80 psi. The International Plumbing Code sets 20 psi as the absolute minimum at any fixture outlet and 80 psi as the maximum static pressure. Most fixtures and appliances perform well in the 50 to 60 psi range. 

Q: How is residential water pressure tested? 

Thread a pressure gauge onto an outdoor hose bib with all fixtures off. Open the bib fully and read the gauge. A Zurn HGI-25 gauge reads up to 200 psi and has a maximum-pressure indicator that holds the peak reading, which helps identify pressure surges. 

Q: What causes a sudden drop in water pressure? 

A sudden, whole-house pressure drop usually traces to a partially closed valve (the main shutoff or the meter valve), a PRV failure, or a municipal main break. Check every valve in the system for full open position first. If all valves are open, contact the water authority to ask about service interruptions. 

Q: Can a water heater cause low pressure? 

Yes, but only on the hot side. Sediment accumulates at the bottom of tank-style water heaters over time, and in severe cases it partially blocks the outlet or dip tube. If cold pressure is normal and hot is weak, the heater is the prime suspect.  

Q: What is a pressure reducing valve (PRV)? 

A PRV is a brass valve installed on the main supply line that steps high municipal pressure down to a safe residential level, typically 50 psi. It has an internal spring and diaphragm that regulate the outlet pressure regardless of fluctuations on the inlet side. The Watts LF25AUB-Z3 is a standard 3/4-inch replacement unit for most residential applications. 

Q: How long does a PRV last? 

Most PRVs last 7 to 12 years depending on water quality, incoming pressure, and usage patterns. Hard water and high-pressure environments shorten lifespan. Signs of a failing PRV include erratic pressure swings, low delivered pressure despite normal street-side supply, or visible corrosion and weeping at the valve body. For a full installation walkthrough, see How to Install and Set a Pressure Reducing Valve. 

Q: Do galvanized pipes reduce water pressure? 

Over time, absolutely. Galvanized steel corrodes from the inside out, narrowing the pipe’s interior diameter by as much as 75 percent after 40 to 60 years. A 3/4-inch galvanized pipe that started with a 0.824-inch interior bore can narrow to 0.4 inches or less. The only permanent fix is repiping the corroded sections with copper or PEX. 

Q: Will installing larger pipe increase pressure? 

Larger pipe reduces friction loss, which can improve delivered pressure at fixtures, but it doesn’t increase the source pressure coming into the building. If static pressure at the meter is already low, larger pipe won’t fix it. Larger pipe helps most when pressure drops significantly under flow (high dynamic loss), which indicates the existing pipes are too small for the demand. 

Q: Can a well pump cause low water pressure? 

Yes. A worn well pump with degraded impellers can’t maintain the cut-out pressure setting on the pressure switch. Symptoms include the pump running constantly without reaching full pressure, short-cycling (rapid on-off), and gradually declining pressure over weeks or months. Short-cycling and low pressure commonly indicate a waterlogged or improperly charged pressure tank. Check the tank’s precharge and condition before condemning the pump; a failed bladder tank may require replacement.. 

Q: When should a plumber be called for low pressure? 

Call a plumber if the problem affects the entire house and basic checks (valves, aerators, PRV adjustment) don’t resolve it. Galvanized pipe repiping, well pump replacement, and in-wall valve repairs are not DIY-friendly jobs. Also call if the static pressure gauge reads above 80 psi (the PRV has failed open and over-pressure can damage fixtures) or if a Zurn HGI-25 gauge shows extreme fluctuation, which may indicate a failing pump or waterlogged pressure tank. 

Restoring the Flow 

Low water pressure is a symptom, not a diagnosis. Start with a baseline reading from a Zurn HGI-25 gauge at the hose bib, then work through the system from the street to the fixture. A Watts LF25AUB-Z3 pressure reducing valve handles the full replacement when the original PRV has reached the end of its service life. For detailed PRV installation guidance, see How to Install and Set a Pressure Reducing Valve.  The full pressure reducing valve lineup, including 1/2-inch, 3/4-inch, and 1-inch models, is at supplyhouse.com/Pressure-Reducing-Valves-17082000. Pressure problems always have a traceable cause, and the fix is almost always simpler than it looks once the diagnostic work is done.