The AC is running. Most of the house is fine at 72 degrees F. But the upstairs master bedroom sits at 81 degrees F. Or a south-facing office never cools down no matter what the thermostat says. The system is not broken. Airflow is the problem. Airflow problems have specific, diagnosable causes, and most of them have fixes that do not require an equipment replacement.
Understanding Duct System Pressure First
A forced-air HVAC system is a pressure-balanced loop. The blower creates positive pressure in the supply ducts and negative pressure in the return ducts. The whole thing is designed around a specific static pressure. Mess with the pressure by closing vents, adding restrictions, or running undersized returns, and comfort suffers in predictable ways.
Cause 1: Insufficient Return Air
Every room that gets conditioned air also needs to return that air back to the air handler. A room with a supply register but no return path (and a closed door with no undercut) builds up pressure as air comes in. The supply vent works against itself.
Fixes:
- Undercut interior doors 3/4 to 1 inch above the carpet or floor
- Add a transfer grille between the room and the adjacent hallway
- Add a dedicated return grille to the room if ductwork allows
This is free or nearly free and resolves a surprisingly large number of comfort complaints.
Cause 2: Closed or Partially Closed Vents
Closing vents in unused rooms to “redirect” airflow is one of the most persistent HVAC myths. Closing a vent increases static pressure in the duct system, which reduces airflow through every remaining open vent and stresses the blower motor. No room gets more air. The whole system gets less.
Keep all vents open throughout the house. Look at the full registers and grilles collection at SupplyHouse if any vent hardware needs upgrading.
Cause 3: Duct Leakage
The Department of Energy estimates the average home loses 20 to 30% of conditioned air through duct leaks, air that ends up in attics, crawl spaces, and wall cavities instead of living spaces.
Signs of duct leakage:
- Rooms that are consistently harder to condition regardless of filter condition
- Excessively dusty home (ducts pulling from unconditioned spaces)
- Higher-than-expected utility bills relative to usage
- Cool air blowing from some registers but not others on the same zone
Fixes: in accessible areas, inspect duct joints for gaps and seal with mastic duct sealant or foil-backed HVAC tape. For ducts in finished walls or attics, a professional duct blaster test quantifies the leakage.
Cause 4: Attic Heat Gain and Upstairs Rooms
Heat rises. Roof assemblies absorb massive amounts of solar energy and radiate it downward into attic spaces. An attic running at 140 degrees F above a poorly insulated ceiling pushes heat into upstairs rooms faster than the system can remove it.
| Fix | Cost | Impact |
| Air seal attic floor penetrations | Low | High |
| Add attic insulation to R-38 to R-60 | Moderate | High |
| Radiant barrier on roof deck | Moderate | Moderate |
| Add mini split to upper floor | Higher | Highest |
For persistent upstairs cooling problems, a dedicated single-zone mini split is frequently the most cost-effective long-term fix.
Cause 5: Blocked or Mispositioned Supply Registers
A supply register covered by a couch, rug, or curtain might as well not exist. Walk every room and confirm:
- All floor registers are uncovered and open
- All sidewall and ceiling registers are not blocked by furniture or drapes
- Registers are aimed appropriately
- The damper on each register is fully open
Cause 6: Blower Motor Speed Settings
Variable-speed and multi-speed air handlers have selectable speed settings. An installer may have set the blower to a lower speed to reduce noise, at the cost of airflow and distribution. An HVAC technician can check and adjust the blower speed setting.
Diagnosis Checklist: Room by Room
- All supply and return vents fully open
- Furniture and rugs clear of all floor registers
- Interior doors undercut or have transfer path for return air
- Duct joints in accessible areas checked and sealed
- Attic insulation level confirmed (R-38 minimum in most zones)
- Blower speed setting appropriate for the system
- Thermostat zone assignment correct for affected room
- Outdoor unit clean and unobstructed
- Air filter clean and replaced within 30 to 60 days
Frequently Asked Questions
Why is one room always hotter than the rest of the house?
The most common causes are insufficient supply airflow to that room, a blocked or undersized supply register, duct leakage before the air reaches that register, or inadequate return airflow. Poor attic insulation above the room is another frequent culprit.
Does closing vents in unused rooms save energy?
No. Closing vents increases duct system static pressure, reduces overall airflow efficiency, and stresses the blower motor. Keep all vents open and balance the system with duct dampers inside the ductwork.
What is the cheapest fix for uneven cooling?
Undercutting interior doors, clearing furniture from floor registers, and opening all vents are free or nearly free and address the most common causes.
How does duct leakage affect comfort?
Leaky ducts dump conditioned air into attics, crawl spaces, and wall cavities. The DOE estimates the average home loses 20 to 30% of conditioned air this way. The system works harder, runs longer, and still cannot evenly condition rooms far from the air handler.
Would a mini split fix persistent hot rooms better than duct modifications?
In many cases, yes. Adding a ductless mini split to a chronically hot room handles the load directly without asking the existing duct system to compensate. It is often cheaper than a full duct remediation and solves the problem permanently.
Is upstairs always going to be hotter than downstairs in summer?
With stock construction and no modifications, yes. With proper attic insulation, air sealing, and either a dedicated upper-floor mini split or a correctly zoned system, the temperature difference drops to 2 to 4 degrees, which is manageable.
Choose Wisely, Breathe Easily
Hot rooms in summer are almost never caused by a failing AC. They are caused by airflow problems: closed vents, blocked registers, duct leakage, poor attic insulation, or inadequate return air paths. Start with the free fixes (undercut doors, open vents, clear registers) before spending anything. For persistent upper-floor heat problems, a dedicated mini split handles the load directly and permanently. SupplyHouse carries floor registers, sidewall registers, and the full range of mini split systems to solve whatever combination of issues a specific home presents.