SupplyHouse Blog Banner 2




Air Clean Enough to Eat off of: Filters and More!

Nick B

  As the name suggests, an air cleaner, or air purifier, removes the impurities out of the air.  Their's a unit for all kinds of situations, from a single room, to a whole house, and even to an entire industrial workspace.  They are typically used in situations where the air can become un…

read more...

Better Baseboard Covers: Truth in the Name?

Greg

Existing hot water baseboard covers over time can fall victim to rust, scratches, and damage.  Exposed sharp metal edges can be a hazard to young children.  Replacing these covers can go a long way towards improving the appearance and performance of your existing baseboard radiators. Better Baseb…

read more...

If You’re Looking For The #1 Tankless Water Heater, We’ve Found It.

Adam

Rinnai is the number 1 selling tankless water heating brand in the U.S. Their main focus is innovating water heating and home heating gas appliances for residential and commercial applications - and they're good at what they do! The tankless water heaters can use up to 40 percent less energy than…

read more...

Cozy Up Key Spaces with Towel Radiators

Steffy

  You’re stepping out of the shower when—bam!—you’re hit with a shock of cold air that makes you want to scamper back to bed and jump under the covers. If that scenario sounds too, too familiar, then it may be time to install a towel radiator. You may know a similar entity—the to…

read more...

Warm Up Your Workspace with a Unit Heater

Steffy

Tired of wearing a winter jacket while working? Rather than put progress on hold as the temperature drops, why not make the area more comfortable? One cost-effective method would be to install a unit heater. Designed expressly for the purpose of introducing warmth to work spaces, unit heaters co…

read more...

4 Reasons Why Modine’s Hot Dawg Heater is Mans Best Friend…

Eli

1. SO MANY BTU'S!!!! //   The Hot Dawg units range in sizes from 30,000 BTU to 125,000 BTU’s. Need more? The PDP heaters range from 150,000 to 400,000 BTU’s!   2. They are certified for residential, commercial, and industrial use!   //   3.…

read more...

How To Win At Winter With Runtal Towel Warmer Radiators

Adam

If you don't look forward to warm showers because you dread the aftermath, you're doing winter all wrong. Yes, "towel warmers" exist, and we promise they are life changing. Runtal Towel Warmer Radiators leave your towels warm and toasty, so you never have to feel chilly at the end of your shower…

read more...

Learn the Little-Known Benefits of Pipe Insulation

Steffy

Pipe insulation wears many hats. Yes,  it keeps the water in your plumbing system from turning to ice and expanding, but pipe insulation also performs several far less dramatic roles in the home. These not only help to save money on utility bills, but also make everyday life a little easier. &nb…

read more...

Azel Technologies: The Secret To Guilt-Free, Energy Effecient, Radiant Heating.

Adam

Imagine a winter where you can leave your heat on, guilt free. Energy savings no longer has to be top of mind, because your heating products have your back. Your thermostat, zone valve controls and switching relays WANT to promote energy efficiency because they care... about both you, and the envir…

read more...

Everything You Need To Know About McDonnell & Miller Products

Steffy

Who is McDonnell & Miller? An industry leader in the engineering and manufacturing of flow switches, low water cut-offs and water feeders for over 80 years, McDonnel & Miller specializes in keeping all kinds of boilers running safely. The boiler is the most important part of a central…

read more...

Put An End To Snow Shoveling Once And For All…

Steffy

  Though winter’s worst storms are likely yet to come, many homeowners around the country have already had ample opportunity to grow tired of shoveling snow. After all, it’s a tedious, time-consuming, back-breaking chore, one that’s regrettably unavoidable in cold climates. But wai…

read more...

Signs Your Broan Big Heat 6201 Heating Unit Is A Stage 5 Clinger…

Adam

Does your heater follow you room-to-room?   Do you catch it glancing up at you, sneakily,  looking for attention?   ... I think you've got yourself a stage 5 clinger.  If not, your heater is JUST. THAT. GOOD.   The Big Heat 6201 is an efficient two-level heater…

read more...


SupplyHouse.com Logo