SupplyHouse Blog Banner 2





Solar Powered Device Cleans Water and Produces Energy

Gregory

solar power, solar energy, sun, green energy, alternative energy, climate change, solar panel, water, water distiller, water distillation, water power, hydro power, water, energy, global warming, efficiency, material, research, experiment, engineer, scientist, environment, environmentalWhen in doubt, try something new! That’s what a group of engineers did when it came to combining solar energy with clean water.

 

A team of engineers installed a water distillation system on the back of a solar power cell, thus creating a device that doubles as both an energy generator and a water purifier. “It’s really good engineering at work,” George Ni, an engineer who worked on water distillation projects during his time as a graduate student at MIT, said.

 

 

These machines use the sunlight harvested by the photovoltaic cells in the solar panels to provide electricity, while heat from the panel also stimulates evaporation in the attached water distiller. From there, the vapor will be sent through a porous membrane that will filter out salt and other contaminants, thus producing clean water. The study’s co-author Peng Wang says “it doesn’t affect the electricity production…and at the same time, it gives you bonus freshwater.”

 

If implemented at solar farms, for example, then these dual-operational machines could help meet the globally increasing demand for both clean, fresh water and solar-powered alternative energy. During one of the experiments performed, the prototype device converted about 11% of the incoming light into electricity–which is right on par with commercial solar cells. While on the lower end, it is still a huge success for the team. When testing the water distillation feature, dirty water and salt water was fed into a device approximately one meter wide, and after it filtered out the pollutants, was able to generate about 1.7 kilograms (60 ounces) of clean water per hour.

solar power, solar energy, sun, green energy, alternative energy, climate change, solar panel, water, water distiller, water distillation, water power, hydro power, water, energy, global warming, efficiency, material, research, experiment, engineer, scientist, environment, environmental

 

Ni wants to know what’s next. “How are you doing to deploy this? Is it going to be on a roof?” His questions bring about the next phase of research and experimentation: practicality. The team now has to design models that will prove usable in various situations and applications, such as on the roofs of homes and floating in the ocean. Stability and structural security are a must, as are efficiency, cost, the materials used, and many other factors.

 

While this project is still in the middling stages, the concept behind it is quite extraordinary. It’s a way to combine two of the greatest green energy initiatives, and if made applicable to real-life situations, could open up a whole slew of future possibilities.

 

Credit: ScienceNews

 

 

Posted in All Posts, Industry Buzz | Tagged , , , , , , , , , , , , , , , , , , , , ,

3 Responses to Solar Powered Device Cleans Water and Produces Energy

  1. DL Nelson says:

    Great insights to new technology.
    Thanks for sharing.

  2. Roger Mello says:

    I like their thinking. The folks in Flint Michigan could surely use this. I was hoping that someone would come up with a solar panel and battery that could provide just enough energy to operate a dehumidifier. Dehumidifiers are energy pigs but serve a great purpose in order to avoid unhealthy mold. If the battery could carry the dehumidifier during the off hours this would be a winner for the consumer and help defer building new power plants. Consumers are not negative towards solar power, but the cost, etc. that goes along with filling up your roof with panels hasn’t taken off. If the consumer could try solar with a smaller investment, such as the concept above, and it proves to be cost effective you would see more participation in whole house solar.

    • Gregory says:

      Thanks for your insight, Roger. We actually produced a Trade Life video about Flint, Michigan, called Uniting for Flint and this was actually nominated for an award at the WATERtown Film Festival. This is a very interesting idea you have, and solar power would is a great benefit to those who have it. Testing at a smaller scale is, as you say, a nice way to try it out in order to see the results. Thanks again for sharing!

Leave a Reply to DL Nelson Cancel reply

Your email address will not be published.


Logo

Join Our Mailing List - Sign up and receive special offers and coupons