Skip to main content

A pinhole leak behind a washing machine used to mean a soggy subfloor and an insurance claim weeks later. In 2026, that same leak triggers a phone alert before the homeowner gets out of bed. Connected plumbing has moved from novelty upsell to a standard line on service estimates, driven less by gadget appeal than by tighter labor, rising insurance costs, and owners who want proof a system is working before it fails. 

Why It’s Showing Up on More Estimates 

Device-level data lets a technician roll a truck already knowing what failed, turning a two-visit job into one. Rising water bills and insurance premiums are pushing homeowners toward hardware that pushes back, and some carriers now discount premiums for houses with intelligent leak detection installed. Labor adds a third layer: a pair of studies released this month project a 550,000 plumber shortfall by 2027, making every avoided emergency call worth more than it used to be. 

What’s Actually in the Van This Year 

Two categories cover most of the current demand. Whole-home leak detection, like Flo by Moen, sits on the main line and shuts off water automatically. For spot monitoring, a Smart Leak Detector covers washing machines and water heaters; the full range is in the Leak Detectors category. 

Backflow assemblies now carry flood sensors too. A Backflow Preventer Assembly with an integrated flood sensor alerts when a relief valve discharges excessively; standard options remain in the RPZ Assemblies category. Digital mixing valves with building automation connectivity are also entering the mix for multifamily and healthcare work; the Digital Mixing Valves category covers that emerging niche, while a conventional mechanical valve for a simpler job stays in the standard Mixing Valves category. 

Comparing the Two Categories 

Device Category  What It Monitors  Best Fit  Install Note 
Smart leak detection & shutoff  Flow, pressure, temperature, moisture  Whole-home or point monitoring  Needs Wi-Fi and nearby power 
Backflow with flood sensor  Relief valve discharge volume  Unattended mechanical rooms  Alerts need an add-on connection kit 

Specification Checklist 

  1. Check the Wi-Fi signal at the install location before quoting the job. 
  1. Confirm nearby power is available for any valve or sensor that needs it. 
  1. Verify manual override so water never fully cuts off due to a dropped connection. 
  1. Read the vendor’s subscription and app terms before finalizing the proposal. 
  1. On commercial jobs, confirm the device’s protocol matches the building’s BAS. 

Quick Wins on Existing Calls 

  • Pair water heater replacements with a leak sensor recommendation. 
  • Offer a standalone detector for laundry rooms on any service call. 
  • Mention insurance discounts when quoting a whole-home smart valve. 

Frequently Asked Questions 

Does a smart leak detector replace a regular inspection? 

No. It adds a layer of protection between visits, not a substitute for physical inspection. 

What happens if the power goes out? 

Behavior varies by model, so confirm the failure mode before installing. Reputable systems fail in a safe, predictable state. 

Do these devices need a subscription? 

Some do for advanced features like history or remote alerts. Confirm terms during the proposal stage. 

Should a job get a whole-home valve or point sensors? 

It depends on risk. A whole-home valve protects the entire structure; point sensors cost less and suit specific high-risk spots. Many jobs benefit from both. 

How does a flood sensor on a backflow assembly send its alert? 

The base assembly detects the flood condition, but sending an alert to a phone or building system requires an add-on connection kit, quoted separately. 

Leaks Happen, Detection Doesn’t Have To Be an Afterthought 

Connected plumbing responds to real pressure, not a marketing push, since tighter labor means fewer hands for emergency callbacks and rising water and insurance costs mean homeowners are actively looking for hardware that pushes back on both. None of that requires a plumber to become a smart-home specialist overnight. It requires knowing which two categories, whole-home shutoff and flood-sensing backflow, cover most of what customers are asking for, and knowing the handful of install details that separate a device that works from one that becomes a callback. The technicians who get ahead of this trend are not the ones with the most gadgets on the truck, but the ones who confirm Wi-Fi coverage before quoting, verify power availability before the rough-in, and walk the customer through manual override before calling the job done. Spec it with that discipline, and a one-time install becomes something closer to a service contract. The customer who gets a leak alert at two in the morning and remembers who installed the system is a customer who calls that same number for the next job.