Skip to main content
Thermal Image of Electrical connection

A well-planned electrical maintenance program can help facility owners improve equipment reliability, manage downtime, and plan service needs more effectively. NFPA 70B, Standard for Electrical Equipment Maintenance, gives electrical contractors a structured framework for building that approach. Rather than focusing primarily on repairs as they arise, contractors can use NFPA 70B to help customers establish planned maintenance practices that support equipment performance, electrical safety, and long-term reliability.  

The Missteps That Cost the Most 

The single most common and costly misstep is not having a written maintenance program at all. Without one, there is no consistent basis for deciding what gets inspected, how often, or by whom, which means every maintenance decision defaults to whoever happens to notice a problem first. A handful of other missteps compound that first one: 

    • Relying on run-to-failure maintenance for equipment whose failure mode carries real safety or production risk 
    • Skipping technician training specific to the tasks being performed, rather than assuming general electrical experience covers every piece of equipment 
    • Collecting inspection data without a process for analyzing it, which buries early warning signs in a folder nobody reviews 
    • Treating the maintenance program as a one-time setup instead of a living document that gets updated as equipment, staffing, and technology change 

What NFPA 70B Actually Asks For 

NFPA 70B is not a mandate to inspect everything constantly. It is a framework for building a maintenance program scaled to the criticality of the equipment involved. The standard supports a written program based on identifying critical equipment first, then matching inspection frequency and method to how much risk that equipment failure carries. A backup generator feeding life-safety systems gets a different maintenance cadence than a rarely used convenience outlet, and NFPA 70B gives contractors a documented basis for making that distinction defensible to a client or an inspector. 

The Technology That Makes It Practical 

A written program is the foundation, but modern diagnostic tools are what make a maintenance program catch problems before they become failures rather than after. Thermal imaging and clamp meter readings turn a visual inspection into a documented data point that can be compared against the last visit, not just a technician’s gut sense that something looked fine. 

Tool  What It Catches  Why It Matters for a 70B Program 
Thermal imaging camera  Loose connections, overloaded circuits, failing components showing early heat rise  Non-contact scan documents a full panel in seconds, without opening it live 
Clamp meter  Current draw drifting outside normal range on a motor or circuit  Establishes a baseline reading to compare against on every future visit 
CMMS software  Missed or overdue inspection intervals across a large equipment inventory  Turns a written program into a tracked, auditable schedule instead of a binder 

A thermal imaging camera with onboard image storage lets a technician document panel scans across dozens of stops without carrying a laptop, which matters on a maintenance route that covers multiple properties in a single day. For contractors documenting findings for a formal report, a higher-resolution model like the Klein Tools TI290 transfers images wirelessly, cutting the administrative time between the scan and the client-facing report. 

A reliable clamp meter rounds out the basic diagnostic kit for establishing the current-draw baselines a maintenance program depends on. The Clamp Meters category covers models from a basic auto-ranging meter to a True-RMS unit built for logging trend data across repeat visits. 

Building the Program 

    1. Inventory the equipment on-site and flag which pieces are critical based on safety risk, production impact, or cost of unplanned downtime. 
    1. Set an inspection frequency and method for each criticality tier, using NFPA 70B as the reference for what a defensible schedule looks like. 
    1. Confirm every technician assigned to a task is properly trained and qualified for that specific equipment, not just electrical work in general, per OSHA and NFPA safety standards. 
    1. Establish a baseline reading with a thermal scan and clamp meter check on every piece of critical equipment before the program’s first scheduled maintenance visit. 
    1. Log every inspection result in a CMMS or equivalent tracking system rather than a paper file, so nothing falls through on a busy month. 
    1. Review the accumulated data on a set schedule to catch drifting trends before they become failures, not just to confirm nothing broke since the last visit. 
    1. Revisit and update the written program itself at least annually, incorporating new equipment, new technology, and lessons learned from the past year’s findings. 

Reading the Data Instead of Guessing 

A maintenance program only pays off if someone actually reviews what it collects. A few habits separate a program that catches problems early from one that just generates paperwork: 

    • Compare each new thermal scan against the prior visit’s image for the same equipment, not just against a generic temperature threshold 
    • Flag any clamp meter reading that drifts more than a small percentage from its established baseline, even if it is still within a nameplate-rated range 
    • Treat a repeat finding at the same location as a signal to investigate root cause, not just to note it and move on again 
    • Share trend data with the client in plain terms, since a facility owner who understands what the numbers mean is more likely to approve the repair before a failure forces the issue 

Frequently Asked Questions 

Does NFPA 70B require inspecting every piece of electrical equipment on the same schedule? 

No. The standard supports scaling inspection frequency and method to the criticality of each piece of equipment, so a life-safety generator and a rarely used convenience circuit do not need the same cadence. 

What is the difference between reactive, preventive, and predictive maintenance under this framework? 

Reactive maintenance responds after a failure occurs. Preventive maintenance follows a set schedule regardless of equipment condition. Predictive maintenance uses tools like thermal imaging and trend data to catch developing problems before they cause failure, which is where NFPA 70B pushes contractors toward over time. 

Can a small electrical contractor realistically offer an NFPA 70B-based program without a large CMMS investment? 

Yes. A written program, a thermal camera, a clamp meter, and a consistent spreadsheet or basic tracking tool can support a defensible maintenance program at a small scale. CMMS software becomes more valuable as the equipment inventory and client base grow. 

How does a thermal imaging camera actually prevent a failure rather than just detect one already happening? 

It catches early heat rise from a loose connection or overloading component before that heat progresses to a burned connection or component failure, giving time to schedule a repair rather than respond to an outage. 

What training does a technician need before performing NFPA 70B-based maintenance tasks? 

Training should be specific to the tasks and equipment being maintained, not just general electrical experience, and should align with OSHA and NFPA safety standards, including NFPA 70E where energized work or arc flash risk is involved. 

Is a written maintenance program a legal requirement, or just a best practice? 

NFPA 70B itself is a standard, not a law, though some jurisdictions, insurers, or contracts may reference it or require compliance. Even where it is not legally mandated, it is widely regarded as the best available framework for structuring a defensible maintenance program. 

How often should a written maintenance program itself be updated? 

At minimum annually, and also whenever new equipment is added, staffing changes significantly, or new diagnostic technology becomes available that changes how inspections are performed. 

What is the most common reason a maintenance program fails to catch a problem in time? 

Collecting inspection data without a consistent process for reviewing and comparing it against prior readings. A thermal scan or clamp meter reading that never gets compared to its baseline provides little more benefit than not taking it at all. 

Can predictive maintenance data help win new contract business, not just retain existing clients? 

Yes. Documented trend data and a clear maintenance history make a strong case in a bid, since a prospective client can see exactly how a contractor’s program would be structured and what it would catch, rather than taking a generic promise on faith. 

Does adding thermal imaging to a maintenance route significantly slow down a technician’s day? 

A modern handheld thermal camera scans a panel in seconds, which adds minimal time to a routine visit compared to the diagnostic value it provides. The larger time investment is in reviewing and comparing the resulting data afterward, not in capturing it. 

Powering Through 

A written maintenance program is not a hard sell once a client understands the alternative: paying for the same failure twice, once in downtime and once in the emergency repair bill. NFPA 70B gives contractors the structure to make that case with a document instead of a guess, and modern thermal and clamp meter tools turn every scheduled visit into data that actually justifies the next one.