Skip to main content
HVAC technician using a clamp meter to test the wiring on a ceiling-mounted unit heater in a warehouse.

A multimeter sits in every tech’s bag, gets pulled out on every call, and gets used wrong more often than it should. Touching leads to a terminal and calling out a number doesn’t mean anything without understanding which function to select, what a good reading looks like, and why the reading matters for the component being tested. Used correctly, a multimeter diagnoses a failed zone valve actuator in 30 seconds, catches a weak capacitor before a compressor lockout, and confirms a wiring fault before pulling apart a control board. 

Choosing the Right Meter: Multimeter vs. Clamp Meter 

A standard digital multimeter (DMM) measures voltage, resistance, continuity, and sometimes capacitance and temperature via test leads in contact with the circuit. A clamp meter adds a current jaw that measures amp draw by clamping around a single conductor, without breaking the circuit. 

For HVAC and plumbing work, the right setup is both. Use the DMM for voltage, resistance, continuity, and capacitor testing. Use the clamp meter for motor amp draw checks on compressors, circulators, and fans. An HVAC-specific clamp meter also measures DC microamps for flame sensor testing and includes a K-type thermocouple port for temperature readings. 

Measurement  Use Multimeter  Use Clamp Meter 
Voltage (AC/DC)  Yes, test leads  Yes, test leads on most models 
Continuity / wiring faults  Yes  Yes 
Resistance (coils, contacts)  Yes  Less common 
Capacitor microfarads (MFD)  Yes, with capacitance function  Rarely 
Motor amp draw  Awkward, requires breaking circuit  Yes, jaw clamps around conductor 
Inrush current (startup amps)  No  Yes, inrush mode 
Flame sensor microamps (DC)  Some models  HVAC clamp meters specifically 
Temperature  With K-type probe add-on  HVAC clamp meters include K-type port 

Browse clamp meters at SupplyHouse, including the Klein CL445 HVAC Clamp Meter (which Klein says measures AC current, inrush current, AC/DC voltage, DC microamps, capacitance, and temperature,) and the Klein CL800 AC/DC Clamp Meter with LoZ mode for eliminating ghost voltages. 

Safety First: Meter Ratings and Lead Placement 

CAT ratings on multimeters indicate the level of protection against transient overvoltages, which are dangerous voltage spikes that can occur on electrical systems. CAT III 600V is the minimum for HVAC and residential electrical work. CAT IV is required for work at the service entrance or main panel. Never use a CAT II meter (designed for electronic equipment) on HVAC circuits. 

Always set the function selector to the correct measurement type before connecting leads. Voltage mode presents high input impedance and will not damage the meter if connected to a live circuit, but always confirm what you are measuring before making contact. Connecting leads in resistance or continuity mode to a live circuit blows the meter fuse at best and damages the meter or causes injury at worst. 

  • Red lead: positive terminal, labeled V/Ω/mA 
  • Black lead: negative terminal, labeled COM 
  • For current measurement above 10A on a standard DMM: move red lead to the 10A input jack (if equipped) or use a clamp meter instead 
  • Always de-energize the circuit before testing resistance or continuity 

How to Test Voltage 

Voltage testing is the most common multimeter task on HVAC and heating work. The most important distinction: AC (alternating current) for line voltage and low-voltage control circuits; DC for certain control boards and battery-backed systems. 

  1. Set the selector to VAC (AC voltage). If the meter is not auto-ranging, select a range above the expected voltage. 
  1. Insert the black lead into COM and the red lead into the voltage input. 
  1. Touch the black lead to neutral or ground and the red lead to the hot terminal or test point. 
  1. Read the display. On a 24V control circuit, expect 24-28V. On a 120V circuit, expect 115-125V. On a 240V circuit, expect 230-250V. 

Testing 24V zone valve actuator terminals: set to VAC, touch leads across the two motor terminals with the zone calling for heat. Reading of 24V confirms the ZVC is sending voltage. No voltage means the problem is upstream: thermostat, wiring, or ZVC panel. 

Ghost voltages: induced voltages from nearby conductors can show 5-50V on a supposedly dead circuit. LoZ (low impedance) mode on meters like the Klein CL800 eliminates ghost voltages by presenting a low-resistance load that collapses induced voltage. Use LoZ when confirming a circuit is de-energized. 

How to Test Continuity 

Continuity testing confirms an unbroken electrical path between two points. It’s the fastest way to verify that a switch, fuse, thermostat contact, or wire run is intact. 

  1. Set the selector to the continuity symbol (typically a diode symbol with a sound wave, or Ω with a tone indicator). 
  1. Touch both leads together to confirm the meter beeps (circuit complete). 
  1. De-energize the circuit under test entirely. Continuity tests only work on dead circuits. 
  1. Touch leads to both ends of the component or wire segment being tested. 
  1. A continuous tone means continuity: the path is intact. Silence or OL (open loop) means the path is broken. 

Practical uses: testing a suspected blown fuse (no tone = blown), verifying a thermostat contact closes when the setpoint is reached, confirming a zone valve end switch closes when the valve reaches full-open, checking a wire run for a break. 

How to Test Resistance 

Resistance testing (in ohms, Ω) characterizes coils, motor windings, and heating elements. Unlike continuity, resistance gives a specific value that can be compared to spec. 

  1. De-energize the circuit. Resistance testing on live circuits damages the meter. 
  1. Set the selector to Ω. If not auto-ranging, start at a higher range and step down. 
  1. Touch leads to both terminals of the component. 
  1. Read the value. 

 

Component  Expected Resistance Range  Notes 
Zone valve actuator coil  20-200 Ω depending on brand  Typical coil reads ~45 Ω. OL = open coil, 0 = shorted 
Circulator pump motor winding  5-50 Ω depending on HP  Check lead-to-lead and lead-to-ground 
Electric heat strip element  5-50 Ω  OL = open element 
Thermostat bimetal or contact  0 Ω when closed, OL when open  Test with thermostat calling 
Transformer primary winding  Varies — no universal range  Verify against nameplate VA rating 

How to Test a Capacitor 

A failing run capacitor is the most common single-component cause of no-cooling calls. Many multimeters with a capacitance function can check MFD values quickly and safely. 

  1. Discharge the capacitor before testing. Use the capacitor and meter manufacturer’s recommended safe-discharge method, and never short the terminals directly. 
  1. Set the selector to capacitance (usually labeled F or μF with a horseshoe symbol). 
  1. Touch leads to the capacitor terminals. 
  1. Read the MFD value on the display. 

A capacitor rated at 45 MFD should read within its labeled tolerance. Many HVAC run capacitors are marked ±6%, which would put a 45 µF capacitor at about 42.3 to 47.7 µF. A reading outside that range means the capacitor is weak and should be replaced before the motor fails. A reading of zero or OL means the capacitor is open and has already failed. 

How to Use a Clamp Meter for Motor Amp Draw 

Amp draw testing with a clamp meter is the fastest way to catch a motor running hard before it fails. It’s non-invasive: no circuit interruption, no exposed terminals beyond what’s already accessible. 

  1. Open the jaw of the clamp meter by pressing the trigger. 
  1. Clamp the jaw around a single conductor only. Clamping around a two-conductor or multi-conductor cable reads net current (which is nearly zero on a balanced circuit) and gives a meaningless reading. 
  1. Read the display. Compare to the nameplate FLA (full load amps) on the motor or component. 

A motor drawing significantly above nameplate FLA is running hot. Common causes: capacitor weak or failed, mechanical binding in bearings, low voltage, refrigerant system restriction (for compressors). 

A motor drawing below nameplate FLA isn’t necessarily healthy. An abnormally low reading can still point to an electrical or load problem, depending on the motor and system. Cross-reference with voltage testing and resistance to complete the diagnosis. 

Browse HVAC tools at SupplyHouse, including the Klein CL320 HVAC Clamp Meter with DC microamp mode for flame sensor testing and the Klein CL220 Clamp Meter with Thermocouple. 

Frequently Asked Questions 

What is the difference between True RMS and average-responding multimeters? 

True RMS meters accurately measure non-sinusoidal waveforms, including the distorted waveforms produced by variable frequency drives, ECM motors, and electronic controls. Average-responding meters assume a pure sine wave and read low on distorted signals. For HVAC work with modern equipment, True RMS is the correct choice. 

My meter reads around 5V on a supposedly dead circuit. Is the circuit live? 

Probably not. Induced voltage from adjacent conductors can show apparent voltage on a high-impedance meter input. Switch to LoZ (low impedance) mode to confirm. If the reading collapses to zero in LoZ mode, the circuit is dead. If it stays up in LoZ mode, the circuit has actual voltage. 

Can I test a capacitor while it’s still in the circuit? 

No. Parallel resistances in the circuit affect the reading and give false values. Always disconnect at least one lead of the capacitor from the circuit before testing. Discharge it first. 

What does OL mean on the display? 

OL stands for overload or over limit. On voltage, it means the reading exceeds the selected range. On resistance or continuity, it means the circuit is open (no path). On capacitance, it typically means the capacitor is open. 

How do I test a flame sensor with a multimeter? 

Set the meter to DC microamps (µA DC) and connect it in series by disconnecting the wire at the flame sensor terminal, then connecting one meter lead to the sensor rod and the other to the disconnected wire. Meters with a dedicated DC microamp mode like the Klein CL320 or CL445 make this test straightforward. A healthy sensor reads between 0.5 and 10 µA, with 2 to 6 µA most common in the field. Below 0.5 µA typically indicates a dirty or failing rod. Always verify against the equipment manufacturer’s minimum threshold, as control boards vary in sensitivity. 

What is CAT rating and which do I need for HVAC work? 

CAT ratings indicate how much transient overvoltage a meter can withstand. CAT III 600V covers most HVAC and residential electrical work including panel interiors, feeders, and control circuits. CAT IV is required at the service entrance. Using an under-rated meter on high-energy circuits is a safety risk. 

Can I test 24V thermostat wiring with the same meter as 240V circuits? 

Yes. A CAT III 600V meter handles both. The key is setting the correct function (VAC) and an appropriate range before connecting leads. Auto-ranging meters handle range selection automatically. 

Measure Twice, Diagnose Once 

A multimeter used correctly cuts diagnostic time in half and eliminates parts-swapping. Set the right function, understand what a good reading looks like for the component being tested, and the meter tells the truth. A circulator drawing 2.1 amps when nameplate says 1.6 amps is failing. A zone valve coil reading OL has an open winding. A capacitor at 38 MFD on a 45 MFD rating is already compromised. The meter knows. All that’s needed is knowing how to ask. 

Browse clamp meters including the Klein CL445 HVAC Clamp Meter and all HVAC tools at SupplyHouse.