Skip to main content
Installing an electrical outlet in to the white wall box

Replacing an electrical outlet improves safety, reduces energy waste, and solves common electrical annoyances like flickering lights or weak connections. Follow this detailed, step-by-step guide to confidently replace an electrical outlet.

Why Replace an Electrical Outlet?

  • Makes the home safer: Modern outlets feature tamper-resistant shutters to protect children and pets.
  • Energy Efficiency: Secure connections lower resistance, saving energy and extending the life of connected devices.
  • Reliable Performance: New outlets eliminate flickering, buzzing, and overheating issues.

Tools You’ll Need

Materials to Get

Step-by-Step Guide

Step 1: Turn Off the Power

  • Go to your breaker panel and turn off the circuit breaker connected to the outlet.
  • Confirm the power is off by placing a voltage tester near the outlet slots and terminals.

Step 2: Remove the Old Outlet

  • Unscrew and remove the wall plate.
  • Unscrew the outlet from the electrical box and carefully pull it out.
  • Re-check for voltage before touching any wires.

Step 3: Identify and Label the Wires

  • Typical color codes: hot (black/red wires), neutral (white wires), ground (green or bare copper).
  • Mark each wire with masking tape or take a clear photo for easy reference.

Step 4: Disconnect and Inspect Wires

  • Loosen the screws or use a small screwdriver to release push-in connections.
  • Gently straighten hooked wires with needle-nose pliers.
  • Replace damaged or brittle wires immediately.

Step 5: Prepare the New Outlet

  • Match your new outlet’s amperage rating (15A or 20A) with your existing circuit.
  • Choose outlets labeled “TR” (tamper-resistant) for enhanced safety.

Step 6: Connect Wires to the New Outlet

  • Strip approximately ¾ inch of insulation from wire ends.
  • Loop each wire clockwise around respective screws:
    • Hot (black/red) to brass screws
    • Neutral (white) to silver screws
    • Ground (green/bare) to green screws
  • Tighten screws until wires are secure (firmly, but not overtightened).

Step 7: Install the New Outlet

  • Fold the wires neatly into the electrical box without sharp bends.
  • Securely fasten the outlet with screws so it sits flush against the wall.
  • Attach the new wall plate carefully to avoid cracking.

Step 8: Turn Power On and Test

  • Restore power by turning the circuit breaker back on.
  • Test the outlet using a voltage tester or a plug-in device.
  • Ensure the plugs fit securely and there is no sparking or looseness.

Troubleshooting Tips

  • Outlet not working? Confirm the breaker is fully reset and check connections.
  • No downstream power? Inspect previous outlets or switches for loose connections.

Expert Recommendations

  • Install GFCI outlets in kitchens, bathrooms, garages, and outdoors per NEC guidelines.
  • Consider USB-charging outlets for convenient charging.
  • Use AFCI circuit breakers in bedrooms and living areas for additional fire protection.
  • Ensure your electrical boxes sit flush; use drywall spacers if needed.
  • Choose high-quality specification-grade or hospital-grade outlets for heavy-duty use.
  • Replace wall plates to match décor and maintain a professional look.

Frequently Asked Questions (FAQs)

Q: How can I tell if my outlet needs replacement?

A: If it feels loose, sparks, or exhibits visible damage, discoloration, or burn marks.

Q: What’s the difference between a 15A and 20A outlet?

A: 20A outlets have a horizontal slot for certain high-current devices; typically, household outlets are 15A.

Q: Is it necessary to turn off the circuit breaker?

A: Yes, absolutely. Otherwise you’ll get shocked. Turning off the power keeps you safe.

Q: Can I install a GFCI outlet myself?

A: Yes, GFCI installation follows similar steps but includes built-in protection for damp areas as per NEC guidelines.

Q: Why use tamper-resistant outlets?

A: Tamper-resistant outlets include shutters that only open when equal pressure is applied simultaneously, protecting children from inserting objects.

Replacing an electrical outlet is an accessible DIY task that enhances the safety and functionality of your home. With the right tools, clear instructions, and quality materials available from Supplyhouse, anyone can complete this project successfully. Take your time, follow each step carefully, and enjoy the satisfaction of improving your home’s electrical safety and efficiency.