Skip to main content
radiant-floor-heating-pex-tubing-installation

Radiant and hydronic systems reward good design. A well planned system delivers even temperatures, quick recovery, quiet operation, and lower energy bills for decades. A thrown together layout with guesswork sizing and random zoning delivers the opposite. Hydronic design looks complex from the outside, but it breaks into a series of decisions that follow a clear order. 

The goal here is not to replace local codes, manufacturer manuals, or full engineering work. The goal is to give a working blueprint for how a tradesperson or advanced DIY planner can think through hydronic design from first sketch to material list, with the right tools and product families bookmarked along the way. 

Design goals for a hydronic system 

Before diving into BTUs and pipe sizes, it helps to define what a good system does in real life. 

A solid hydronic design: 

  • Delivers target room temperatures on the coldest design day 
  • Uses supply water temperatures that match the chosen emitters 
  • Keeps flows, velocities, and pressure drops within reasonable limits 
  • Runs quietly, without air noise or water hammer 
  • Uses controls that match the building and occupants 
  • Protects the heat source and components from oxygen, dirt, and abnormal conditions 

Hydronic systems can be forgiving once they are installed. Design mistakes, however, often hide inside oversized boilers, short cycling, noisy loops, or rooms that lag behind. Starting with load, then working forward through emitters, piping, and equipment keeps decisions in the right order. 

Step 1: Start with heat loss and design conditions 

Hydronic design starts with load, not with boiler catalogs. 

Key decisions at this stage: 

  • Outdoor design temperature for the region 
  • Indoor design temperatures by room or space type 
  • Construction details such as insulation levels, windows, and air leakage 
  • Floor coverings for any radiant zones 

Room by room heat loss calculations provide the best foundation. Tools such as the Slant/Fin Hydronic Explorer heat loss calculator app allow an installer or designer to enter rooms, surfaces, and construction details, then calculate required BTUs and suggest baseboard or boiler sizes. 

For a quick first pass on whole building load or boiler capacity, the Boiler BTU Calculator from Supplyhouse is a useful starting point: 

The broader calculators page collects other tools, including radiant heat resources: 

For a deeper dive into boiler sizing math and safety factors, this article pairs well with the design work: 

Once room loads are in hand, the design can move on to emitters. 

Step 2: Pick system type and heat emitters 

Hydronic design revolves around the relationship between three things: 

  • Room heat loss 
  • Emitter output at a given water temperature 
  • Boiler or heat source capability 

Common emitter options: 

  • Baseboard 
  • Panel radiators 
  • Cast iron radiators 
  • Radiant floor, wall, or ceiling 
  • Fan coils or air handlers 

Relevant Supplyhouse categories: 

Radiant floor options get extra help from products such as Ultra-Fin plates and above floor panels. For example: 

Emitter comparison at a glance 

Exact numbers depend on manufacturer data and water temperatures, but the table below gives a quick feel for where each emitter shines. 

Emitter type  Typical supply temps (approx.)  Strengths  Common Supplyhouse links 
Baseboard  160–200 °F  Simple, familiar, easy to zone  Baseboard heaters: https://www.supplyhouse.com/Baseboard-Heaters-808000 
Panel radiators  120–180 °F  Good at low temps, fast response, clean look  Buderus panel radiators: https://www.supplyhouse.com/Buderus-Panel-Radiators-13370000 
Cast iron radiators  140–200 °F  High mass, gentle heat, long coast down  Radiators: https://www.supplyhouse.com/Radiators-21844000 
Radiant floors  90–140 °F  Very even comfort, invisible equipment, quiet  Radiant heat: https://www.supplyhouse.com/Radiant-Heat-297000 
Fan coils  120–180 °F (or lower, variable)  Compact units, pairs well with ducted air movement  Heating supplies: https://www.supplyhouse.com/Heating-Supplies-193000 

Radiant heat benefits from careful surface temperature control. Many designers keep finished floor temperatures below roughly 87 °F to keep surfaces comfortable and protect wood floors: 

Once emitter types and target water temperatures are picked, loop layouts and zoning can start to take shape. 

Step 3: Plan zones, loops, and manifolds 

Zoning is where design begins to match real buildings and real people. 

Common zoning strategies: 

  • By floor 
  • By exposure (north vs south) 
  • By room type (living areas vs bedrooms vs baths) 
  • By usage patterns (spaces used all day vs rarely used zones) 

Hydronic manifolds sit at the center of many modern designs. Manifolds distribute supply water to multiple loops and make balancing, isolation, and service much easier. 

Key Supplyhouse resources: 

A good example of flexible manifold design: 

Practical zoning tips: 

  • Pair spaces with similar load profiles on the same zone where possible. 
  • Avoid over zoning tiny rooms with micro zones that will short cycle the boiler. 
  • Give bathrooms and high comfort spaces their own loops or circuits when budget allows. 
  • Keep loop lengths within manufacturer recommendations to limit pressure drop and keep balancing manageable. 

Radiant heat packages from Supplyhouse can shortcut some of this work by bundling manifolds, controls, and tubing for common square footages: 

Step 4: Choose piping, tubing, and oxygen control 

Pipe choice affects longevity and boiler protection more than most people realize. 

Common materials: 

  • Copper for near boiler piping, air eliminators, and closely spaced tees 
  • Barrier PEX or PEX AL PEX for radiant floors and many distribution runs 
  • Steel or black iron where boilers require it 

Oxygen barrier PEX deserves special attention. Many hydronic heat sources and cast iron components do not tolerate constant fresh oxygen. Oxygen barrier tubing and closed loop designs protect boilers, cast iron circulators, and ferrous components from rust. 

More detail on barrier tubing: 

Relevant categories at Supplyhouse: 

Careful coordination between tubing layout, manifold locations, and joist structure prevents fights with framing later. 

Step 5: Select and size the boiler or heat source 

Once loads and emitters are settled, boiler selection can finally happen. 

Major decisions: 

  • Fuel type (natural gas, propane, oil, electric) 
  • Boiler style (standard, condensing, combi, or dedicated heat only) 
  • Output capacity in BTU/h 
  • Minimum firing rate and turndown ratio for modulating models 

Supplyhouse covers a wide range of boilers and hydronic heat sources: 

Hydronic and radiant accessories live in the Heating Supplies section: 

Design pointers: 

  • Match boiler output to calculated load with a reasonable safety factor, not random square footage rules. 
  • Check that the boiler minimum firing rate plays well with the smallest active zone to limit short cycling. 
  • Confirm boiler compatibility with low temperature emitters when radiant floors dominate the load. 

For retrofit jobs where existing baseboard or radiators stay in place but radiant floors are added, this article outlines a design path: 

Step 6: Circulators, controls, and balancing 

Circulators are the heart muscles of a hydronic system. Flow must be high enough to carry heat, but not so high that noise and erosion show up. 

Supplyhouse circulator resources: 

A small detail that saves service time: 

Circulator design considerations: 

  • Total system head at design flow 
  • Variable speed vs fixed speed pumps 
  • Primary/secondary setups where supply temperatures differ across circuits 
  • Internal flow checks vs separate check valves 

On the control side, hydronic design might involve: 

  • Standard thermostats for baseboard zones 
  • Outdoor reset controls that trim supply temperature based on outdoor conditions 
  • Mixing controls or injection pumps to feed radiant floors at lower temperatures than the boiler loop 
  • Radiant specific thermostats and floor sensors that prevent overheated floors 

Many manifolds include flow meters and balancing valves. That hardware makes fine tuning loop flows easier once the system is filled and purged. Radiant and PEX manifold options from Supplyhouse give a range of choices for stainless, brass, and composite headers: 

Step 7: Air elimination, expansion, and protection 

A beautifully sized boiler and carefully zoned manifold will still misbehave if air and dirt ride along for the trip. 

Core protection pieces: 

  • Air eliminators at the hottest, lowest pressure point near the boiler 
  • Automatic air vents on radiators and high spots where appropriate 
  • Expansion tank sized for system volume and temperature swing 
  • Dirt separators or combination air and dirt separators in systems with steel, cast iron, or older piping 

Supplyhouse air elimination resources: 

Air separators such as microbubble style eliminators remove very small bubbles that standard vents often miss, which leads to quieter operation and more reliable flow through emitters. 

Expansion tank selection should follow manufacturer charts based on total water volume, temperature swing, and static fill pressure. Many designers mount the expansion tank at the same point as the primary air eliminator to keep the system point of no pressure change consistent. 

Design checklist for a hydronic heating system 

A quick checklist helps lock in the sequence: 

  1. Gather project data 
  • Climate and outdoor design temperature 
  • Building envelope details and floor finishes 
  1. Run heat loss calculations 
  • Room by room loads using hydronic calculators 
  • Whole building load for boiler sizing 
  1. Select emitters and target water temperatures 
  • Baseboard, radiators, radiant floors, or combinations 
  • Match output at design temperatures to room loads 
  1. Lay out zones and manifolds 
  • Logical zoning by use and exposure 
  • Manifold locations and loop lengths 
  1. Choose tubing, piping, and oxygen control strategy 
  • Barrier PEX where required 
  • Pipe sizes and materials for distribution 
  1. Size and select boiler or heat source 
  • Output matched to heat loss with appropriate safety margin 
  • Modulation range aligned with smallest active loads 
  1. Pick circulators and controls 
  • Flow and head calculations for each circuit 
  • Thermostats, mixing, and reset controls that fit the building 
  1. Add air elimination, expansion, and dirt separation 
  • Location and type of air separator 
  • Expansion tank and protection accessories 

Each step can be revisited as new information comes in, but following the order above avoids the trap of starting with equipment and then trying to make piping and emitters bend around it. 

Frequently asked questions about hydronic heating design 

How precise should heat loss calculations be? 

Close enough to match emitters and boiler size without padding the numbers. A room by room load prevents oversizing and keeps comfort consistent. 

Is boiler oversizing really an issue? 

Yes. Oversized boilers short cycle, waste fuel, and create uneven heat. A boiler matched to the actual load runs steadier and more efficiently. 

How many zones make sense? 

Enough to match how the building is used, but not so many that tiny zones cause short cycling. Group spaces with similar loads and schedules. 

Can radiant floors and baseboard run together? 

Yes, as long as water temperatures are managed. Radiant floors need lower temps, so mixing valves or primary secondary piping often enter the picture. 

How do you pick a circulator? 

Match the pump to the system’s required flow and head. Calculate both, then choose a circulator that can deliver that performance without strain. 

When does a buffer tank help? 

When the boiler’s minimum firing rate is high and the system has small zones. Added water volume steadies run times and cuts down on cycling. 

Is oxygen barrier PEX necessary? 

Barrier tubing is recommended for most closed loop hydronic systems with ferrous components. It limits oxygen entry and helps reduce internal corrosion. 

Big picture: why hydronic design matters 

Hydronic system design comes down to matching loads, emitters, water temperatures, and controls so everything works together instead of fighting itself. With a clear heat loss, well planned zones and manifolds, the right tubing and boiler, and solid air elimination and circulation, hydronic systems deliver quiet, even heat and lower energy bills over the long haul. A thoughtful design up front turns the mechanical room into an asset instead of a troubleshooting project every winter.