Skip to main content

Spring start-up can be quiet and predictable. Or it can start with a drip behind the siding and a sprinkler geyser near the driveway. 

Most failures trace back to one mistake: bringing water back too fast. 

A controlled start-up prevents split pipes, cracked fittings, and backflow leaks. Both tradespeople and serious DIYers can run the full process in under an hour on a typical home. Larger irrigation systems take longer, but the sequence stays the same. 

Quick Summary: Spring De-Winterization Checklist 

Outdoor Faucets 

  • Remove covers, hoses, timers, and splitters 
  • Open the interior shutoff slowly 
  • Open the faucet and inspect three leak points
  • Replace a leaking vacuum breaker if needed 

Irrigation Systems 

  • Return all valves and test cocks to operating position 
  • Open the irrigation main valve slowly 
  • Inspect the backflow device first
  • Run every zone and correct leaks or pressure issues
  • Reset the controller schedule for spring   

Follow the order. Speed is what causes damage. 

When to De-Winterize by Region 

Turning water on too early can lead to re-freeze damage. 

Use a simple rule across the U.S.: 
Wait until overnight lows stay above 32°F consistently, then pick a mild day for start-up. 

Regional patterns to keep in mind: 

  • Upper Midwest and Northern New England: Minneapolis, Fargo, Duluth, Bangor often require later spring start-ups. 
  • Mountain West: Denver, Salt Lake City, Boise can see late cold snaps. Stable overnight temperatures matter. 
  • Northeast and Mid-Atlantic: Philadelphia, New York City, Boston swing between warm days and cold nights. Pick a steady week. 
  • Pacific Northwest: Seattle and Portland have fewer deep freezes, but saturated soil exposes irrigation leaks quickly. 
  • South and Southwest: Atlanta, Dallas, Phoenix start earlier, but pressure spikes still crack weak fittings. 

A careful start-up prevents repeat service calls. 

Part 1: How to De-Winterize Outdoor Faucets 

Outdoor faucet failures usually show up in three locations: 

  1. Inside the wall 
  2. Behind the handle
  3. At the vacuum breaker 

Each location tells a different story. 

Step 1: Identify the Faucet Type 

Most homes use either: 

Standard Hose Bibb 

Water shuts off directly behind the handle. 

Frost-Free Sillcock 

Water shuts off inside the wall. The barrel drains when installed with proper pitch. 

If a hose stayed attached during freezing weather, water can remain trapped inside the frost-free barrel. That is a common cause of spring leaks. 

Step 2: Remove Covers and Disconnect Everything 

Remove: 

  • Foam covers 
  • Hoses 
  • Y-splitters
  • Timers 
  • Quick-connect fittings

Even fittings that look intact may have hairline cracks from freeze events. 

Step 3: Open the Interior Shutoff Slowly 

Locate the interior shutoff feeding the faucet. 

Controlled sequence: 

  • Open the valve slightly 
  • Wait 10 to 15 seconds
  • Open fully once the line stabilizes  

Fast pressurization can turn a weak joint into a visible leak. 

Step 4: Open the Faucet and Inspect Three Leak Points 

Run water for 30 to 60 seconds. Then check carefully. 

Leak Point A: At the Wall or Foundation 

Water at siding, rim joist, or foundation often indicates a split pipe inside the wall. 

Immediate move: shut off water and repair before using. 

Leak Point B: Behind the Handle 

A drip here often means the packing nut needs slight tightening. Small adjustments work best. Avoid over-tightening. 

Leak Point C: At the Vacuum Breaker 

Spray or dripping from the top cap usually signals freeze damage or internal wear. 

Replacement backflow and vacuum breaker options: 
https://www.supplyhouse.com/Backflow-Preventers-1619000 

Outdoor Faucet Troubleshooting 

Symptom  Likely Cause  First Move 
Water appears inside wall  Split pipe or failed joint  Shut off water and repair 
Drip behind handle  Packing nut loose  Tighten slightly and recheck 
Spray at vacuum breaker  Damaged vacuum breaker  Replace breaker components 
Weak flow  Debris or partially open valve  Flush line and verify valve position 

Why Backflow Protection Matters 

Hose connections create contamination risk. Fertilizer sprayers, buckets, and stagnant hoses can pull water backward into potable lines during pressure drops. 

ASSE-rated hose connection vacuum breakers exist for that reason. 

Browse compliant backflow options: 
https://www.supplyhouse.com/Backflow-Preventers-1619000 

Part 2: How to De-Winterize an Irrigation System 

Irrigation start-up is controlled re-pressurization. 

Large systems rarely fail from water alone. They fail when water returns too quickly. 

Step 1: Return the System to Operating Position 

Winterization usually leaves: 

  • Main irrigation valve closed 
  • Drain valves open
  • Backflow test cocks open
  • Controller powered off 

Reset everything before introducing water. 

Irrigation parts and repair components: 
https://www.supplyhouse.com/Irrigation-Supplies-and-Parts-36380000 

Step 2: Pressurize the Mainline Slowly 

Open the irrigation main valve gradually. 

Pause halfway to let the mainline fill. Once pressure stabilizes, open fully. 

Slow filling protects valve bodies, fittings, and backflow assemblies. 

Step 3: Inspect the Backflow Device First 

Backflow devices sit above grade and experience freeze exposure. 

Look for: 

  • Leaks at unions 
  • Cracked bodies 
  • Continuous discharge

Backflow repair and replacement options: 
https://www.supplyhouse.com/Backflow-Preventers-1619000 

Step 4: Run Every Zone, One at a Time 

Run each zone for at least 1 to 2 minutes. 

Watch for: 

  • Bubbling soil near a head, often a cracked riser 
  • Missing or broken heads 
  • Low pressure across an entire zone 
  • A zone that does not shut off

Sprinkler heads and accessories: 
https://www.supplyhouse.com/Irrigation-Sprinkler-Accessories-36391000 

Step 5: Reset the Controller for Spring 

Spring watering requirements differ from peak summer. 

Adjust: 

  • Run times 
  • Days per week 
  • Start times 

Controller options: 
https://www.supplyhouse.com/Irrigation-Sprinkler-Controls-36384000 

Irrigation Troubleshooting Table 

Symptom  Likely Cause  Fast Diagnostic Move 
One zone low pressure  Lateral break or missing head  Walk zone, look for pooling 
Bubbling around a head  Cracked riser or loose fitting  Dig and replace riser 
Poor coverage  Clogged or incorrect nozzle  Clean or replace nozzle 
Zone will not shut off  Valve debris or diaphragm failure  Inspect and rebuild valve 
Backflow leaks continuously  Freeze damage  Isolate and repair assembly 

A Practical Inspection Sequence 

A reliable order keeps spring callbacks down: 

  1. Pressurize slowly 
  2. Inspect backflow 
  3. Run zones 
  4. Fix hard leaks first 
  5. Correct performance issues second
  6. Adjust controller last  

Small discipline early prevents larger repairs later. 

FAQs 

How long should water run when de-winterizing an outdoor faucet? 

Thirty to sixty seconds usually reveals slow leaks. Longer runs help expose seepage behind siding or at the handle. 

Why remove the hose before turning water back on? 

Hoses and timers trap water inside frost-free barrels. Pressurizing trapped water reveals freeze damage quickly. 

What is the most common outdoor faucet leak in spring? 

Vacuum breaker leakage and packing nut seepage are common. 

What is the safest way to start an irrigation system in spring? 

Open the main valve slowly, inspect the backflow device, then run zones individually. 

Why does one sprinkler zone have low pressure after winter? 

Often caused by a broken lateral line, cracked riser, or missing head. Walking the zone typically identifies the wet spot. 

Should compressed air be used during spring start-up? 

Compressed air belongs in fall winterization. Spring start-up focuses on controlled refilling and inspection. 

What parts commonly need replacement after winter? 

Vacuum breakers, cracked risers, swing joints, broken heads, and clogged nozzles. 

Irrigation repair categories: 
https://www.supplyhouse.com/Irrigation-Supplies-and-Parts-36380000 

Final Thoughts 

Water does not cause most spring damage. Sudden pressure does. 

Slow fill. 
Careful inspection. 
Zone-by-zone testing. 

For frozen pipe prevention context: 
https://blog.supplyhouse.com/how-to-prevent-frozen-pipes/ 

Spring is busy enough already. A controlled start-up keeps it that way.