Skip to main content
Mini-split systems offer powerful heating and cooling without ducts and without tearing apart walls. But choosing the right one takes more than matching a brand name to a product page. This how-to guide walks through every step, from sizing and zoning to install details and advanced features whether you’re a seasoned tradesperson or a homeowner picking out the first ductless system.

1. How to Measure and Size a Mini-Split

Measure Your Room

– Measure the length and width of each room you want to heat or cool. – Multiply length times width for square footage. – For odd shapes, break the room into rectangles and add the areas. Example: – A 12’ x 15’ bedroom equals 180 ft² – Add a connected closet (5’ x 6’ equals 30 ft²) – Total equals 210 ft²

Estimate Required BTUs

Use this rough guide:
Room Size (ft²) BTU Needed
150–250 6,000
250–350 9,000
350–450 12,000
450–550 18,000
*These are estimates, we recommend you consult an expert for a more detailed assessment of your system requirements. Adjust for: – High ceilings over 8 feet. – Large windows or lots of sunlight. – Poor insulation, add capacity or consider improving insulation. In cold climates, check each system’s heating capacity at low outdoor temperatures. Some can maintain heat down to minus 5 degrees Fahrenheit or even minus 13 degrees Fahrenheit.

Special Note for Garages

Garages come with unique challenges: – Insulation is often minimal, so heat and cool air escape faster. – Large garage doors leak heat and let in outside air every time you open them. – If your garage will be a gym, office, or living space, choose a unit with extra capacity above the standard BTU estimate. – Check local codes, as some regions limit heating in garages for safety reasons. Planning to condition a garage? It’s wise to size slightly larger and look for low ambient heating if you live in colder climates.

2. How to Pick Single-Zone vs. Multi-Zone

Single-Zone Systems

– One indoor head connects to one outdoor unit. – Ideal for a single room, garage, finished basement, or home addition. – Typically simpler to install. – Browse single-zone systems here:

Multi-Zone Systems

– One outdoor unit serves multiple indoor heads, often two to eight. – Useful for homes needing different temperatures in bedrooms, living spaces, or offices. – Reduces the number of outdoor units on exterior walls. – Browse multi-zone systems here: If you’re unsure, start exploring all mini split options here

3. How to Use a Mini-Split Calculator

Guessing is risky, especially if you’re choosing equipment for your home. Use Supplyhouse’s calculator to estimate BTUs for your space: https://www.supplyhouse.com/sh/control/MiniSplitCalculator The calculator recommends the right capacity. For precise results, consider hiring an HVAC professional to run a Manual J calculation.

4. How to Read Efficiency Ratings

SEER: Seasonal Energy Efficiency Ratio

– Measures cooling efficiency. – A higher SEER means lower electricity use during air conditioning season. – Example: A 20 SEER unit typically uses about 20 percent less electricity than a 16 SEER model for the same cooling load.

HSPF: Heating Seasonal Performance Factor

– Measures heating efficiency. – A higher HSPF means lower electric use in winter. – A good HSPF for cold climates is 10 or higher.

Energy Star

– Usually means a unit has at least 18 SEER and 9 HSPF or higher. – These units cost more initially but lower operating costs over time.

5. How to Compare Mini-Split Features

Must-Have vs. Nice-to-Have Features

Feature Must-Have Nice-to-Have
Inverter technology ✔️
Low ambient heating ✔️
Dry/Dehumidify mode ✔️
Wi-Fi/app connectivity ✔️
Auto swing louvers ✔️
Sleep mode ✔️
Turbo mode ✔️

Inverter Technology

Controls compressor speed instead of switching fully on or off. Benefits include precise temperature control, quieter operation, longer equipment life, and lower energy use during mild weather.

Heat Pump vs. Cooling Only

Heat pump models both heat and cool. Cooling-only models cost less upfront but can’t heat in winter.

Wi-Fi Connectivity

Lets you connect the mini-split to a smartphone app. Benefits include remote control from anywhere, scheduling, monitoring energy use, and geofencing that adjusts temperatures based on your phone’s location.

Auto Swing Louvers

Louvers move side-to-side or up-and-down automatically to help spread air evenly through the room.

Dry or Dehumidify Mode

Runs the fan at lower speeds to remove moisture without dropping room temperature too much.

Sleep Mode

Gently raises or lowers temperature overnight, balancing comfort and efficiency, and often changing the temperature by one or two degrees each hour until morning.

Turbo or Powerful Mode

Runs the compressor at maximum output for fast cooling or heating.

Low Ambient Heating

Important for cold climates. Standard heat pumps often struggle below about 30 degrees Fahrenheit. Low ambient models maintain heat operation down to 5 degrees Fahrenheit or lower. Always check manufacturer performance charts.

6. How to Plan for Installation

Electrical Requirements

– Most mini-splits use 208 or 230 volts and need 15 to 20 amps. – Check your electrical panel to ensure there’s space for a dedicated breaker. – Multi-zone systems might need higher amp circuits.

Line-Set Length

– Check the maximum line length in manufacturer specs, often between 50 and 65 feet. – Longer runs might need extra refrigerant.

Indoor Unit Location

– Must mount on a solid wall like studs or concrete. – Leave space around the unit for airflow, typically 6 to 12 inches on top and sides. – Avoid direct airflow blowing on people for comfort.

Outdoor Unit Placement

– Keep on a level pad. – Maintain at least 12 to 24 inches from walls for proper airflow. – Avoid places where snow, leaves, or debris can pile up.

Drainage

– Indoor units produce condensation. – A gravity drain is best. – If gravity draining isn’t possible, install a condensate pump.

7. How to Review Warranty and Support

– Compressor warranties often last 5 to 10 years. – Parts warranties usually cover 1 to 5 years. – Labor warranty varies by installer. – Check whether replacement parts are available locally for the brand you choose. Choosing a brand with solid support can save headaches if repairs are ever needed.

8. Troubleshooting Quick Guide

While professional service is best for major repairs, here’s a quick look at common mini-split issues and basic checks you can do:
Problem Possible Cause
System won’t power on Check breaker, power supply, or remote batteries
Weak cooling or heating Filters might be dirty, or low refrigerant charge
Strange noises Loose panels or foreign objects in the fan housing
Remote not responding Check for battery replacement, or re-pair the remote with the unit

9. Pre-Purchase Checklist

– Room measurements complete – Mini-Split Calculator used – Single-zone or multi-zone decision made – SEER and HSPF goals identified – Must-have feature list defined – Electrical requirements confirmed – Mounting and drainage plan established – Warranty terms reviewed – Troubleshooting knowledge ready – Installation plan or installer secured

10. Your Next Steps

Choosing the right mini-split system isn’t just picking a brand or a price tag. It’s about knowing your space, planning the install details, and deciding which features matter most for your comfort and budget. Whether you’re upgrading a single room, transforming a garage, or outfitting an entire home, the right mini-split keeps temperatures steady, energy bills lower, and noise to a whisper. Measure carefully, compare your options, and don’t rush the decision. A few extra minutes spent planning now can save hours—and dollars—later. When you’re ready to dive in, Supplyhouse has everything from detailed specs and calculators to a wide selection of trusted brands. Explore our mini-split lineup: Comfort shouldn’t be complicated. With the right information and tools, it isn’t. Optional Video Resource If you’d prefer a quick visual overview before diving into details, check out this helpful video explaining mini-split basics: