Skip to main content
An electrician wearing gray work gloves is stripping electrical wires with a stripper.

Overview 

Wire strippers are one of those tools you don’t think about until they let you down. A cheap pair will mangle insulation, nick copper, or fatigue your hands after a few hours. A quality pair makes every cut smooth, repeatable, and safe. For the electrician trimming out a 200-breaker panel or the DIYer replacing a light fixture, the right strippers save time and prevent callbacks. 

Browse the full selection of Wire Strippers and other Electrical Tools & Instruments at Supplyhouse. 

Why Tool Choice Matters 

Wire insulation is designed to protect copper and resist heat. Strip it wrong, and the conductor is weakened before it ever carries current. 

  • Nicked conductors: Even a shallow score reduces strand count or introduces stress points that can snap during terminations. 
  • Over-stripped conductors: Too much bare copper increases the risk of arcing in a box. 
  • Inconsistent lengths: Sloppy strips make terminations uneven and unreliable. 
  • Lost time: Re-cutting and re-stripping add minutes that pile up fast on high-volume jobs. 

A seasoned tradesperson knows how much productivity comes down to rhythm. Wire strippers are part of that rhythm. 

Quick Reference Chart 

Type  Best For  Gauge Coverage  Advantages  Tradeoffs 
Manual notched strippers  Everyday residential or commercial branch circuits  Typically 10–22 AWG  Durable, precise, inexpensive  Slower when hundreds of wires need stripping 
Spring-loaded strippers  Panelboard trim-outs, fixture terminations, repetitive work  10–22 AWG (solid & stranded)  Faster cycles, reduced hand fatigue  Slightly heavier and costlier 
Self-adjusting/automatic  Mixed-gauge, large-scale projects (industrial panels, control wiring)  8–22 AWG on many models  Consistent results without changing notches  Bulkier, less precise in cramped boxes 
Multi-purpose tools (strip + cut + crimp)  Service calls, light kits, or DIY work  Varies by model  All-in-one convenience; cuts screws, crimps terminals  Less durable for daily stripping 
Insulated 1000V-rated strippers  Live-adjacent work under NFPA 70E or site safety programs  Model-specific (often 10–20 AWG)  Added arc-flash protection; often spring-loaded  Higher cost, thicker grips 

Step-by-Step: Choosing the Right Wire Stripper 

Step 1: Match to Conductor and Jacket 

Goal: Strip insulation cleanly on the wire type you use most. 

  • NM-B (Romex®): Standard manual or spring-loaded strippers cover 12 and 14 AWG solid. 
  • THHN/THWN-2 in conduit: Look for strippers marked for stranded wire; stranded copper needs a slightly larger notch. 
  • Control wiring (16–18 AWG stranded): Automatic/self-adjusting strippers prevent strand loss. 
  • MC cable or larger feeders: Heavy-duty strippers or combination cutters handle thick jackets before stripping conductors. 

If the wrong tool is used, you’ll see shredded jackets, cut strands, or uneven pulls. Switching to the right notch or tool solves the problem. 

Step 2: Prioritize Features That Save Time 

  • Clear gauge markings (on both sides of the jaw) reduce mis-strips when working fast. 
  • Integrated screw cutters for 6-32 and 8-32 screws are handy during device installs. 
  • Length stops or scales keep strip lengths consistent for wirenuts or terminal blocks. 
  • Smooth pivots make repetitive use easier on the hands. 
  • Spring return keeps jaws open and speeds one-handed work in tight spaces. 
  • Textured grips stay secure with gloves or sweaty hands. 

A service tech may prefer a Klein 6-in-1 Multi-Purpose Stripper, while a panel installer may lean toward a spring-loaded dedicated stripper for speed. 

Step 3: Match to the Work Environment 

  • Tight junction boxes: Compact, slim-nose strippers avoid bumping walls or terminals. 
  • Service calls: Multi-purpose tools reduce how much goes in the pouch. 
  • Industrial work: Self-adjusting strippers excel when gauges change constantly across bundles. 
  • Live-adjacent environments: Insulated 1000V strippers, like the Klein Tools 9421R, add another layer of safety compliance. 

From Choosing to Using 

Once the right pair of strippers is in hand, the next step is technique. The tool only does its job if the wire is placed in the correct notch, held steady, and stripped with smooth pressure. The following steps walk through how to use wire strippers on both solid and stranded conductors without damaging the copper or the insulation shoulder. 

Step-by-Step: How to Use Wire Strippers 

Solid Copper (12 or 14 AWG) 

  • Select the exact gauge notch for solid wire. 
  • Insert wire to desired strip length, close handles evenly. 
  • Rotate slightly if jacket resists, then pull insulation off cleanly. 
  • Correct result: copper is bright, unscarred, and insulation shoulder is crisp. 

Stranded Copper (control or fixture wire) 

  • Use the stranded gauge notch, not the solid. 
  • Support the conductor to prevent strands from splaying. 
  • Strip in one steady motion. 
  • Correct result: no missing strands, no “brushy” copper ends. 

If Results Look Wrong 

  • Nicks: wrong notch size or dull jaws. 
  • Jagged pulls: jaws misaligned or sticky pivot. 
  • Slipping: worn edges or improper placement. 

From Using to Maintaining 

Good strippers will last years, but only if they’re treated like precision tools. Dirt, moisture, and wear can make even the best model start tearing insulation instead of cutting it clean. Regular cleaning, lubrication, and inspection extend service life and keep every strip consistent. The next section covers how to keep strippers in peak shape and when to retire them. 

Step-by-Step: Maintaining Wire Strippers 

Daily / Weekly 

  • Wipe jaws to remove insulation debris. 
  • Apply a drop of light oil to the pivot; cycle open/close. 
  • Keep them dry — wipe down after damp site work. 

Monthly 

  • Inspect jaws for burrs, chips, or dull edges. 
  • Check handle grips for wear or slippage. 
  • Verify screw-shear holes are intact. 
  • Test strip common gauges on scrap — results should be repeatable and smooth. 

Replacement Signs 

  • Persistent tearing or nicking even after cleaning. 
  • Excess side play at the pivot. 
  • Cracks in the jaws. 
  • Gauge markings worn beyond readability. 

When replacement time comes, stock up from Wire Strippers and keep a backup pair in the truck. 

Helpful Add-Ons for Better Work 

FAQs 

What size strippers work for most household wiring? 
A tool covering 10–22 AWG with separate notches for solid and stranded handles 12 and 14 AWG residential circuits plus common control wires. 

Manual vs automatic — which is better? 
Manual strippers give precision and control in tight boxes. Automatic/self-adjusting models shine on repetitive, mixed-gauge industrial or panel work. 

Are insulated 1000V strippers necessary? 
On live-adjacent work sites governed by NFPA 70E, yes. They provide extra arc-flash protection. For general residential DIY, standard non-insulated models suffice. 

Why do my strippers keep cutting strands? 
Likely you’re using the solid notch on stranded wire, or the jaws are worn. Always use the stranded markings and replace tools that dull. 

How long do strippers last? 
With daily pro use, expect several years. With DIY use, a quality pair can last decades if cleaned and oiled regularly. 

Which tool is best for one-bag service calls? 
A multi-purpose design like the Klein 6-in-1 Multi-Purpose Stripper combines stripping, cutting, crimping, and screw shearing. 

Conclusion 

Wire strippers may not look like much, but they influence every termination, splice, and panel you touch. The wrong pair slows you down, while the right one saves minutes on every connection — minutes that add up to hours over a job. Clean stripping also means fewer callbacks, stronger joints, and safer installs. 

Choose the right style for the work — manual for precision, spring-loaded for speed, automatic for volume, multi-purpose for service calls, insulated for compliance. Maintain them with cleaning and oil, inspect for wear, and retire them before they become a liability. 

Build a kit that covers all bases with Wire Strippers, Cable Cutters, Cutters & Scissors, Crimp Tools & Accessories, and Electrical Wire & Cable. With the right tools, both the seasoned tradesperson and the DIYer can make every strip clean, fast, and professional.