Boilers do one thing: move heat. But how much heat they move, and how efficiently they move it, depends on one critical factor: sizing. An undersized boiler runs constantly and never catches up. An oversized one short-cycles and wastes fuel. Either way, you lose.
Correct boiler sizing comes down to math and materials. Once you know how to calculate BTU requirements, you can match your boiler to the building, the climate, and the job.
Step 1: What Is a BTU?
BTU stands for British Thermal Unit — the amount of energy it takes to raise one pound of water by one degree Fahrenheit.
Boiler ratings are measured in BTUs per hour. A 100,000 BTU boiler delivers that much heat every hour, assuming ideal conditions.
Residential boilers usually fall between 50,000 and 300,000 BTU depending on home size, insulation, and outside temperature.
Step 2: Why Boiler Sizing Matters
If your boiler is too small, it won’t keep up on cold days. If it’s too big, it will short-cycle, turning on and off constantly, burning excess fuel, and wearing out faster.
Properly sized boilers run smoother, heat evenly, and last longer. They also cut operating costs and minimize maintenance.
Step 3: Rule of Thumb BTU Estimate
This quick reference gets you in the ballpark:
| Climate Zone | BTUs per Square Foot |
| Warm (South) | 25–35 |
| Moderate (Mid-Atlantic) | 40–45 |
| Cold (North/Northeast) | 50–60 |
Example:
A 2,000-square-foot home in Boston:
2,000 × 50 = 100,000 BTU/hr
That gives you a rough starting point. For real accuracy, you’ll need to run a full heat-loss calculation.
Step 4: How to Calculate Heat Loss Properly
Heat loss measures how much energy a building loses every hour on its coldest day. That’s the number your boiler needs to match.
Measure Heated Square Footage
Include any living spaces the boiler will serve.
Choose Your Climate-Based BTU Factor
| Region | Design Temp (F) | Heat Loss Factor (BTU/hr/ft²) |
| Southern States | 35–45 | 25–30 |
| Midwest | 20–30 | 35–45 |
| Northeast / Cold Climate | 0–20 | 45–60 |
| Mountain / Northern Zone | Below 0 | 55–70 |
Tip: Reference ASHRAE Climate Zones or Heating Degree Days (HDD) to fine-tune your design temp.
Adjust for Insulation and Windows
- Poor insulation or single-pane windows: Add 15–20%
- Excellent insulation or new windows: Subtract 10–15%
Multiply and Add a 10% Buffer
Multiply your square footage by the BTU factor, then add 10% for safety.
Example:
2,000 × 50 = 100,000
+10% = 110,000 BTU/hour
To check your estimate, use the BTU Calculator from SupplyHouse.
Step 5: Input vs. Output — What You’re Really Sizing
All boilers are rated by:
- Input BTU: the amount of fuel energy it uses
- Output BTU: the usable heat it delivers
A boiler with 100,000 BTU input and 80% efficiency delivers 80,000 BTU of actual heat.
Always size to output. If you need 100,000 BTU of heating, and your boiler is 90% efficient, you’ll need 111,000 BTU input.
Step 6: Matching Boiler Type to the Application
Not all boilers are built the same. Choose the right type for your system and climate.
Standard Gas Boilers
80–85% efficiency, great for baseboard and radiator systems. See Boilers
Condensing Boilers
90–97% efficiency, ideal for radiant and low-temp hydronic systems. See Condensing Boilers
Steam Boilers
Size based on radiator EDR, not square footage. Total your radiators’ EDR and use manufacturer guidelines.
Step 7: Add BTUs for Domestic Hot Water
If the boiler also heats your hot water, don’t forget to add that load. A heating load of 90,000 BTU and a domestic hot water load of 40,000 BTU means you need a boiler that delivers 130,000 BTU output. See Combination Boilers
Step 8: Don’t Forget Circulator Sizing
Moving heat is just as important as generating it.
Each gallon per minute (GPM) of water flow delivers about 10,000 BTU/hr at a 20°F temperature drop. So a 100,000 BTU system needs 10 GPM.
Choose circulators that match your system’s flow and head pressure. Browse Pumps and Flanges
Step 9: Match Boiler Output to Emitters
Your boiler may be sized perfectly for the structure, but can your emitters move that heat? Use these general capacities:
| Emitter Type | Output BTU/hr per ft or unit |
| Slant/Fin Baseboard | 550–700 per foot |
| Cast Iron Radiators | 150–250 per square foot |
| Panel Radiators | 2,000–5,000 per panel |
| Radiant Floor Loops | 20–40 per square foot |
Make sure your distribution system can handle the load your boiler delivers.
Step 10: Controls and Outdoor Reset
High-efficiency systems get even better with smarter controls. Adding outdoor reset improves boiler modulation and return water temperature, especially in condensing boilers.
Turndown ratio matters too: a boiler with 10:1 modulation can reduce cycling and run quieter during shoulder seasons.
Zoning with thermostats and circulators or zone valves also lets you customize comfort and reduce wasted energy.
Step 11: Real-World Example
House Size: 2,400 sq ft
Region: Northeast
Heat Loss Rate: 55 BTU/hr/ft²
Boiler Efficiency: 90% condensing boiler
2,400 × 55 = 132,000
+10% = 145,200
/ 0.90 = 161,333 BTU input required
Look for a boiler that delivers 145,000 BTU output and 160,000 BTU input. See Weil-McLain Boilers or Burnham Boilers
Step 12: Boiler Types and Efficiency
| Boiler Type | Efficiency | Best For |
| Gas / Propane | 80–85% | Baseboard and radiator systems |
| Condensing Gas | 90–97% | Radiant or low-temp hydronic |
| Oil | 84–87% | Homes without gas lines |
| Electric | 95–100% | Small zones or off-grid homes |
| Steam | 75–85% | Legacy steam systems |
Step 13: When to Recalculate BTU Load
Recheck your numbers if:
- You add insulation or upgrade windows
- You renovate or build an addition
- You switch emitters (e.g., from baseboard to radiant)
- You zone or re-pipe your system
Frequently Asked Questions (FAQs)
How many BTUs do I need per square foot?
Between 25 and 60 BTUs per square foot depending on climate and insulation.
Is it better to oversize a boiler?
No. Oversizing leads to short-cycling, fuel waste, and faster wear. Add only 10–15% for safety.
What’s the difference between input and output BTUs?
Input is the fuel the boiler uses. Output is the usable heat it delivers. Always size based on output.
Can one boiler heat both the house and water?
Yes. Combination boilers do both. Just be sure to size for both loads.
How do I calculate boiler horsepower?
1 boiler horsepower = 33,475 BTU/hr. Divide total BTUs by 33,475.
Do I need a condensing boiler?
If your system runs at low temps (like radiant floors), condensing makes sense. If not, standard efficiency may work fine.
What size circulator do I need?
Match flow rate (GPM) and head loss. Roughly 1 GPM per 10,000 BTU at 20°F drop.
How does insulation affect boiler sizing?
Tighter buildings lose less heat. That means lower BTU needs and smaller boilers.
What is turndown ratio and why does it matter?
Turndown ratio tells you how much a boiler can modulate its firing rate. A 10:1 boiler can drop to 10% of its max capacity, improving comfort and reducing cycling.
Final Thoughts
Boiler sizing isn’t a chore. It’s a check against waste, callbacks, and expensive mistakes. Get it right, and your system will hum for decades.
Start by calculating the heat loss. Add hot water if needed. Choose a boiler that meets the load, not one that looks close. Then size your circulators and zoning components accordingly.
Whether you’re planning a radiant system, retrofitting baseboard zones, or converting from oil to gas, SupplyHouse has everything you need, from high-efficiency boilers and circulators to fittings, valves, and controls.
Measure carefully. Size smart. Heat happy.