Skip to main content

SIG110DL BreezSignature G2 Series, Dual Speed Bath Fan with Light (110 CFM)

It’s likely you haven’t thought much about the air that you’re breathing in, especially in your bathroom. Unless there was a lack of oxygen, why would the thought ever occur to you? But now we’re sure it is on your mind.

 

Indoor air quality matters, which is why we decided to add Delta Breez ventilation fans to our site. Delta Breez offers high-quality and top-performing bathroom ventilation fans of varying sizes, airflow levels, and features to fit any budget. Taking control of the moisture in your home will improve indoor air quality and help to reduce the health risks associated. They’re ENERGY STAR qualified, (except for the BreezRadiance RAD80L), and most have been designated ENERGY STAR Most Efficient 2015. All of their fans are HVI-certified, California Title 24 compliant, and UL-listed.

 

5 Delta Breez Fans To Pick From

Recently Updated7

 

1. BreezSignature:

Offer ventilation solutions with motion and humidity-sensing andoffered in single or dual speed options. The energy efficiency exceeds the ENERGY STAR requirements by as much as an incredible 685% and has extremely quiet noise levels as low as <0.3 sones.

 

2. BreezSlim:

Combines a small size with fantastic power and performance, and is perfect for when there are space constraints. At only 1.0 sone, the Slim is the quietest fan around for its size, and the G2 models include a 4” metal oval duct with a 3” plastic adapter, and its enlarged grille helps when there are cutting errors. Take a look at the G1 and G2 models here.

 

3. BreezGreenBuilder:

Exceed ENERGY STAR efficiency requirements by as much as a whopping 835%, and also has the lowest noise rating available of <0.3 sones, with the use of DC motors. The fan only models are UL listed for both ceiling and wall mounted installations.

 

4. BreezSmart:

Combine power and efficiency through 3-phase DC motors for a cleaner environment. These also have a noise level of <0.3 sones when at full speed, and have motion and humidity-sensing options. They are sturdily built, yet don’t sacrifice appearance quality.

 

5. BreezRadiance RAD80L:

Low noise ceiling mounted ventilation fan and light with heater. Its 1300W heating element confirms to UL safety standards and it has a built-in thermostat to regulate temperature.