The first hard freeze of the season always brings the same calls. No water at the kitchen sink. A dry laundry box. A restaurant that can’t open. Every one of them is a race between the ice and the split it may already have caused.
Contractor Magazine’s Nov. 11 guide to frozen pipe calls laid out a workflow worth adopting before the cold settles in: triage on the phone, shut off the main before any heat goes on, thaw hidden lines without opening walls, inspect after the water comes back, and leave with a plan to keep it from happening again. Worth knowing up front: the author works for a plumbing tool retailer and points readers toward one brand of thawing machine. The workflow holds up regardless of brand.
Triage Before the Truck Rolls
A few questions on the phone sort an inconvenience from an emergency:
- Is there any water at all, or is the whole house dry?
- Is it one fixture or one area, or everywhere?
- Is water showing up anywhere it shouldn’t?
Water where it doesn’t belong moves the call to the top of the list. Commercial calls deserve extra urgency too, since a leak behind a wall or above a ceiling in a commercial space can travel a long way before anyone sees it.
While on the phone, give the customer one clear safety instruction: external heat only. The Nov. 11 guide lists heating pads, hair dryers, and hot towels as safe options, and it’s blunt about the rest: “never use an open flame.”
Shut Off the Main First
The single most important step happens before any thawing starts. Shut off the main. A split pipe on a closed system is a repair. A split pipe on an open system is a flood.
Two habits make this step smoother:
- Warn the customer. A crack hidden in a wall or crawlspace often shows up only once water starts moving again.
- Stock the truck. The guide recommends carrying repair couplings and push-to-connect fittings in common sizes on every truck. The SharkBite slip coupling lineup covers quick repairs on a split section, and a SharkBite Max 1/2″ coupling handles the most common branch size.
Thawing Hidden Lines Without Opening Walls
When the freeze sits inside a wall, under a floor, or in a buried service line, direct heat means demolition. Electric pipe thawing avoids that. A thawing machine passes low-voltage, high-current electricity through a metal water line, which heats the pipe wall and melts a thin layer of ice. Once water starts flowing, the flow finishes the job. The Nov. 11 guide puts a typical thaw at about 10 minutes.
The method works on copper and iron lines, since it depends on current passing through the pipe itself. Plastic lines need a different approach.
The guide’s setup procedure:
- Isolate the frozen section and open a faucet downstream.
- With the machine unplugged, clean two connection points on opposite sides of the freeze.
- Attach the cable clamps at least 15 feet apart.
- Remove any nearby insulation or heat tape.
- Uncoil the cables completely.
- Confirm the connections are tight before powering the machine.
Follow the machine manufacturer’s instructions on top of these steps. Every unit has its own limits and safety requirements.
| Machine | Output | Circuit | Reach (per manufacturer, as cited) |
| General Pipe Cleaners Hot-Shot HS320 | 320 amps | Standard 15-amp | Up to 100 ft. of pipe up to 1-1/2″ |
| General Pipe Cleaners Hot-Shot HS400 | 400 amps | 20-amp, with a low setting for 15-amp outlets | Up to 175 ft. |
Both models include two 20-foot cables and clamps. The Hot-Shot HS320 and Hot-Shot HS400 are both listed in the pipe thawing machine category. Both were on backorder at the time of writing, which reinforces the guide’s best piece of business advice: get a thawing machine on the truck in October, not the morning after the first cold snap.
After the Thaw: Walk the Whole System
Thawing isn’t the finish line. Run the water and walk the system. Freeze damage often stays hidden until pressure comes back, so check for leaks and confirm every affected fixture is flowing again before calling the job done.
Then find out why it froze. The Nov. 11 guide lists the usual causes:
- Poor or missing insulation
- Piping in exterior walls
- Outdoor plumbing that was never winterized
- Damaged siding letting cold air into a wall cavity
- Additions that changed how heat moves through a crawlspace
- Power outages during a cold snap
Turn the Emergency Into Prevention Work
The customer has never been more open to prevention than right after a freeze. The guide recommends booking follow-up work before leaving the site and framing it as protection, not a sales pitch. Natural next steps:
- Heat cable on exposed runs. Self-regulating cable like the Easy Heat PSR 50-foot pipe tracing cable protects lines that can’t be rerouted.
- Frost-free hose bibbs. A SharkBite 8″ anti-siphon frost-free sillcock installs without soldering, and a Bluefin 12″ expansion PEX frost-free sillcock fits expansion PEX systems with a longer reach into the heated space.
- Rerouting or replacing a line that freezes every year.
- Leak detection and automatic shutoff for homes left empty during cold weather.
- A fall winterization visit on the calendar for next year.
For the full prevention checklist to share with customers, SupplyHouse’s How To Prevent Frozen Pipes guide covers insulation, heat cable, outdoor fixtures, and sensors step by step.
Frequently Asked Questions
What’s the fastest way to thaw a frozen pipe inside a wall?
An electric pipe thawing machine can thaw a metal line inside a wall without opening it. It passes high current through the pipe to melt a thin layer of ice, and water flow does the rest, typically in about 10 minutes.
Can an electric pipe thawer be used on PEX or CPVC?
No. Electric thawing machines pass current through the pipe itself, so they work on copper and iron lines. Plastic lines need external heat.
Should the main be shut off before thawing a pipe?
Yes. Shutting off the main first means a split pipe becomes a repair instead of a flood once the ice clears.
Is it safe to use a torch on a frozen pipe?
No. The Nov. 11 guide is clear: never use an open flame. Use external heat sources such as heating pads or hair dryers, or an electric thawing machine on metal lines.
How far apart should the thawing machine clamps go?
The Nov. 11 guide recommends at least 15 feet apart, on opposite sides of the freeze. Always follow the machine manufacturer’s instructions.
Why do leaks show up after the pipe thaws?
Ice can split a pipe without any visible sign. The crack only leaks once pressure returns, which is why walking the whole system after thawing matters.
What causes pipes to freeze in the same spot every year?
Common causes include poor insulation, piping in exterior walls, damaged siding letting in cold air, and changes from additions or crawlspace modifications. Recurring freezes usually call for rerouting, insulating, or adding heat cable.
What should a plumber offer after a frozen pipe call?
Heat cable on exposed lines, frost-free hose bibbs, replacing lines that freeze repeatedly, leak detection with automatic shutoff, and a fall winterization visit.
Breaking the Ice on Winter Calls
Frozen pipe calls reward the shops that prepare early. Triage on the phone, shut off the main before thawing, use electric thawing for hidden metal lines, and walk the whole system once the water’s back. Then fix the reason it froze and book the prevention work while the customer’s still listening. Handle the first call right, and the second call is a winterization visit instead of an emergency.