Skip to main content

Recently Updated9

 

Quick and easy–  two words everyone wants to hear, and two words we can promise you perfectly describe press fittings. While conventional soldering gets the job done, there are many advantages associated with using a press fitting. It is much easier and quicker to install, with safety not being an issue. Copper press can be used in nearly all residential, commercial and industrial purposes, which is why we expanded our selection to include Cello’s Copper Press Fittings to the site.

 

 

The plus side to Copper press? They can be used for many applications such as potable water. Press fittings offer an alternative to soldering, with connections being forged using a fastening method between the fittings or valve and the tubing or piping.

 

 

You’ll find on our Fittings Finder the variety of copper press fittings available including elbows, couplings, tees, adapters, caps, unions, ball valves, and much more!