Skip to main content

Safety Staff Pointing on R32 with Warning SignA2L refrigerants aren’t new anymore, but the paperwork around them keeps evolving. As permitting offices and inspectors get more systems under their belts, the questions they ask have shifted from basic refrigerant identity toward specific compliance details: proper labeling, calculation documentation, and what needs to sit on-site during an inspection. Technicians who treat those details as an afterthought are the ones getting called back to a jobsite after a failed inspection. 

The Compliance Questions Inspectors Are Actually Asking 

Chapter 11 of the 2024 International Mechanical Code governs the design, installation, and repair of refrigeration systems using A2L refrigerants, and it doesn’t offer one blanket answer for every install. Calculations depend on the specific equipment, refrigerant charge, and building type, and because those calculations are equipment-specific, the manufacturer’s instruction manual has to spell out exactly how to complete them. That manual needs to travel with the job, not stay in a truck or a filing cabinet

What Belongs in the Permit Package 

  • The equipment- and refrigerant-specific instruction manual used to complete required calculations 
  • Documentation showing the calculated minimum room area or charge limit for the space 
  • Confirmation that installed equipment is listed and labeled to current product safety standards 
  • Proof that state and local A2L restrictions, including rules on mixing or changing refrigerants, have been checked against the job 

Keeping that manual on-site during the inspection isn’t optional in most jurisdictions. Building officials need it to verify the math, and a technician who shows up without it is inviting a second trip. 

Labeling Requirements Got More Specific 

The 2024 IMC requires clear markings on refrigerant piping identifying the flammable refrigerant hazard, and equipment manufacturers now include matching warning labels on the equipment itself under their product listings. The required piping identification reads: “WARNING, Risk of Fire, Flammable Refrigerant.” Skipping or letting a label fade isn’t just sloppy. It’s a code violation waiting to be flagged. 

Tools Still Need to Match the Refrigerant 

Tool Standard A1 Version A2L Requirement 
Manifold gauges Standard brass or aluminum gauge A2L-rated gauge calibrated for R-454B, R-32, and legacy refrigerants 
Recovery machine Standard recovery unit A2L-certified recovery machine 
Leak detector General refrigerant sniffer A2L-compatible detector rated for flammable blends 
Recovery cylinders Standard DOT cylinder Cylinder rated and labeled for A2L service per manufacturer and DOT guidance 

Electronic tools, gauges, and recovery equipment need a rating for flammable refrigerants to eliminate spark risk during operation. Techs stocking up can reach for the Navac N4A4B Pro Plus manifold gauge or the brass-body Navac NMG12A for charging and diagnostics, the Inficon Vortex Dual recovery machine or Fieldpiece MR45 for recovery, and the Fieldpiece DR82, Fieldpiece DR58, or Bacharach H-10 PRO for leak detection. Mixing standard A1 tools into an A2L job isn’t just a compliance issue. It’s a safety issue. 

Getting Ready for the Walkthrough 

  1. Confirm the installed equipment carries a current safety listing for the specific A2L refrigerant charged. 
  1. Pull the manufacturer’s calculation worksheet for minimum room area or charge limit and keep a printed copy with the permit documents. 
  1. Verify piping labels meet the updated warning language and haven’t faded or been covered during rough-in. 
  1. Check that every recovery machine, gauge, and leak detector on the truck carries an A2L rating before arriving on-site. 
  1. Bring the full equipment manual to the inspection rather than relying on a phone photo or a summary sheet. 

Frequently Asked Questions 

Does every A2L system need a refrigerant detection system installed? 

Yes, in most residential and light commercial applications above minimal charge thresholds. The specific requirement depends on refrigerant charge, room volume, and the calculation method built into the equipment manual. 

Can an existing R-410A system get retrofitted to run A2L refrigerant? 

No. A2L refrigerants aren’t drop-in replacements for A1 systems, and there’s no approved retrofit path. A full system change-out is required, though an existing compatible furnace can often stay in place with an added leak detection kit. 

What happens if a technician shows up to an inspection without the equipment manual? 

Inspectors may fail the inspection outright since they can’t verify the required calculations without it. Keeping a printed or digital copy on-site avoids the delay entirely. 

Are A2L refrigerants actually dangerous to work with? 

They’re mildly flammable, classified as Class 2L under ASHRAE Standard 34, and need a larger release plus an ignition source to combust. Following updated tool, ventilation, and handling practices keeps risk low. 

Do all states enforce the same A2L permitting rules? 

No. Adoption of the 2024 IMC and related A2L restrictions varies by state and municipality, so checking local amendments before pulling a permit is essential. 

What’s the difference between A2L mitigation levels m1, m2, and m3? 

They represent escalating charge thresholds under ASHRAE Standard 15 that trigger different levels of required mitigation, from basic shutdown controls to more rigorous ventilation and additional sensors as charge size increases. 

Do brazing procedures change with A2L refrigerant? 

Brazing should never happen on a charged system regardless of refrigerant type, but techs should work in a well-ventilated area and follow A2L-trained procedures as an added precaution against flammable refrigerant exposure. 

Is R-32 treated the same as R-454B for compliance purposes? 

Both are A2L refrigerants and fall under the same general code requirements, though specific charge limits, sensor requirements, and manufacturer instructions vary by refrigerant and equipment model. 

Does a service call on an existing A2L system require the same documentation as a new install? 

Repairs that involve changing refrigerant or replacing major components typically require rechecking compliance, especially around labeling and leak detection, even when a new permit isn’t pulled. 

How long will the industry keep generating new A2L compliance questions? 

Given the phased GWP limits running through 2027 across different equipment categories, expect permitting and inspection questions to keep evolving for at least another couple of years. 

Staying Cool Under (Low) Pressure 

The refrigerant shortage headlines have faded, but the compliance side of the A2L transition hasn’t slowed down one bit. Technicians who keep the right manual on the truck, label piping correctly, and carry A2L-rated tools walk into inspections with confidence instead of crossed fingers. That’s the difference between a quick sign-off and a return trip nobody wanted to make.