Skip to main content
HVAC technician sitting in the back of a service van stocked with refrigerant cylinders

The call usually starts with a good deal. A brand nobody’s heard of, a condenser at a number that’s hard to ignore, and a seller who swears it’ll work with R-410A, R-32, or R-454B. Whatever the customer wants. 

A pitch like that should set off alarms. On Oct. 27, ACHR News reported that HARDI, the trade association for HVACR distributors, is warning contractors and distributors about products that might not comply with federal efficiency and safety regulations, and urging them to report suspicious equipment “before they become dead inventory…or worse.” For a contractor, “or worse” means equipment that’s already installed in a customer’s home. 

What HARDI Is Seeing in the Channel 

The warning builds on an earlier alert. ACHR’s Oct. 9 coverage reported that unfamiliar manufacturers, importers, and brands have been offering equipment to HARDI members, including R-410A condensing units built in 2025 or 2026 that may not meet DOE efficiency standards. 

The rules around those units are specific. Per the same report, newly built R-410A condensing units can still be manufactured or imported to service existing systems, but not for full system replacement. They also have to meet DOE efficiency standards and carry a “for servicing only” label. Some equipment must also be tested and listed by independent labs such as UL or ETL. 

Alex Ayers, HARDI’s vice president of government affairs, summed up the right move: “The right response is to stop and ask questions before putting the equipment into inventory.” The same advice works at the contractor level, just one step later in the chain. 

Where the R-410A Rules Stand Now 

Part of the confusion comes from rules that changed this year. In June, ACHR News explained the EPA’s final changes to the 2023 Technology Transitions Rule. The changes removed the Jan. 1, 2026, installation deadline for residential and light commercial AC and heat pump systems using refrigerants with a GWP above 700, and allow equipment manufactured or imported before Jan. 1, 2025, to be installed until that inventory is gone. 

The manufacture date matters. A unit built in 2025 or 2026 doesn’t get the same treatment as pre-2025 inventory, which is exactly why HARDI flagged new-build R-410A condensers marketed for new systems. For the service side of the equation, keeping existing R-410A systems running well, see The R-410A Service Window Contractors Can’t Afford to Waste. 

State rules can be tighter too. ACHR’s coverage of Washington’s HFC rules noted that starting Jan. 1, 2026, Washington prohibits refrigerants with a GWP above 750, including R-410A, in newly installed residential and nonresidential AC equipment. A state Ecology official said state law will supersede the federal extension. Contractors working in states with their own HFC rules need to check both levels. 

Unit What to Confirm 
R-410A, made before Jan. 1, 2025 Federal rule allows installation until inventory runs out; check state rules 
R-410A, made in 2025 or later For servicing existing systems only; must carry a “for servicing only” label and meet DOE standards 
A2L equipment (R-454B, R-32) Listed for A2L use by a recognized lab; certified in the DOE and AHRI databases 
Any unit claiming multiple refrigerant classes Treat as a red flag (see below) 

Six Red Flags to Check Before Buying or Installing 

Ayers laid out the warning signs in the Oct. 9 report. Here’s what to look for: 

  1. The manufacturer or model isn’t in the DOE database. No certification record is a stop sign. 
  1. The supplier can’t produce certification information. Legitimate sellers have it ready. 
  1. The model number doesn’t match the certification record. Close isn’t good enough. 
  1. An AHRI, UL, or Intertek ETL claim can’t be verified. Marks on a box or a spec sheet can be faked. 
  1. A newly made R-410A unit is marketed for a new system, or it’s missing the “for servicing only” label. 
  1. Seller claims about refrigerant, efficiency, or certification don’t match the records. 

One more that deserves its own line: a unit claimed to work with refrigerants in different safety classes. Ayers gave the example of a condenser advertised for “R-410A, R-32, and R-454B” and said that claim “violates the safety standard.” Equipment gets listed for a specific refrigerant safety class, so a do-everything claim doesn’t hold up. 

How to Verify in Five Minutes 

The Oct. 9 coverage listed the four places to check. Each takes a model number and a few minutes: 

  • DOE Compliance Certification Database for federal efficiency compliance 
  • AHRI Directory of Certified Product Performance for rated performance and matched systems 
  • UL Product iQ for UL listings 
  • Intertek ETL Listed Mark Directory for ETL listings 

The key detail: verify with the organization whose mark appears on the unit. A sticker isn’t proof. The database entry is. 

A good habit is to run the check against the nameplate before the unit goes on the truck, then photograph the nameplate for the job file. It protects the warranty conversation later, and it protects the company if the equipment’s legitimacy ever gets questioned. 

Sourcing Equipment That Checks Out 

The simplest protection is buying from established brands with records that line up. The air conditioner condenser and heat pump condenser categories list nameplate details like refrigerant and SEER2 right in the product titles, which makes the database check quick. Two R-454B examples: 

Even with a known brand, run the same check: model number against the DOE and AHRI records, and the listing mark against its own directory. Trust, then verify. 

Refrigerant claims deserve the same skepticism as equipment claims. The A/C and refrigeration analyzer lineup covers digital system analyzers for checking pressures and temperatures at startup against the manufacturer’s data. 

Reporting Suspicious Equipment 

HARDI runs an online form for reporting suspected non-compliant products. According to the Oct. 9 report, it asks for: 

  • Brand and seller names 
  • A link to the seller or product listing 
  • The model number 
  • The suspected compliance issue 

A nameplate photo and spec sheet aren’t required, but they help. HARDI reviews submissions and may forward likely violations to DOE or EPA for investigation. 

Frequently Asked Questions 

Can new R-410A condensing units still be sold? 

Newly manufactured or imported R-410A condensing units can be used to service existing systems, not for full system replacement, according to HARDI. They must meet DOE efficiency standards and carry a “for servicing only” label. 

Can pre-2025 R-410A equipment still be installed? 

Under the EPA’s revised Technology Transitions Rule, equipment manufactured or imported before Jan. 1, 2025, can be installed until that inventory runs out. Some states, such as Washington, have stricter rules. 

How can a contractor check if a unit is DOE compliant? 

Search the model number in the DOE Compliance Certification Database. The model number on the nameplate should match the certification record exactly. 

Is a UL or ETL sticker enough proof? 

No. Certification marks can be faked. Verify the listing in UL Product iQ or the Intertek ETL Listed Mark Directory. 

Can one condenser work with R-410A, R-32, and R-454B? 

HARDI says a unit claimed to work across refrigerant safety classes, such as A1 and A2L, violates the safety standard. Treat that claim as a red flag. 

What happens if non-compliant equipment gets installed? 

It can leave the contractor and the customer exposed on warranty and liability. Verifying before installation is far easier than sorting it out afterward. 

How do I report a suspicious HVAC product? 

Use HARDI’s online reporting form. It asks for the brand, seller, product link, model number, and suspected issue. HARDI may forward likely violations to DOE or EPA. 

Do state refrigerant rules override the federal changes? 

They can. Washington’s rules prohibit refrigerants above 750 GWP, including R-410A, in newly installed AC equipment as of Jan. 1, 2026, regardless of the federal extension. 

Check the Nameplate, Not the Pitch 

A too-good deal and a vague spec sheet aren’t a bargain. They’re a question. HARDI’s warning is a reminder that the database check takes five minutes and a bad install takes far longer to undo. Confirm the model in the DOE and AHRI records, verify listing marks at the source, know which R-410A units are for servicing only, and report anything that doesn’t add up. The best equipment story is the one where nothing interesting happens after the install.