Skip to main content
Tradesmen carrying an HVAC unit during installation

R-410A allowed a fair amount of margin for error. A duct run sized slightly small, a charge estimated by gauge feel rather than measured by scale, a coil paired with a condenser outside its rated combination: systems built on R-410A generally kept operating, simply at reduced performance. A2L equipment does not offer the same tolerance, and two articles published within days of each other in ACHR News illustrate the point clearly: practices that went largely unnoticed on R-410A systems are now surfacing as callbacks, failed startups, and voided warranties on R-454B and R-32 equipment.

The Rule Behind the Shift

The EPA’s Technology Transition Rule, part of the AIM Act, capped the global warming potential of refrigerant in newly manufactured residential and light-commercial equipment at 700 GWP starting January 1, 2025. In practice, that pushed the industry to R-454B and R-32, both classified as A2L: mildly flammable, lower toxicity. Pre-2025 R-410A equipment can still be installed while supply lasts, but new production has moved on.

A2L systems are built to UL 60335-2-40, which requires refrigerant detection and mitigation and ties allowable charge to room size, a single requirement that changes what belongs on a service truck, since A2L-rated recovery equipment and updated leak detection aren’t optional accessories anymore.

Three Practices That No Longer Hold Up

Contractor Paolo Weston, writing for ACHR News, identified three installation practices that once went largely unnoticed and no longer do:

  1. Undersized ductwork: higher-efficiency A2L equipment is less tolerant of the high static pressure that comes from ducts sized for an older, less efficient system. Airflow problems that used to just cost a few SEER points now show up as comfort complaints and short-cycling.
  2. Charging by gauge feel: factory charge only accounts for a standard line-set length. Topping off to a gauge reading instead of weighing in the correct charge for actual line length leaves the system under- or overcharged from day one.
  3. Unmatched components and undocumented startup: pairing coils and condensers outside their AHRI-certified combinations, skipping commissioning paperwork, or running crews without A2L-specific training can void a manufacturer warranty that only gets discovered years later, at the worst possible time.

Reading the Charge Right: the 70/70 Rule

A companion piece built on ACCA guidance and published the same week lays out the measurement side of the problem. Both coils need to reach at least 70 degrees Fahrenheit before a technician takes a reading, and the system should run for 15 to 20 minutes before any measurement is trusted, since a system barely started up hasn’t settled into a stable state yet.

Which number matters most, subcooling or superheat, depends on the metering device, and that distinction gets more important with A2L blends that exhibit refrigerant glide.

Metering Device Primary Measurement Why It Matters
TXV or EEV Subcooling The valve actively regulates superheat, so subcooling becomes the more reliable charge indicator.
Fixed orifice Superheat Without active regulation, superheat responds more predictably to charge level and outdoor conditions.

Verifying which type is installed before taking a single reading, rather than assuming, is worth the extra minute on every A2L call.

Equipment That Matches the Job

A few tools distinguish a properly executed A2L install from one likely to generate a callback:

FAQs

What refrigerants count as A2L?

R-454B and R-32 are the two most common A2L refrigerants replacing R-410A in new residential and light-commercial equipment.

Can R-410A equipment still be installed?

Existing R-410A equipment built before the cutoff can still be installed while supply lasts, but new manufacturing has shifted to refrigerants under the 700 GWP limit.

Why does duct sizing matter more with A2L equipment?

Higher-efficiency A2L systems are less tolerant of the high static pressure that comes from ductwork sized for an older, less efficient system, which shows up as comfort complaints and premature component wear.

Why can’t a tech just top off the charge to a gauge reading anymore?

Factory charge only covers a standard line-set length. Actual line length varies by install, so weighing in charge and verifying subcooling or superheat is the only reliable method.

How does a tech know whether to check subcooling or superheat?

It depends on the metering device. Systems with a TXV or EEV are read by subcooling, while fixed-orifice systems are read by superheat.

What is the 70/70 rule?

It’s a guideline to get both coils to at least 70 degrees Fahrenheit and let the system run 15 to 20 minutes before taking any charge measurement, so the reading reflects a stable, settled system.

What tools does an A2L-ready truck need?

A2L-rated recovery equipment, a refrigerant-rated leak detector, a digital scale, and a manifold with a micron gauge are the core additions beyond a standard R-410A tool set.

Can unmatched coil and condenser combinations really void a warranty?

Yes. Manufacturers certify specific AHRI-matched combinations, and installing outside those combinations, or skipping documented startup and commissioning, can void coverage that only gets discovered at a major failure years later.

Does A2L refrigerant require special safety precautions on site?

A2L refrigerants are mildly flammable, so systems built to UL 60335-2-40 include refrigerant detection and mitigation tied to room size, and techs should follow manufacturer handling guidance accordingly.

Is this shift affecting commercial equipment too?

The EPA rule and 700 GWP limit apply broadly across newly manufactured residential and light-commercial equipment, so the same charging and installation discipline applies on both fronts.

A Charge Worth Getting Right.

A2L equipment is not harder to install, it is simply less forgiving of the shortcuts R-410A once absorbed quietly. Weighing the charge, sizing the ducts for the equipment actually being installed, and confirming matched components on paper before the first startup addresses the issue directly.