A system can run every single day, cool the space, and still be quietly bleeding efficiency the entire time. ACHR News calls the phenomenon performance drift, and contractors interviewed for the story describe a problem that starts the moment a system is commissioned and never really stops. Component wear, sensor drift, and a string of well-intentioned thermostat adjustments accumulate slowly enough that nobody notices until the energy bill or the callback volume forces the issue. For technicians, the story is a reminder that a running system is not the same thing as a properly operating one, and that the gap between the two often hides in plain sight.
What Performance Drift Actually Is
Every piece of HVAC equipment moves away from its original commissioning parameters over time. Lee Harpham, director of refrigeration strategy at IMS Evolve, described the pattern as inevitable in complex commercial estates: systems gradually drift from the standard set when they were first balanced and started. Component wear, fluctuating refrigerant charge, sensor inaccuracies, and changing operating conditions all contribute, and the drift compounds because each small adjustment masks whatever caused it in the first place.
Brian Garry, field supervisor at Donnelly Mechanical in Queens, New York, put a number on how quickly it begins: drift starts almost immediately after startup. Environmental conditions, equipment cleanliness, and everyday operating changes all accelerate it from there. A thermostat bumped down two degrees to quiet a comfort complaint, left in place for months, becomes another small tax on run time and compressor cycling.
How Small Problems Compound
- Dirty filters restrict airflow, forcing the blower and compressor to work harder for the same output.
- Fouled evaporator and condenser coils reduce heat transfer, driving up head pressure and cutting system capacity.
- Aggressive thermostat setpoint changes made to solve an immediate complaint often stay in place long after the comfort issue passes.
- Sensor inaccuracies feed the control board bad data, so the system responds to conditions that no longer exist.
- Refrigerant charge that has drifted low or high changes superheat and subcooling readings without tripping an obvious fault.
Leonard Stupak, CEO of LA Construction, Heating and Air, described a case at a retail customer where a previous contractor installed inline duct fans to push air farther through the ductwork after a poor-airflow complaint. The fans never solved the problem because the real cause was a severely fouled indoor coil with an old filter lodged inside it, restricting airflow long before the air ever reached the fans. Cleaning the coil made the supplemental fans unnecessary. The story captures the core risk of performance drift: symptoms get treated while root causes stay in place, sometimes for years.
Traditional Maintenance vs Continuous Commissioning
| Approach | Detection Method | Timing | Best Suited For |
| Scheduled preventive maintenance | Visual inspection during a fixed-interval visit | Only catches drift present at the time of the visit | Standard residential and light commercial service agreements |
| Continuous commissioning | IoT sensors and AI models compared against baseline performance | Flags deviations in near real time between visits | Complex commercial estates, supermarkets, and multi-site refrigeration |
Continuous commissioning does not replace a technician’s judgment; it gives that judgment better data to work with. Harpham pointed to a North American retailer running 1,800 stores on continuous commissioning and automated health checks that improved reliability while cutting energy consumption. Stupak cited a Los Angeles Department of Water and Power Tune-Up Program project where filters were replaced, condenser coils cleaned, and refrigerant charges adjusted across more than 600 units, resulting in roughly 60 percent fewer summertime service calls at the property. Neither result required new equipment. Both came from catching drift before it became a failure.
Field Signs a Tech Can Catch on a Routine Call
- Amperage or pressure readings that run higher than the equipment’s rated specifications, even though the system still produces cooling or heating.
- Filters that show heavy loading well before the recommended replacement interval, suggesting the current schedule no longer matches actual conditions.
- Recurring temperature complaints or nuisance alarms tied to the same zone or unit.
- Supplemental equipment, like inline duct fans or portable units, added to a space that should not need them if the primary system were performing correctly.
- A noticeable gap between rated capacity and the airflow or temperature split actually measured at the register.
A Practical Filter and Coil Maintenance Routine
- Check filter condition at every service call regardless of the posted replacement schedule, since actual loading often outruns the calendar.
- Inspect evaporator and condenser coils for visible fouling, and clean proactively rather than waiting for a capacity complaint.
- Record amperage, pressure, and temperature-split readings at each visit to build a baseline for comparison over time.
- Investigate any supplemental equipment already on site as a possible symptom of an unresolved airflow or capacity issue.
- Verify refrigerant charge against target superheat and subcooling rather than relying on pressure alone.
- Flag any zone with repeat service calls for a root-cause review instead of another symptom fix.
Tools and Products That Help Catch Drift Early
Coil condition drives a large share of performance drift, and a properly cleaned coil restores capacity fast. For evaporator coils, Nu-Calgon’s Evap Pow’r-C no-rinse cleaner handles routine buildup without pulling the coil, while heavier grease and grime on condensers responds well to Refrigeration Technologies’ Viper Heavy Duty coil cleaner and degreaser. For techs cleaning coils on a regular route, the SpeedClean CoilJet CJ-125 portable coil cleaning system speeds up rooftop and remote-unit cleaning without dragging a pressure washer around, and a Supco coil cleaning brush clears out matted debris that a spray alone will not lift.
Catching charge drift depends on accurate diagnostics, and a digital manifold pays for itself the first time it flags a problem a mechanical gauge would have missed. The Fieldpiece SM382V 3-port SMAN digital manifold with built-in micron gauge calculates superheat and subcooling live during a charge check, and the Navac NX4V NEXUS digital manifold kit with Bluetooth connectivity adds wireless temperature clamps and app-based logging for techs building a baseline record across visits. On the filter side, SupplyHouse.com’s replacement filters category covers sizing across MERV ratings, and a stock item like the Honeywell Home 17.5″ x 27″ x 5″ MERV 10 filter keeps a common deep-pleat size on the truck for same-visit swaps.
Frequently Asked Questions
What is HVAC performance drift?
Performance drift describes the gradual movement of a system away from its original commissioning parameters, driven by component wear, sensor inaccuracy, fouling, and accumulated setpoint adjustments.
When does performance drift start?
According to field supervisors interviewed by ACHR News, drift begins almost immediately after initial startup and continues at a rate influenced by environmental conditions and equipment cleanliness.
How is performance drift different from a system failure?
A failure produces an obvious fault or shutdown. Drift develops gradually without triggering an alarm, so the system keeps running while operating further and further from its design parameters.
What is continuous commissioning?
Continuous commissioning compares real-time operating data against expected performance using IoT sensors and, increasingly, AI models trained on HVAC and refrigeration behavior, catching deviations between scheduled maintenance visits.
Can performance drift be fixed without new equipment?
Often yes. Cited examples include filter replacement, coil cleaning, and refrigerant charge correction restoring significant efficiency without any equipment replacement.
How much efficiency can drift cost over time?
Contractors interviewed for the ACHR News report cited efficiency losses in the range of 10 to 40 percent once maintenance issues accumulate, though the exact figure depends on the system and how long drift goes unaddressed.
Does a clean filter schedule prevent performance drift entirely?
No single task prevents drift completely, since coil condition, refrigerant charge, and sensor accuracy all contribute independently. A consistent filter schedule addresses one major contributor but not all of them.
Why do traditional maintenance programs sometimes miss drift?
Scheduled programs are built around fixed inspection intervals and fault response, so subtle changes that develop between visits can go unnoticed until they become significant enough to trigger a complaint or a spike in energy costs.
Is continuous commissioning only for large commercial accounts?
Most current applications are commercial, particularly in supermarkets and multi-site refrigeration, where the energy stakes justify sensor investment. Residential contractors can apply the same root-cause mindset during routine visits without the sensor infrastructure.
What is the fastest way to check for drift on a service call?
Comparing current amperage, pressure, and temperature-split readings against the equipment’s rated specifications and any prior visit’s baseline data gives a quick read on whether a system has moved away from its design parameters.
Staying Cool Under the Right Pressure
Performance drift never announces itself. It shows up in an energy bill, a repeat service call, or a customer who assumes the system is fine because it is still blowing air. The fix rarely requires new equipment. It requires treating symptoms as clues rather than the whole story, checking amperage and pressure against spec on every visit, and cleaning coils before a capacity complaint forces the issue. A system running as designed costs less to operate and calls the shop back less often, which is a better outcome for everyone on the invoice.