Every electrician who has slapped a generic arc flash sticker on a panel and moved on is about to have a harder time getting away with it. The 2026 National Electrical Code rewrote Section 110.16 from the ground up, expanding which equipment needs a label, spelling out exactly what information belongs on it, and renumbering huge sections of the code in the process. States are adopting the 2026 edition at different speeds, but the direction is clear, and contractors who get ahead of it now avoid scrambling later.
Why Section 110.16 Got a Rewrite
The 2023 NEC limited arc flash hazard warning requirements to service and feeder equipment rated 1,000 amps or higher in buildings other than dwellings. The 2026 edition removes that threshold entirely. Service and feeder equipment such as switchboards, enclosed panelboards, switchgear, industrial control panels, and motor control centers all now require a permanent arc flash hazard marking, regardless of amperage, in anything other than a dwelling unit.
The section title itself changed too, moving from a general “warning” requirement to a more specific “Arc-Flash Hazard Marking” standard, a small wording shift that signals a much bigger change in scope.
What the Label Actually Needs Now
- The nominal system voltage
- The arc flash boundary
- Either the available incident energy or the minimum required level of personal protective equipment
- The date the arc flash assessment was completed, not the date the label got applied
2023 NEC vs. 2026 NEC: Arc Flash Marking
| Requirement | 2023 NEC | 2026 NEC |
| Equipment covered | Service/feeder equipment rated 1,000A or higher | All service and feeder equipment, regardless of amperage |
| Label date required | Date label applied | Date assessment completed |
| Content detail | General reference to industry practice | Specific voltage, boundary, incident energy, or PPE level spelled out |
| Handwritten labels | Generally accepted | No longer permitted; label must be permanently affixed per Sec. 110.21(B) |
That date change matters more than it looks. NFPA 70E requires arc flash studies to get reviewed at least every five years, and putting the assessment date on the label instead of the install date gives everyone, including the next electrician on the job, a real way to track when that clock started.
The Renumbering Nobody Can Ignore
Beyond arc flash, the 2026 NEC restructured the entire code from nine chapters to twenty, a change meant to prep the document for further restructuring in the 2029 edition. Load calculations moved from Article 220 to Article 120. Energy management systems moved from Article 750 to Article 130. Fire-resistive cable systems shifted from Article 728 to Article 772. Anyone still citing the old article numbers on a design document or spec sheet risks confusing an inspector or delaying a plan review, even when the underlying technical requirement hasn’t changed at all.
Getting Panels Inspection-Ready
- Walk existing panelboards and switchboards to identify anything currently missing an arc flash label, not just equipment rated 1,000 amps or higher.
- Schedule or update arc flash studies on any equipment where the assessment date is missing, unclear, or older than five years.
- Replace handwritten or improvised labels with permanent markings that include voltage, boundary, incident energy or PPE level, and assessment date.
- Update design documents, submittals, and internal references to reflect the new article numbers before the next permit application.
- Confirm with the local authority having jurisdiction which edition of the NEC is currently enforced, since adoption timelines vary by state.
On the Truck for Compliance Checks
- A reliable clamp meter, such as the Klein Tools CL800 or CL390, for verifying voltage and current before opening a panel
- A non-contact voltage tester like the Klein Tools NCVT-3PR for a fast first pass before deeper testing
- Panel and breaker stock on hand for upgrades, browsable through the Load Centers and Breaker Boxes categories
- A documentation folder or tablet loaded with the most recent arc flash study for equipment on the route
- A dedicated punch list for renumbered article references on any active design sets
Frequently Asked Questions
Does the 2026 NEC apply immediately in every state?
No. Adoption depends on the state and local jurisdiction, and some areas take years to formally enforce a new NEC edition or adopt it with amendments.
Do dwelling units need arc flash labels under the 2026 NEC?
Generally, no. The expanded labeling requirement applies to service and feeder equipment in buildings other than dwelling units, following the same carve-out that existed in the 2023 edition.
Can a sub-panel be handled the same as service equipment for labeling purposes?
It depends on how the sub-panel is fed. A sub-panel supplied downstream of a meter main or distribution panel may not automatically qualify as “service and feeder equipment,” so checking with the local authority having jurisdiction is the safer move.
What method calculates the arc flash boundary and incident energy for a label?
IEEE 1584-2018 is the most widely used method, and NFPA 70E Table 130.7(C)(15)(a) also provides reference tables for determining PPE categories.
Is a handwritten arc flash label still acceptable anywhere in the 2026 NEC?
No. The 2026 edition requires labels to be permanently affixed per Section 110.21(B), which rules out handwritten markings.
How often does an arc flash study need updating under NFPA 70E?
At minimum every five years, and sooner if the electrical system changes in a way that affects available fault current or equipment ratings.
Does the article renumbering change any technical requirements?
Mostly no. Sections like load calculations moved to new article numbers, but the underlying technical content stayed largely consistent. The risk lies in outdated references confusing plan reviews, not in the substance changing.
Do arc flash labels need to reference NFPA 70E directly?
The 2026 NEC language aligns closely with NFPA 70E content requirements without explicitly citing the standard on every label, so the information itself, not a citation, is what matters.
Will every small disconnect switch need a full arc flash label now?
That’s still being worked out in practice. The code doesn’t specifically exclude smaller equipment, so coordinating with the local authority having jurisdiction on borderline cases is the safest approach until more guidance emerges.
Does a panel upgrade trigger a new arc flash study automatically?
Any change that affects available fault current, such as a service upgrade or new equipment, generally calls for a fresh study rather than relying on the prior assessment.
Don’t Get Grounded by Outdated Labels
Arc flash labeling has been evolving for roughly twenty five years, and the 2026 NEC pushes it further toward the data-driven standard NFPA 70E always intended. Electricians who audit their panels now, update the paperwork, and swap handwritten stickers for real assessments won’t just pass the next inspection. They’ll keep the crew working on equipment where everyone actually knows what they’re walking up to.