Skip to main content
An electrician changes a circuit breaker in an electrical panel

A breaker that trips repeatedly, fails to reset, runs warm to the touch, or carries the faint smell of burned plastic isn’t just an inconvenience. It’s communicating something. The device has either reached the end of its service life or it’s no longer sized correctly for the load it protects. Either way, another reset isn’t the answer. A replacement is. For licensed electricians, this is a straightforward panel task. Done correctly, with power verified off and the right part in hand, a single-pole swap typically takes under 30 minutes. A double-pole runs a bit longer. Here’s how to do it right. 

Important:Circuit breaker replacement involves working inside a panel with energized components. The main breaker cuts power to branch circuit bus bars, but utility-side service entrance lugs remain live at all times. Verify circuit power is off with a non-contact voltage tester before touching any wiring. If work will be performed within close proximity of the service entrance lugs, contact the utility to pull the meter before proceeding. All work must comply with the locally adopted edition of the NEC and applicable local amendments. 

When a Breaker Actually Needs Replacing 

Not every trip calls for a new breaker. But these symptoms make replacement the correct call: 

  • Won’t reset or hold: The handle moves to ON but springs back to the tripped position. The internal mechanism is fatigued or the bimetal strip has deformed. 
  • Trips well below rated load: A 20A breaker tripping consistently on a 10A circuit with no fault present has lost calibration. 
  • Physical damage: Burn marks, cracked housing, or heat discoloration at the terminal. Carbon tracking cannot be fixed by resetting. 
  • Protection upgrade required: Standard breaker in a location now requiring AFCI or GFCI protection under the locally adopted NEC. See the section below. 
  • Panel upgrade or circuit addition: Adding a new circuit or replacing a breaker from a discontinued brand using a classified replacement. 

Know the Breaker Family Before Ordering Anything 

The most common mistake on a breaker swap is ordering the wrong part. Breakers are panel-specific. An Eaton BR breaker does not fit a Square D QO panel. Before ordering, open the panel door and read the label. It identifies the manufacturer, panel series, and lists the approved breaker part numbers for that enclosure. 

Panel Brand Breaker Series Notes 
Square D QO Series Plug-on; Visi-Trip indicator; 10 kAIC standard interrupt rating 
Square D Homeline Series Plug-on neutral available for AFCI/GFCI types; economical residential line 
Eaton BR Series 1-inch width; pigtail neutral required for AFCI and GFCI types 
Eaton CH Series Larger residential and light commercial panels 
Siemens / Murray QP Series Compatible with Siemens, Murray, and select ITE panels; verify label 
Classified Replacement Various (DiversiTech, etc.) UL-classified to fit multiple panel brands; verify the compatibility label on the package 

For panels where the original breaker brand is discontinued, UL-classified replacement breakers provide a code-compliant alternative. Always confirm the classified listing covers the specific panel in question. 

AFCI and GFCI Requirements: What the 2023 NEC Requires 

A straight standard-for-standard breaker swap may leave a circuit non-compliant if the location now requires arc-fault or ground-fault protection under the jurisdiction’s adopted NEC edition. Verify requirements before ordering a replacement. 

AFCI: NEC 2023 Section 210.12(B) 

Section 210.12(B) of the 2023 NEC requires combination-type AFCI protection for all 120-volt, single-phase, 10A, 15A, and 20A branch circuits supplying outlets or devices in dwelling units in the following locations: kitchens, family rooms, dining rooms, living rooms, parlors, libraries, dens, bedrooms, sunrooms, recreation rooms, closets, hallways, laundry areas, and similar rooms and areas including finished basements. 

When an existing branch circuit in one of these locations is modified, replaced, or extended, Section 210.12(D) requires AFCI protection to be installed. The only exception: extensions not exceeding 6 feet that add no new outlets or devices. 

Jurisdiction note: The NEC is a model code. The edition currently enforced varies by jurisdiction. Verify the locally adopted NEC edition through the AHJ before specifying protection type. 

GFCI: NEC 2023 Section 210.8(A) 

Section 210.8(A) of the 2023 NEC requires GFCI protection for receptacles rated 125 volts through 250 volts, supplied by single-phase branch circuits rated 150 volts or less to ground, in dwelling unit locations including: bathrooms, garages, outdoors, crawlspaces, all portions of basements (finished or unfinished), kitchens (all receptacles, not limited to countertop service), laundry areas, sinks within 6 feet of the bowl, and areas with sinks and permanent provisions for food or beverage preparation or cooking. 

The 2023 NEC notably removed the phrase ‘where installed to serve countertop surfaces’ from kitchen requirements. GFCI protection is now required for all dwelling unit kitchen receptacles. 

Protection Type Applicable NEC 2023 Section Where Required in Dwelling Units 
Combination-type AFCI 210.12(B), 210.12(D) Kitchens, bedrooms, living areas, hallways, laundry, closets, finished basements, and similar rooms on 120V 10/15/20A circuits 
GFCI (Class A, 5mA) 210.8(A) Bathrooms, garages, outdoors, all basements, kitchens, laundry, sinks, and similar wet/damp locations; 125V-250V receptacles on single-phase circuits ≤150V to ground 
Dual Function (AFCI+GFCI) 210.12 + 210.8 Where both requirements overlap (kitchens, laundry areas, finished basements with wet locations) 
Standard Thermal-Magnetic N/A (no upgrade trigger) 240V appliance circuits, locations not listed in 210.12(B) or 210.8(A), service panels 

Browse Eaton BR AFCI/GFCI dual-function breakers (SKU: BRN115DF) for areas requiring both protections in BR panels. For Square D Homeline panels, the HOM120PCAFI plug-on neutral AFCI breaker connects directly to the neutral bar and eliminates the pigtail, reducing panel clutter. 

Tools and Materials 

  • Non-contact voltage tester, verified working before panel entry 
  • Flathead and Phillips screwdrivers 
  • Insulated needle-nose pliers 
  • Calibrated torque screwdriver or torque tool (required per NEC 110.14(D) when a numeric torque value is listed on the equipment or installation instructions) 
  • Multimeter 
  • Arc-rated PPE: safety glasses, arc flash-rated gloves, face shield for any live-panel proximity work 
  • Replacement breaker (correct panel series, pole count, amperage, protection type) 
  • Permanent marker or panel directory label for circuit documentation 

Step-by-Step: Replacing a Standard Single-Pole Breaker 

Step 1: Identify and Prepare the Circuit 

  1. Open the panel cover door and locate the circuit directory. 
  1. Identify the breaker to be replaced by label and physical position in the panel. 
  1. Turn the target breaker to OFF. If the handle won’t move cleanly to OFF, move it to the tripped center position first. 
  1. At the circuit location, confirm all devices are off or unplugged. Use the non-contact voltage tester at a nearby outlet to confirm no voltage is present. 

Step 2: De-Energize and Verify 

  1. Locate the main breaker inside the panel and flip it to OFF. On a standard residential panel, this removes power from both bus bars feeding the branch circuits. 
  1. Critical: The service entrance lugs at the top of the panel remain energized even with the main breaker off. Do not contact these lugs or any conductors connected directly to them. If work requires access near the service entrance, contact the utility to pull the meter first. 
  1. After switching the main breaker OFF, test both bus bars with the non-contact voltage tester. Both should read no voltage. If either bar reads live, stop immediately and contact the utility. 
  1. Stand on an insulated mat. Wear arc-rated PPE for all panel work. 

Step 3: Remove the Old Breaker 

  1. Remove the panel cover screws and set the cover aside safely. 
  1. Locate the circuit conductor connected to the breaker terminal. On a single-pole breaker, this is typically one black (hot) conductor. On a double-pole, there are two hots. 
  1. Loosen the terminal screw and remove the conductor. Note the wire gauge; it determines whether the replacement amperage is appropriate for the circuit. 
  1. Plug-on breaker: Grip the outer edge of the breaker firmly and rock it outward away from the bus stab. The breaker clip releases with moderate pressure. 
  1. Bolt-on breaker: Remove the mounting screws first, then pull the breaker free from the bus. 
  1. Remove the old breaker completely. Inspect the bus stab for damage, corrosion, or carbon tracking. 

Step 4: Install the Replacement Breaker 

  1. Confirm the replacement is the correct series, pole count, amperage, and protection type for the panel and circuit. 
  1. Plug-on breaker: Align the clip with the bus stab and press firmly until the breaker snaps fully into position. A loose fit is not acceptable. 
  1. Bolt-on breaker: Seat the breaker fully and torque the mounting screws per the manufacturer’s specification. 
  1. AFCI/GFCI with pigtail neutral: Connect the white pigtail to an open terminal on the neutral bar. The pigtail connects to the neutral bar, not to the load-side neutral wire. The circuit’s neutral wire connects to the breaker’s neutral terminal. 
  1. Plug-on neutral AFCI/GFCI: Align the neutral clip to the neutral bar slot and press firmly into position. No pigtail is used. 
  1. Terminal torque (NEC 110.14(D)): Connect the circuit conductor to the breaker terminal and torque the terminal screw to the value stamped on the breaker face or listed in the manufacturer’s installation instructions. NEC 110.14(D) requires the use of an approved torque tool when a numeric value is specified. Torque values vary by manufacturer and wire size; always use the value marked on the specific breaker being installed, not a generic reference value. 

Step 5: Verify and Restore Power 

  1. Inspect all connections inside the panel. No conductor strands should be visible outside any terminal. 
  1. Reinstall the panel cover and tighten all cover screws. 
  1. Restore main breaker power. 
  1. Switch the new breaker to ON. 
  1. AFCI breaker test: Press the TEST button on the breaker face. The breaker should trip to the middle or off position. Reset to ON to confirm correct operation. 
  1. GFCI breaker test: Press TEST and verify no voltage at the load. Press RESET and verify voltage is restored at the load. 
  1. Test the circuit under normal load and confirm the breaker holds. 
  1. Update the panel directory to reflect the circuit and any protection type changes. 

Wire Sizing Reference 

The replacement breaker must be rated to protect the conductor size on the circuit. A higher-amperage breaker on undersized wire removes overcurrent protection. Confirm wire gauge before ordering. 

Circuit Amperage Minimum Copper Wire Gauge Common Applications 
15A 14 AWG General lighting and receptacle circuits 
20A 12 AWG Kitchen small-appliance circuits, bathrooms, bedrooms 
30A 10 AWG Dryers, water heaters, HVAC disconnect circuits 
40A 8 AWG Electric ranges, larger HVAC equipment 
50A 6 AWG EV chargers, large appliance loads 

Product Reference at SupplyHouse 

Shop the full circuit breaker category at SupplyHouse. For Eaton BR panels, browse Eaton BR Series breakers, including the BRN120AF 20A AFCI (SKU: BRN120AF) and the BRN115DF 15A dual-function AFCI/GFCI (SKU: BRN115DF). For Square D panels, shop QO Series and Homeline Series, including the HOM120PCAFI plug-on neutral AFCI (SKU: HOM120PCAFI). When the original panel brand is no longer available, browse classified replacement breakers for UL-listed cross-compatibility. For full panel replacements or subpanel additions, see breaker boxes and load centers. 

Common Mistakes to Avoid 

  • Wrong breaker family: Mixing brands without checking classified compatibility. A breaker that almost fits is not a fit. 
  • Skipping the torque requirement: NEC 110.14(D) requires a torque tool when a numeric value is listed on the equipment. Loose terminals arc, generate heat, and fail. 
  • Ignoring AFCI/GFCI upgrade triggers: A direct standard-for-standard swap in a location covered by NEC 210.12(B) or 210.8(A) leaves the circuit non-compliant when the work is permitted and inspected. 
  • Misconnecting the neutral pigtail: On AFCI and GFCI breakers with pigtails, the white pigtail goes to the neutral bar. The circuit neutral wire connects to the breaker’s neutral terminal. Reversing these connections prevents the protective function from operating. 
  • Assuming the main breaker de-energizes the full panel: It does not. Service entrance lugs stay live at all times. Keep hands clear of the top section of the panel. 
  • Using aluminum conductors with CU-only terminals: Breakers marked CU-only are not listed for aluminum wiring. Use terminals marked AL/CU with aluminum conductors, and apply anti-oxidant compound. 

Frequently Asked Questions 

Can a homeowner replace a circuit breaker? 

Most jurisdictions permit homeowners to pull a permit and perform their own electrical work, but the work must pass inspection and comply with the locally adopted NEC. Given the live service entrance conductors present in every residential panel, homeowners without electrical training should hire a licensed electrician for panel work. 

How do I know if the panel accepts classified replacement breakers? 

Check the panel label inside the door for the list of approved breakers. Classified replacement breakers also carry a panel compatibility chart on the product packaging. The chart lists the panel brands and series for which the device holds a UL classified listing. 

Does replacing a breaker reset its mechanical life? 

Yes, a new breaker has a fresh mechanical service life. But if the circuit has an underlying fault causing repeated trips, the new breaker will trip on the same fault. Diagnosing the cause before assuming the breaker was the problem is the correct approach. 

What does it mean when a breaker trips immediately on reset? 

An immediate trip on reset typically indicates a hard fault: a short circuit, a ground fault, or a heavily overloaded circuit. The fault must be located and cleared before the breaker will hold. 

Can a 15A breaker be replaced with a 20A to stop nuisance trips? 

Only if the circuit conductor is 12 AWG copper or larger. Installing a 20A breaker on 14 AWG wire removes the overcurrent protection the conductor depends on and creates a fire hazard. The correct fix is to reduce the circuit load or rewire the circuit with appropriately sized conductors. 

What is a tandem breaker and where can it be installed? 

A tandem breaker, sometimes called a double-stuff or slimline, places two single-pole circuits in one panel space. Not every panel space accepts a tandem; the panel label or directory identifies approved tandem positions. Installing a tandem in an unapproved slot is a code violation. 

Do AFCI breakers require a neutral conductor at the panel? 

Most do. AFCI breakers require either a pigtail that connects to the neutral bar or a plug-on neutral design that clips directly onto the bar. Standard thermal-magnetic breakers do not use a neutral connection at the panel. 

What NEC section governs torque requirements for breaker terminals? 

NEC 110.14(D) requires that tightening torque values for terminal connections match the values specified on the equipment or in the manufacturer’s installation instructions, and that an approved torque tool be used to achieve that value. Torque values for a specific breaker are typically stamped on the breaker face or listed in the installation sheet. 

Can a higher interrupt-rated breaker replace a lower-rated one of the same amperage? 

Yes, as long as the replacement is the same amperage, pole count, and panel-compatible series. A breaker with a higher AIC (ampere interrupting capacity) rating provides better fault clearing performance and is always the safer direction when upgrading within the same panel family. 

What is required for circuits with aluminum conductors? 

Breaker terminals used with aluminum conductors must be rated AL/CU. Terminals marked CU-only are not listed for aluminum wiring. Aluminum wiring also requires anti-oxidant compound at the terminal to prevent corrosion-related resistance at the connection point. 

Back on the Circuit  

A breaker replacement done correctly takes under 30 minutes and delivers reliable overcurrent protection for the life of the panel. Done incorrectly, it creates a latent problem that shows up months later as a failed inspection, a nuisance trip, or a damaged connection. 

Match the replacement to the panel series. Confirm the wire gauge supports the breaker amperage. Check NEC 210.12(B) and 210.8(A) requirements for the circuit location before defaulting to a standard breaker. Torque the terminal to the value marked on the device. Test every protective function before closing the panel. 

The work behind the cover door sets the standard for everything downstream on that circuit. Get it right, document it, and move on. 

SupplyHouse stocks Eaton BR, Square D QO, Square D Homeline, and classified replacements for discontinued panel brands, all with fast nationwide shipping. 

Shop All Circuit Breakers   |   Eaton BR Breakers   |   Square D QO Breakers   |   Square D Homeline Breakers   |   Classified Replacement Breakers