What Is Bluefin?
Bluefin offers dependable, job-ready parts for plumbing, hydronic heating, HVAC, and electrical repair.
Bluefin carries the breadth and depth of inventory tradespeople rely on. When it is needed on the job, Bluefin has it, and it works.
Bluefin is available exclusively at SupplyHouse.com and backed by SupplyHouse’s service and support.
“I’ve used 100′ and 300′ rolls of 1/2 Pex-b from big box stores and I can say the SupplyHouse Bluefin has superior surface finish quality. Box store material is dull and matte which is often very hard to pull through walls and other areas we install radiant heat lines. Bluefin has a gloss finish surface and it pulls like a dream, even for Pex-b”
Mark G., West Michigan
Bluefin FAQs
What kinds of parts does Bluefin cover?
Core Bluefin categories include PEX tubing, press fittings and valves, circulator pumps, zone valves, radiant manifolds, expansion tanks, common HVAC electrical parts, and ductless mini-split systems. These categories reflect the parts used most often on installs and service calls.
Is Bluefin suitable for residential and commercial jobs?
Yes. Bluefin covers core plumbing, hydronic heating, HVAC, and electrical components used in both residential and light commercial applications. Product categories such as oxygen barrier PEX, press fittings, circulator pumps, zone valves, expansion tanks, and mini-split systems are commonly used across home installs, multifamily projects, and light commercial work.
Always confirm system specifications, local code requirements, and load sizing before ordering for commercial applications.
Is Bluefin suitable for hydronic systems?
Yes. Bluefin oxygen barrier PEX and hydronic components are built for closed-loop systems where oxygen control, circulation, and pressure management matter. Use oxygen barrier PEX in systems with ferrous components to limit corrosion.
Are Bluefin press fittings a practical alternative to soldering?
Press fittings speed installation and remove open flame from many jobs. Confirm press profile and jaw compatibility before ordering, as press systems are profile-specific.
What should be checked before buying a Bluefin mini-split?
Confirm refrigerant type, BTU capacity, efficiency rating, and which accessories are included with the SKU. Some packages require separate purchase of line sets and communication wire.
Before selecting a system, size it for the space using SupplyHouse’s Mini-Split Calculator:
- Mini-Split Calculator for ductless-specific sizing guidance:
https://www.supplyhouse.com/sh/control/MiniSplitCalculator
For additional sizing and HVAC calculators:
https://www.supplyhouse.com/resources/calculators
Sizing errors are one of the most common reasons systems run short of comfort or waste energy. Using the calculators before ordering helps match the BTU output and system type to the space.
Where can Bluefin products be purchased?
Bluefin is available exclusively at SupplyHouse.com. Browse the full Bluefin lineup at: https://www.supplyhouse.com/Bluefin
What Bluefin Offers
See below for a short, linked inventory that points to category and product pages, making it quick and straightforward to check dimensions, materials, and compatibility before ordering.
Bluefin PEX and Radiant Heating
Oxygen barrier PEX for closed-loop hydronic systems helps limit oxygen intrusion in systems with pumps, boilers, and valves. Bluefin also supplies plumbing PEX and full radiant accessories.
- Bluefin Oxygen Barrier PEX
https://www.supplyhouse.com/Bluefin-Oxygen-Barrier-PEX-Tubing-26044000 - Plumbing PEX
https://www.supplyhouse.com/Bluefin-PEX-Plumbing-Tubing-11916000 - Radiant heat supplies
https://www.supplyhouse.com/Radiant-Heat-297000
Bluefin Press Fittings and Valves
Press technology reduces install time and removes open flame from many applications. Bluefin offers PEX press fittings, imported copper press fittings, and press ball valves. Confirm pipe material, press profile, and jaw compatibility before ordering.
- PEX press fittings: https://www.supplyhouse.com/Bluefin-PEX-Press-Fittings-29543000
Bluefin Hydronic Heating Components
Bluefin supports complete hydronic builds with circulator pumps, zone valves, radiant manifolds, and expansion tanks. Components are selected to support circulation, zoning, pressure control, and oxygen management.
- Pumps: https://www.supplyhouse.com/Bluefin-Pumps-34292000
- Zone valves: https://www.supplyhouse.com/Bluefin-Zone-Valves-34096000
- Manifolds: https://www.supplyhouse.com/Bluefin-Radiant-Heat-Manifolds-13310000
- Expansion tanks: https://www.supplyhouse.com/Bluefin-Hydronic-Heating-Expansion-Tanks-32510000
Bluefin HVAC Electrical Parts
Bluefin covers the small electrical components that often determine whether a service call is a quick fix or a multi-hour job. The range includes contactors, motor run capacitors, A/C disconnects, and other common parts. Verify voltage, amperage rating, and pole count before replacing a part.
- Contactors: https://www.supplyhouse.com/Bluefin-Contactors-39960000
- Motor run capacitors: https://www.supplyhouse.com/Bluefin-Motor-Run-Capacitors-36361000
Bluefin Mini-Split Systems
Bluefin offers ductless mini-split heat pump systems for installs that demand ductless solutions. Single-zone and multi-zone systems are available, along with indoor and outdoor units and replacement parts. Verify refrigerant and capacity at the SKU level and check included accessories before ordering.
- Mini-split systems: https://www.supplyhouse.com/Bluefin-Mini-Split-Systems-36580000
Bluefin YouTube Videos
Bluefin press fittings save time and remove open flame. A SupplyHouse technician says, “Press fittings allow for fast, consistent connections without soldering.” Watch the press fitting demo for jaw and profile guidance:
Bluefin PEX tubing supports plumbing and hydronic installs, including radiant heating applications. The video walks through BlueFin PEX tubing and what to look for when choosing tubing for the job.
Bluefin and SupplyHouse
Bluefin keeps core parts predictable and job-ready. Every Bluefin SKU is manufactured to practical specs and backed by SupplyHouse’s distribution and specification network, so availability and SKU details remain consistent on the jobsite. Bluefin is available exclusively at SupplyHouse.com, giving contractors, trade professionals, and DIYers one place for repeatable parts, clear SKU information, and predictable reorders. When speed, compatibility, and reliable stock matter, Bluefin does the work.
Explore the full Bluefin lineup: https://www.supplyhouse.com/Bluefin