From hot showers to sparkling clean dishes, water heaters are key to keeping a happy home. The U.S. Department of Energy pegs water heating at 18 % of an average household utility bill¹, so replacing a failing tank promptly can reduce annual costs and avoid emergency service calls.
But swapping a water heater isn’t a casual job. You’re dealing with electricity, gas, and up to 120 psi of pressure—all in one system. One misstep, and you’re looking at leaks, shorts, or worse. That’s why we pulled together this step-by-step plan.
¹ Source: Energy Information Administration, Residential Energy Consumption Survey 2020.
Table of Contents
1. Tools, Materials & Safety Gear
4. Pro Maintenance & Troubleshooting
5. How to Maximize Water-Heater Lifespan
6. Wrap-Up
Tools, Materials, and Safety Gear
Every installer’s toolkit involves five columns:
- Tools
Reusable hand- and power-tools carried back to the truck when the job is done.
- Selection Notes
Tips for choosing rugged, job-site-ready versions of each tool.
- Materials
Consumable components (plumbing, electrical, and safety parts) that remain with the installation.
- Usage Tips
Field-tested pointers on how to apply or orient each material for leak-free, code-compliant results.
- PPE
Personal protective equipment that guards hands, eyes, lungs, and hearing while using tools and materials.
| Tools | Selection Notes | Materials | Usage Tips | PPE |
| Adjustable and pipe wrenches | Drop-forged steel, slip-resistant grips | New water heater | Pick capacity (40–50 gal) to match demand | Cut-resistant gloves |
| Flat and Phillips screwdrivers | Magnetic tips for faster handling | Flexible water-heater connectors | Braided stainless resists corrosion | Safety goggles |
| Tubing cutter and hacksaw | Sharp, replaceable blades | Dielectric unions & nipples | Brass unions with EPDM gaskets last longer | Gloves + goggles |
| Tape measure and 24″ level | Laser-etched markings | Drain pan | Polyethylene pans resist cracking | Work gloves |
| Multimeter & voltage tester | True-RMS recommended | Expansion tank | Pre-charge to static pressure (40–60 psi) | Class 00 insulated gloves |
| Propane torch & solder kit | Includes solder and flux, plus a compatible propane torch | Temperature & pressure relief valve | Install full-port, spring-loaded valve | Fire-resistant gloves, face shield |
| Garden hose & bucket | Heavy-duty, kink-resistant | Anode rod (future maintenance) | Magnesium core for corrosion protection | Nitrile gloves |
| Shop-vac | Wet/dry capable for sediment cleanup | Stands & seismic straps | Space straps per local seismic code | Dust mask, hearing protection |
Skipping a dielectric union invites galvanic corrosion and can halve tank life. Checklist once, cry never.
Safety & Legal Must-Knows
Professional installations begin with risk assessment and code compliance:
- Permitting (1–2 days)
- Plumbing permit for water/drain changes
- Electrical permit for circuit modifications
- Gas permit for flex-line and vent work
- Requirements vary by jurisdiction
- Liability & Insurance
- Confirm homeowner policy allows owner-performed plumbing/electrical
- Unpermitted work can void coverage and complicate resale
- Key Codes
- IPC §507: Water-heater installations
- NEC Art 210: Branch-circuit requirements
- IFGC Ch 5: Gas-venting specifications
- Pressure & Temperature
- T&P valves open at 150 psi, discharge 210 °F water
- Discharge piping must end ≤ 6″ above a safe drain or pan
- Thermal Expansion
- Closed systems require an expansion tank
- Pre-charge to match static water pressure (40–60 psi)
- Seismic Safety
- Strap tanks per local ordinance with approved straps
Having a licensed professional review the plan is a small investment compared to the headache of unplanned failure.
Step-By-Step Installation
Phase 1: Decommission and Site Prep (1–1.5 hours)
1. Kill utilities
- Electric: switch off the 240 V breaker; lock/tag out; confirm zero V with meter
- Gas: turn control knob off; close upstream valve
2. Drain the old tank
- Attach hose to drain valve; route to safe drain or outdoors
- Open T&P valve and faucet to vent air
- Wait until flow stops
3. Disconnect components
- Electric: cap wires with rated wire nuts
- Gas: loosen union with two wrenches; avoid twisting the line
- Water: unscrew flex lines or cut copper ~ 2″ above fittings
4. Remove and recycle
- Team-lift tank for recycling
Phase 2: Foundation and Drain Protection (30 minutes)
- Clean and level footprint; use ¼″ shims if needed
- Position the drain pan
- Verify tank fits through all access points
Phase 3: Plumbing Rough-In (1–1.5 hours)
1. Dielectric unions
- Wrap threads with PTFE tape (3–4 wraps); torque to ~ 20 ft-lb
2. Flexible connectors
- Attach cold inlet to supply; hot outlet to manifold
3. T&P valve
- After hand-tightening, use a wrench to ensure the valve is securely installed and properly aligned
4. Gas piping (gas models)
- Install ½″ stainless-steel flex; soap-test all joints
5. Electrical wiring (electric models)
- Route 10 AWG cable; connect L1, L2, ground; clamp cable
Phase 4: Venting and Expansion (Atmospheric Vent Only)
- Attach draft hood to flue collar
- Install UL Type B vent with ¼″ rise per foot on horizontals
- Seal joints with high-temp foil tape
- Tee in the expansion tank upstream
Phase 5: Fill, Purge and Power Up (30 minutes)
1. Fill tank: close drain; open cold inlet; purge air via faucet
2. Leak check: dry-wipe fittings; recheck after 10 minutes under pressure
3. Restore utilities: breaker on (electric) or pilot light (gas); set to 120 °F
Phase 6: Final Tests (15 minutes)
- T&P pull test: lever lifts, water discharges, then reseals
- Element draw (electric): amperage within ± 10 % of spec
- Draft check (gas): flame pulls inward at the hood
Pro Maintenance & Troubleshooting
Video Guide: Anode-Rod Replacement
Anode rods sacrifice themselves to protect the tank. Watch the tutorial, then follow these steps:
1. Shut off water and fuel supply to the heater
2. Drain about 6″ from the tank to expose the rod while keeping weight inside
3. Remove any top cover to access the rod
4. Use a ratchet with a 1-1/16″ socket or an adjustable wrench for nipple-type rods
5. Add a pipe on the ratchet handle for leverage if needed
6. Withdraw and discard the old rod
7. Wrap new rod threads with PTFE tape; insert and tighten
8. Restore water and fuel, then check for leaks
Common Issues and Remedies
This section lists frequent water-heater problems, their likely causes, and quick fixes:
| Symptom | Cause | Remedy |
| No hot water (electric) | Tripped breaker or failed element | Reset breaker; replace element |
| Intermittent heating | Faulty thermostat | Swap thermostat |
| Rotten-egg odor | Spent anode rod | Replace rod; flush tank with peroxide |
| Pilot won’t stay lit | Worn thermocouple | Replace thermocouple |
| Rumbling or popping noises | Scale buildup | Flush tank; vinegar soak; install filter |
How to Maximize Water-Heater Lifespan
Routine care and strategic upgrades can extend tank life well beyond the norm:
1. Lower thermostat to 120 °F to reduce corrosion and save energy
2. Flush sediment annually; add an inline filter in abrasive water areas
3. Inspect and replace anode rods yearly or every two years in hard-water regions
4. Insulate the first 5 ft of hot and cold lines; add a heat-rated tank blanket
5. Install a water softener to prevent scale in mineral-rich areas
6. Place a leak sensor under the drain pan for early alerts
7. Schedule annual professional inspections to catch issues early
Implementing these measures can significantly extend a tank’s service life—ensuring reliable hot water for many more years.
Wrap-Up
Code compliance, craftsmanship, and common sense keep hot water flowing for over a decade. Every component—water heaters, flex connectors, dielectric unions, drain pans, expansion tanks, T&P valves, anode rods, straps & stands—ships quickly from Supplyhouse.