Skip to main content
Electric Panel

When it comes to electrical installations, the right electrical box can make all the difference between a clean, safe setup and a potential headache down the line. Whether you’re wiring up a new home, adding outlets to a workshop, or working on outdoor lighting, choosing the proper electrical box helps to achieve safety, accessibility, and long-term performance.

Let’s break down how to pick the right electrical box for both indoor and outdoor installations, so you’re not just buying something that fits — but something that works and works well.

What to Consider Before Choosing an Electrical Box

Before you even pick up an electrical box, a little prep work is necessary. A few things to keep in mind:

  • Type of Installation: 

Is it for a light fixture, an outlet, or a larger junction box?

  • Location:

Are you installing inside or outside? Different environments require different materials and box ratings.

  • Box Size: 

The box must be large enough to accommodate all wiring and devices, but not too big to create unnecessary space.

  • Material:

Electrical boxes come in plastic, metal, and fiberglass — each suited for specific environments and conditions.

Once you know what you’re working with, it’s time to consider the right box for the job.

Indoor Installations: Versatility and Durability

For indoor electrical work, most installations will use plastic or metal boxes. Here’s why:

  • Plastic Boxes: 

Lightweight, durable, and resistant to corrosion, plastic boxes are perfect for dry environments. They’re commonly used for switches, outlets, and light fixtures. Plastic also provides better insulation, which is great for preventing potential short circuits. Plus, they’re easier to install and can be mounted directly onto studs or in drywalls.

  • Metal Boxes: 

Are stronger and offer more robust protection than plastic. Metal boxes are typically used in areas where added strength is necessary — like in commercial settings or for more permanent fixtures. They also offer a higher fire rating and are often used when installing wiring for heavier loads.

Choosing the Right Box for Indoor Installations: 

When picking a box for indoor use, think about your specific needs:

  • For Light Fixtures: 

You’ll typically need a box with a single gang or a 4-inch square box for more substantial fixtures.

  • For Outlets and Switches: 

A standard single or double gang box should work. Make sure there’s enough room for all the wiring and connectors.

Outdoor Installations: Protecting Your Wiring from the Elements

Outdoor electrical boxes have a tough job. Not only do they have to house and protect wires, but they also have to handle the elements — rain, snow, wind, and dirt. That’s where weatherproof enclosures come in.

  • Weatherproof Boxes: 

Are designed to seal tight against moisture and dust, preventing water from damaging your electrical connections. You’ll find these boxes in outdoor lighting setups, security systems, and outdoor outlets.

  • Metal Boxes for Outdoor Use: 

Metal boxes in outdoor settings are often coated with corrosion-resistant finishes (like galvanized steel) to combat the elements. They’re ideal for installations that need added durability, like heavy-duty outdoor equipment or security cameras.

Choosing the Right Box for Outdoor Installations:

  • For Wet Locations: 

You’ll need an in-use weatherproof box that adheres to NEMA codes 4 and 6 to provide a tight seal when the outlet or switch is in use.

  • For Dry Locations:

If it’s an area that doesn’t face direct rain or moisture, a NEMA 3 rated box will work fine.

Remember, weatherproof and water-resistant are not the same thing — make sure to double-check the IP (Ingress Protection) rating to know how much protection the box provides.

Key Differences Between Indoor and Outdoor Boxes

The biggest difference between indoor and outdoor boxes is their level of protection. Outdoor boxes need to be water-resistant, dustproof, and able to handle extreme weather conditions. Indoor boxes, on the other hand, don’t need that level of sealing but should be sturdy enough to handle the electrical demands of the room.

For indoor installations, the emphasis is on ease of use, accessibility, and adaptability to various fixture types. Outdoor boxes need to go the extra mile in keeping moisture, dirt, and extreme temperatures at bay.

Size and Capacity: Bigger Isn’t Always Better

When choosing an electrical box, size matters — but so does capacity. You need a box large enough to hold all the wires, connectors, and devices you plan to install, but you don’t want to overdo it. Too large of a box means wasted space and unnecessary installation work. Too small, and you’ll end up crowding everything inside, which is a safety risk.

How to Choose the Right Size:

  • Depth and Volume:

Make sure the box has enough volume to house all the wires and connectors, with at least 1/4-inch of space on each side. A box that’s too deep can make it harder to mount fixtures properly.

  • Gang Boxes: 

It refers to how many switches, outlets, or devices the box will hold. For example, a single-gang box holds one device, a double-gang holds two, and so on.

Ready to Make Your Selection? Shop Electrical Boxes

Finding the right electrical box for your next project doesn’t have to be complicated. SupplyHouse carries a broad range of electrical enclosures and boxes to meet all your indoor and outdoor needs. From weatherproof boxes to sturdy metal and plastic enclosures, we’ve got you covered.