Skip to main content

The Takagi T-KJr2 and TK-4 tankless water heaters are great alternatives to traditional, tank based water heaters.  These units are two of the smallest water heaters Takagi has to offer, providing all the hot water you need, while taking up minimal space.  Coming in natural gas, propane, outdoor, and indoor varieties; Takagi has a unit for whatever situation you have.  The Jr is the smaller of the two and is more suitable for small homes and apartments, while the TK-4 can handle homes and apartments with up to 3 three bathrooms.  If you would rather use these units for hydronic baseboard or radiant floor heating don’t worry, they can handle that too.  If you are tired of wasting space on a traditional, tanked water heat, the T-KJr2 or TK-4 might be exactly what you need.  Watch the videos below for more information on the the units!

 

 

 

If you now want a T-KJr2 , TK-4, or any other plumbing, heating, and HVAC products, SupplyHouse.com has what you need!