For much of the latter 20th century, household plumbing systems depended on copper pipe—a difficult-to-master building material whose price only rose along with the ever-increasing demand. Today, many pros (and do-it-yourselfers) prefer to use tubing made of cross-linked polyethylene, or PEX. In addition to being cheaper than copper, PEX boasts the added advantage of being bendable. That means, compared to straight, rigid copper, PEX requires fewer connections and fittings, enabling installers to get the job done more quickly and with relative ease. Furthermore, once in place, PEX tends to fare better over the long haul, because durable plastic resists the mineral buildup and corrosion to which copper often succubus. Even better: PEX stands up admirably well to freezing temperatures, unlike metal pipes that freeze and in severe cases, burst open. In other words, “for many plumbing applications, you can’t do any better than PEX,” says Daniel O’Brian, a technical specialist with us at SupplyHouse.com.
Yet for all its advantages—and despite its soaring popularity across the building and remodeling industry—PEX remains poorly understood by the average person. In part, that’s because cutting, crimping, and clamping the material requires specialty tools to which many are unfamiliar. However, according to O’Brian, those who are new to PEX often get tripped up, not when installing the tubing, but rather when choosing which type to install. After all, PEX comes in more than 20 different varieties, each of which boasts its own set of pros and cons, and its own set of ideal applications. When shopping for PEX, therefore, “you must carefully consider the requirements of the project,” O’Brian explains, and from there, “decide which PEX product would make the best match for the task at hand.” To be successful, O’Brian concludes, “You need a basic understanding of the four main types.”
PEX-A The strongest, most durable, and most flexible option, PEX-A boasts the unique ability to recover from kinks. Normally, if a section of tubing were to become damaged or deformed, you’d have no choice but to remove and replace it. But with PEX-A you can use a heat gun to restore it to its original state. Overall, and for tight spaces in particular, “it’s hands-down the best,” O’Brian says.
PEX-B As you may have guessed, PEX-A commands the highest price. If you’re planning a project that involves, not tight turns, but long, straight runs, you can save money by opting of the next best option, PEX-B. Trading flexibility for rigidity, “PEX-B excels in a number of common applications,” O’Brian says. But there’s a downside to its stiffness: “PEX-B breaks where PEX-A would bend,” a fact that not only limits its utility, but also complicates the installation process at times.
PEX-C “PEX-B and PEX-C are pretty interchangeable,” O’Brian says. If there’s a practical difference between the two, it’s their relative hardness levels. “PEX-C is the softer of the two,” O’Brian continues, and for that reason, “it’s more vulnerable to kinks.” On the plus side: Because a different manufacturing process goes into PEX-C, it typically costs less than PEX-B. If you’re taking on a demanding project, though, bear in mind that to an extent, “you get what you pay for,” O’Brian says.
PEX-AL-PEX The most expensive of the bunch, PEX-AL-PEX, also known as aluminum-barrier PEX, features a special construction—namely, an aluminum layer that goes a long way to help the tubing keep its shape once bent. That means PEX-AL-PEX eliminates the need for the installer to employ tie-downs every few feet. In addition, because the aluminum layer doubles as an oxygen barrier, PEX-AL-PEX often plays a role in heating systems whose components would corrode if exposed to oxygen.
Note that each type of PEX tubing comes in a range of sizes, some as narrow as a quarter inch, others as wide as three inches. That said, for many plumbing and heating applications, building codes often specify the use of half-inch tubing—“the same diameter that would be required if copper pipe were used instead,” O’Brian points out. The fine print here is that half-inch PEX tubing tends to deliver a higher flow rate than identically sized copper piping. If the results of your project hinge on achieving a specific flow rate, be sure to consult a conversation chart like this one. Also, remember that experts don’t recommend PEX for any use that would leave the tubing exposed to sunlight. “PEX isn’t UV-resistant,” O’Brian explains. “After only a month in the sun, it starts to turn get brittle.” Finally, O’Brian cautions, remember that “PEX is freeze-resistant, but it isn’t freeze-proof.”
When looking for PEX or any other plumbing and heating products be sure to go to SupplyHouse.com. With our huge stock of over 90,000 products we are sure to have what you need. If you are looking for more information about any of our products check out our Resource Center or watch the video below to learn more about about PEX.
This post was written in collaboration with BobVila.com