Skip to main content

Recently Updated11

1. Quick, Reliable Connections

ProPEX connection

Each ProPEX joint can be cut, fitted and completed in under 30 seconds.

 2. Superior Flow Rate

hoseflow

 Uponor PEXa pipe and ProPEX fittings have the same inside diameter as eachother. This causes water to flow more consistently out of taps and showers.

3. 25 Year warranty!

Enclosure-Air-Conditioner-Warranty

Covers not only the pipe itself, but also any water damage to buildings in the event of a leak if the pipe is installed by a certified contractor!

4. Cost

DSC_4804