Skip to main content

0650872-4

The age old question of which connection system is best to use at home can finally be put to rest. Our most popular system for homeowners is the PEX crimp connection system.

 

The crimp system uses a copper ring that slips over the fitting and the PEX tubing. When used in conjunction with a crimp tool, the result is a water tight seal.

 

h010375lf-6

Crimp tools come in a variety of styles resulting in several buying choices for the home owner. One of our most popular tools is the “Watts Pex Crimp All Tool Kit.” It’s an all-in-one kit that features four jaws for different PEX sizes ranging from 3/8” making the tool an ideal option for customers who will be working with several different diameters.  This particular kit features the jaws, a calibration tool, a tool case, and a “go/no-go” gauge. Using this gauge correctly grants you peace of mind that the connections are secure and leak free.

 

An alternative to the kits offered by our site can be the individual tools offered by Viega. These tools are designated by the tube size you are working with. You need to buy different tools for every size of tube you are working on, but in the long run it will save time as opposed to spending it switching the jaws. Added benefits include the featured longer handle that requires less human force to complete the crimp connection and the angled head, optimal for crimping in tight places.

 

For more information, this video should do the trick!