We’ve added a range of Noritz Tankless Water Heaters to the site. Noritz has been an innovator of the water heating industry for over 60 years. Having introduced the first modern, electronically controlled tankless hot water heater in 1981 they remain the leader in energy savings and superior hot water delivery today.
At SupplyHouse.com you can find a selection of Noritz Tankless Water Heaters for commercial or residential use, and are available with Natural Gas or Propane. With a Noritz Tankless Water Heater you will never run out of hot water, and because it heats water on demand to the set temperature almost instantaneously you will be saving energy and cutting costs. As it only operates when necessary it’s also eco-friendly.
These tankless water heaters save space, are easy to install, and use cutting-edge technology. The hot water temperature can be easily adjusted using digital remote controllers which keep the temperature stable at all times. Have a look at our Noritz collection here!