SupplyHouse Blog Banner 2





The MOST Accurate Way to Check Your Oil Levels

Rosie

beckett, rocket, wireless, fuel level monitor, supplyhouse, supplyhouse.com, plumbing, hvac, boiler, oil, mechanical float gauge, transmitter, lithium battery, heating, heater, home heating, convenience, accurate, efficient Well folks, the future is here. Prepare for the lift-off of the new Beckett Rocket 17000 System—a wireless fuel level monitor made with efficiency and comfort in mind. This Rocket is an electronic gauge that will measure the amount of fuel in your oil tank with sharp accuracy. But it doesn’t stop there! It will then launch your information wirelessly into an easy-to-read receiver, which you can hear and read conveniently from anywhere in your home! No more lacing up your boots to go check on the oil!

 

With an easy, 10-minute installation, it’s tough to pass up this gadget. The transmitter is mounted on an available opening in the tank and uses ultrasonic technology for measurement. The receiver only needs to be plugged into a 120V outlet to charge and receive data.  Not only is it easy to install—it’s also easy to use. The LCD display on the receiver displays bars on the screen, kind of like a phone battery. Each bar represents about 10% of the tank’s capacity…when the bars are low, you’ll know it’s time to make an order to refill your tank. When the oil level drops below 20% capacity, a nozzle icon will appear, and just in case you forget, at 10% capacity, a red LED will flash, and a beep will sound once an hour to warn you that the fuel level is low. Simple and beautiful!

 

In addition to the comfort of installation and use, the Rocket Fuel Monitor is incredibly accurate and adaptable to different tank sizes and locations. With a 150 ft. range between transmitter and receiver and the ability to work on tanks up to 10ft in height, it still maintains an even higher accuracy and reliability than a mechanical float gauge. Additionally, you can set up multiple receivers, in case you want one in the garage and one in the kitchen. If you have multiple housing units and oil tanks in a close range—don’t worry! Multiple pairings of transmitters and receivers can be set up in a close range without interfering with one another.beckett, rocket, wireless, fuel level monitor, supplyhouse, supplyhouse.com, plumbing, hvac, boiler, oil, mechanical float gauge, transmitter, lithium battery, heating, heater, home heating, convenience, accurate, efficient

 

If all that doesn’t convince you, consider this: the lithium battery can last over 10 years, and is replaceable. Needless to say, this Rocket will take you far.

 

The Kit includes everything you need—receiver, transmitter (battery included), 2” NPT Adapter, 2 mounting screws, and instructions. There are other sized adapters available as well.

 

Give it a shot and explore the Rocket Wireless Fuel Level Monitor, along with its multiple 5-star reviews, on site here.

 

Posted in All Posts, How Tos + Tricks, Products | Tagged , , , , , , , , , , , , , , , , , ,

Leave a Reply

Your email address will not be published.


Logo

Join Our Mailing List - Sign up and receive special offers and coupons