SupplyHouse Blog Banner 2





The CORRECT Way to Put Toilet Paper on a Roll; the Debate is Finally Solved!

Gregory

At one point or another, we’ve all had this discussion: how are we supposed to put toilet paper on a roll? Which way is it supposed to hang, over or under? Well look no further, because we have your answer!

 

 

Toilet paper, toilet paper roll, patent, 1891, seth wheeler, modern toilet paper, toilet paper orientation, inventor, google patent, toilet paper, toilet, debate

There is actually a technical, documented, correct way that one should hang their toilet paper on the roll: by using the “over” position. A debate as old as time (well, maybe not that long, but still well over one hundred year old) can finally be classified as ‘solved.’ The answer lies in a patent from 1891.

 

On September 15, 1891, Seth Wheeler officially became the ‘father’ of modern toilet paper, thanks to identifying the correct method in which to orient it. His patent no. 459,516 classifies that the “over” method is technically the correct way that toilet paper should be hung on a roll. Each of the six associated figures demonstrates this process.

 

 

 

 

 

 

 

Toilet paper, toilet paper roll, patent, 1891, seth wheeler, modern toilet paper, toilet paper orientation, inventor, google patent, toilet paper, toilet, debate

Automated Toilet Paper Server Design

Toilet paper, toilet paper roll, patent, 1891, seth wheeler, modern toilet paper, toilet paper orientation, inventor, google patent, toilet paper, toilet, debate

Flattened Toilet Paper Design

 

 

 

An earlier version of his toilet paper design dates back to his 1887 patent, when toilet paper improvements were on the rise. The patent reads, “This improvement relates to a new article of manufacture, consisting of a roll of wrapping or toilet paper with parallel ends composed of polygonal or curved sheets, the sides of each sheet having edges of broken or curved lines.”

 

 

Needless to say, Seth Wheeler had a lot of time on his hands in the late 1800s. Aside from perfecting the orientation of toilet paper rolls, he also created patents and designs to help with their overall shape and design, the automation of dispensing new sheets, a flattened roll design, multi-roll holder, and even a device to perforate and create ornamental paper with diamond patterns for aesthetics.

 

Toilet paper, toilet paper roll, patent, 1891, seth wheeler, modern toilet paper, toilet paper orientation, inventor, google patent, toilet paper, toilet, debate

Diamond-ribbed Ornamental Toilet paper

 

 

 

Check out this link to the Google Patent page where you can see the full patent from 1891, complete with original figures and the actual patent proposal. And next time this debate comes up, you can argue your point with solid evidence; not to mention that it’s a great fun fact for dinner party conversation!

Posted in All Posts, How Tos + Tricks, Industry Buzz | Tagged , , , , , , , , , ,

11 Responses to The CORRECT Way to Put Toilet Paper on a Roll; the Debate is Finally Solved!

  1. Vincent Gurubatham says:

    Very interesting article on the orientation of toilet paper hanging method. The way the inventor has shown is the way most people do. Just common sense.
    I myself have over 40 Global Patents on different products and my grand son who is ten years of age invented a non clogging nozzle for calking guns and we are helping him with the Patent. This nozzle is designed to easily spit out a hardened calking product in the nozzle.

  2. Lee Leimberg says:

    House cats prefer the overshot configuration.

  3. Martin Magda says:

    Although proper function and ease of use pretty much mandates the “over” position, there is an exception and meaningful reason for using the “under” position. House cats! These playful fur balls start out using these as a scratching post and can’t resist the excitement of unraveling the entire roll. Many cat owners have often come home to this type of a bathroom celebration.

    • Gregory says:

      Martin, you have a great point. Our cats see anything and everything as toys! Nearly everyone who has ever had a cat as a pet can relate to coming home and finding their bathroom in this dreaded condition!

  4. Nancy says:

    I totally agree on the cat issue, not to mention a dog I used to have! My reason however is mostly hygienic. I can’t stand the thought of how many fingers would touch that wall if the paper was under, not to mention where those fingers may have been! I am totally “over” it!

    • Gregory says:

      Nancy, I think all of our pets will eventually play with our toilet paper rolls. They probably just look like so much fun! You have an excellent point about keeping things hygienic and clean.

  5. Mario Trujillo says:

    Awesome! All the time I puted it wrong.

  6. Anon. says:

    But you have to touch the roll to rip the paper either way, and also the roll touches the wall as it rolls. I don’t think there is any special benefits, either way.

  7. W Day says:

    But you have to touch the roll to rip the paper either way, and also the roll touches the wall as it rolls. I don’t think there is any special benefits, either way.

Leave a Reply

Your email address will not be published.


Logo

Join Our Mailing List - Sign up and receive special offers and coupons