SupplyHouse Blog Banner 2




Radiant Heat Without the Concrete: Ultra-Fin Plates

Shyene

Central air heating not doing the trick for your family during those cold East Coast winters? Have a wood-framed home that doesn’t retain heat? One option you have is radiant heat, which consists of a hydronic tubing system underneath your actual flooring. But wait, radiant heat sounds complicated…

read more...

What’s Up with Uponor? A Refresher on the Brand

Shyene

What’s up with Uponor – get it? Yes, no, maybe so. In this post, we’re revisiting the leader in PEX supplies, Uponor (formerly known as Wirsbo in case you’re one of those homeowners with the older manifold/actuator set-up). There is a major update with Uponor’s product line as well. Keep r…

read more...

SharkBite Bits: All You Need to Know about SharkBite

Michelle P

Most of us in the industry have heard of SharkBite as the creators of the famous push-to-connect plumbing fittings, but did you know that in addition to their push-to-connects, SharkBite also produces their own PEX tubing and valves that can be purchased in a variety of lengths and sizes?   …

read more...

SharkBite Swings for the Fences with their Home Run Manifold

Gregory

When SharkBite comes to bat, they never fail! They’ve made manifolds even easier with what’s called a home run manifold!   So what is a home run manifold, you ask? Well, it’s a system that you run your water on a large—typically ¾”—supply line that feeds into a central manifo…

read more...

The Future of Leak Detection

Guest

Hey all! I’m coming to you today with a game changing product in the world of leak detection. We hear it a lot, “The future is here, today!”   Well, we are going to imitate that with a new product from Uponor, named Phyn. Phyn is a connected whole home leak detection monitor. Develo…

read more...

Facebook Live Seminar: Uponor’s PEX Tubing

Mark

For the second installment in our Facebook Live series we brought in a couple experts on Uponor and their PEX tubing. (Watch the first one on Taco here)  Wes Sisco from Uponor fielded questions from our audience using his years of experience plumbing and working with Uponor products, Jim DePalma j…

read more...

PEX: Uponor’s Contribution to the World of Plumbing

Nick B

The modern day Uponor is the culmination of two longstanding and innovative companies.  Uponor’s origins date back to a Finnish carpentry workshop opened in 1918 while the other half, Wirsbo, began in the 1620s as a Swedish forge, crafting top quality steel and weapons for the King of Sweden.  T…

read more...

How to Make ProPEX Expansion Connection

Mark

Uponor's ProPEX expansion connection system is a reliable and easy connection method for PEX-A tubing that actually becomes stronger over time. Using an expansion tool that features an auto-rotating head, like the Milwaukee M12 Tool, connections can be made in under 30 seconds with minimal room to …

read more...


SupplyHouse.com Logo