SupplyHouse Blog Banner 2




3 Plumbing Problems to Look for When House Hunting

Nick B

When you are touring a home or apartment it can be an overwhelming experience.  Between thinking about where you would put all of your furniture, analyzing the commute from that location, and mentally balancing your budget with the new place in mind, it’s easy to forget something like the plumbin…

read more...

How To Prevent Frozen Pipes

Nick B

The cold time of year is upon us.  That means more coats, slicker roads, and for many, pipes frozen to the point of bursting.  The plumber's life has turned into call after call about repairing plumbing systems destroyed at the hands of freezing temperatures, power outages, older pipes, and poor p…

read more...

Got a Stinky House? Give Odor Block a Try!

Nick B

Does your home not smell as good as it should?  It's not always something you can control, all it takes is a little unwanted moisture growing mold or a particularly adventurous animal finding its way into somewhere it shouldn't be.  Once these odors start, regardless if they are in your vents or n…

read more...

Five Ideas to Save Energy On Your Home When Traveling

Guest

  Whether you’re traveling for business or pleasure, there’s one thing you should never forget to do before you go: make your home more energy efficient. Unless you make certain changes, your home can waste a lot of energy while you’re not there, meaning you’ll be greeted with a …

read more...

Your Guide To Apollo Valves…

Adam

We sell a large variety of Apollo Valves, and all have different and unique uses. Here's a breakdown of the most popular, and some information on their uses... Ball valves:- Used for shut-off and/or purposes of control Air Cocks: - Provide an economical way to shut off air lines. &nb…

read more...

What Happened to PEX and Copper Pipe When Frozen…

Steffy

  We put PEX-a, PEX-b and Copper Pipe filled with water and capped with sharkbite end caps in the freezer during our first episode of SupplyHouse Speculations. Find out the result in our video below... …

read more...

Radiant Heat Insulation Saves Money

Steffy

Envious of your neighbor with the tulip-filled lawn in January? Think again.  According to Daniel O'Brian, a technical expert here at SupplyHouse.com, warm soil mid winter comes at a huge cost to the home owner.  Instead of warming the house, the BTU’s are traveling in all directions and are…

read more...

Benefits of Pipe Insulation

Tom

Insulating pipes provides many advantages in a variety of fluid distribution systems. See below for a list of common applications. SupplyHouse.com carries K-Flex Insul-Lock pipe insulation. Insul-Lock comes in 6-foot lengths for pipes with outside diameters ranging from 1/2" to 4-1/8". We offer Insu…

read more...

Control Temperatures and Save Energy with Zoned Heating Systems

Kristine

A zoned heating system allows greater control over heat distribution in the house. You can turn up the heat just where you need it, just when you need it—resulting in significant savings on your utility bills. Need some convincing? Read on to learn more about the benefits of zoned heating. …

read more...

Where there is air

Kristine

Air is the enemy in a hydronic (hot-water) heating system. It blocks their flow to the radiators. It rattles around and annoys customers. It wastes fuel by making our systems less efficient (no heat from an air-bound radiator). It causes callbacks and it makes us look bad. That's why every hydronic …

read more...

Increase Your Comfort Level This Winter With a Humidifier

Kristine

In the winter months, when heating systems are really chugging away, indoor air can become dry and staticky. A whole-house humidifier is a great way to add back a little moisture. Here are the basics. Scratchy throats, frequent nosebleeds, dry skin, and static electricity can be common occurrence…

read more...

Frozen Pipes

Tom

Frozen pipes are a common occurrence during the cold season. To thaw a frozen pipe in your home, try turning on each faucet. If the water is flowing, run warm water through the pipes to help thaw the frozen spot. If no water flows, find the most likely places where pipes may freeze, such as unheated…

read more...


SupplyHouse.com Logo