Water heaters protect their tanks using what are known as sacrificial anode rods. These are metal rods which are suspended inside a water heater so that they are surrounded by the water in the tank. The metal rods are more susceptible to corrosion than the tank walls. The result is that the ro…

No Soldering, Clamps or Glue Needed With SharkBite Fittings.
Quick-connect, push-fit plumbing has been taking a bite out of local plumbing trades, as the general public, tradesman included, discover the ease, versatility, and quality of SharkBite fittings. Their innovative design allows anyone to connect copper, PVC, and PEX tubing—in any comb…

If You’re Looking For The #1 Tankless Water Heater, We’ve Found It.
Rinnai is the number 1 selling tankless water heating brand in the U.S. Their main focus is innovating water heating and home heating gas appliances for residential and commercial applications - and they're good at what they do! The tankless water heaters can use up to 40 percent less energy than…

Control the Thermostat, and The Size of Your Monthly Bill—From Anywhere
The next great step forward in thermostat technology has arrived—Wi-Fi compatibility. Wi-Fi thermostats offer the same functions and features as standard programmable thermostats—with one major difference. They communicate with your home wireless network, allowing you to monitor and control yo…

Why A Denim Blanket Is Necessary For Your Water Heater…
Is energy efficient something you strive for? We're guessing, most likely yes, which is why the UltraTouch Water Heater Blanket makes perfect sense for you! It is manufactured from 90% recycled denim and is a Class-A building product that meets the highest ASTM s…

Make Line Sets Invisible With Rectorseal
We're in mutual agreement that line sets are better unseen. Fortress Line Set Covers manufactured by Rectorseal have been developed as a cost-effective solution in the market, and will offer you strength and longevity at a very good price. The Fortress range is available i…

Take The Reigns on Your HVAC Systems With KMC Controls
Your destiny is in your own hands, and KMC Controls makes it a whole lot easier to shift your HVAC destiny in the right direction! Designing and manufacturing HVAC control systems and building automation systems since 1969, KMC Controls can help improve occupant comfort whil…

Are You Still Cleaning Toilets the Old-Fashioned Way?
Cleaning the toilet isn't fun, no matter how you slice it. It’s tedious and time-consuming, and—when you get right down to it—rather unpleasant. That’s why it makes so much sense to adopt a hands-free approach: Let an automatic toilet cleaner do the job for you! Install …

Like PVC Pipe, But It Can Bend!
One of the largest differences between PVC and PEX is the lack of flexibility that PVC is famous for. But what if PVC Pipe has changed its ways? Red Flag Products range of Ultra Flexible PVC Pipe is the most flexible PVC pipe in its class with incredible ben…

Control Your Thermostat Settings Remotely, No RedLink Needed!
The all-new Honeywell Wi-Fi VisionPRO 8000 Touchscreen Thermostat enables you to remotely control all of your settings, and even manage your energy costs over a wireless network using Honeywell’s free Total Connect Comfort application; available on your Smartphone or on your PC without the need …

We’ve Figured Out a Solution To All of Your Drain Problems…
Who doesn't wish for a job well-done with half of the price tag? SureSeal Floor Drain Trap Seals do just that - they block emissions of noxious sewer gases from backing up into your living or work areas, a job usually performed by a much more expensive tr…

Turning Your Phone into an HVAC Tool Is This Easy…
Step one, own a smartphone. Step two, purchase the Automatic Airflow Balancing Meter- a $39.95 investment that will change the way you work. Step three, download the free app from the Apple or Google app stores. And Voila! Is the job easier yet? The ABM-100 …