SupplyHouse Blog Banner 2




PEX Crimp vs. PEX Clamp

Tom

PEX crimp and PEX clamp connections use the same fittings, normally referred to as “crimp” or “barbed” PEX fittings. Each method requires a different tool and a different type of ring, but the styles are similar enough that PEX newcomers frequently wonder which method is preferable. Crimping…

read more...

Gruvlok Grooved Fittings

Adam

Gruvlok Grooved Fittings have recently been added to SupplyHouse.com. You can find Grooved Elbows, Couplings, Tees, Flanges, Butterfly Valves, and more here.  Gruvlok Grooved Fittings by Anvil International, sets the industry standard for durability, efficiency and flexibility, and these fittings a…

read more...

Intelligent Washing Machine Flow from Watts

Tom

Watts IntelliFlow Washing Machine Water Shut-off Valves automatically regulate hot and cold flow to washing machines. The valves sense increases in electrical current draw when a washing machine operates. This signals the valves to open in order to allow water to flow to the washing machine. The val…

read more...

Noritz Tankless Water Heaters

Adam

We’ve added a range of Noritz Tankless Water Heaters to the site.  Noritz has been an innovator of the water heating industry for over 60 years. Having introduced the first modern, electronically controlled tankless hot water heater in 1981 they remain the leader in energy savings and superior ho…

read more...

Check Webstone First for Any Valve Needs

Tom

The name Webstone is synonymous with valves. SupplyHouse.com carries the full selection of Webstone valves for plumbing and heating applications. Standard ball valves can be purchased almost anywhere, but Webstone ball valves are available with features such as drains and T-handles. The T-Flow Ball …

read more...

AO Smith Vertex Power Direct Vent Water Heater

Adam

Joining the AO Smith Vertex Power Direct Vent Water Heater family is the new 75-gallon model. The GDHE-75 offers the same high level of performance as its 50-gallon sibling, and you can find both on the site. The GDHE-75, with its 96% thermal efficiency rating, is designed to specifically generat…

read more...

Water Heater Leak Detector

Tom

When a water heater starts to leak, it will not stop trying to produce hot water. In a worst-case scenario (a major leak with no one home to notice it), the damage can be severe. Taco’s WAGS valve senses such leaks to prevent this type of damage and provide peace of mind. The WAGS valve should be …

read more...

Takagi T-H3 Tankless Water Heaters

Tom

Tankless water heaters offer the potential for increased efficiency because they do not waste energy heating water during periods of non-use. Takagi’s T-H3 Series of gas-fired tankless heaters offers several useful features in addition to extra efficiency. Created as new-generation T-H2 heaters, t…

read more...

SharkBite Removal Tools

Tom

SharkBite fittings offer an easy way to make basic repairs or permanent installations. They slide directly over PEX, copper, or OD-controlled CPVC without requiring any tools, making them ideal for small jobs and do-it-yourselfers. Removing SharkBite fittings is just as easy – if you have the prop…

read more...

Blue Monster Compression Seal Tape

Adam

Blue Monster Compression Seal Tape is perfect as a quick and cost-effective solution to help stop leakage under pressure without turning off the water source. This makes it the ideal solution equally for crisis and long-term applications, and has been developed for professional plumbing contractors.…

read more...

SharkBite 2XL Fittings

Tom

SharkBite push-fit fittings revolutionized plumbing and hydronic heating, making installations and repairs faster and easier for professionals and do-it-yourselfers alike. Previously available in sizes only up to 1”, SharkBite now makes fittings for larger pipe. SharkBite 2XL fittings work with 1-…

read more...

The Purpose of PEX Oxygen Barriers

Tom

Make sure to use oxygen barrier PEX in any closed-loop hydronic heating system that includes PEX tubing. New water is not routinely introduced to closed-loop systems. The same water cycles through them, under pressure, continuously. Oxygen corrodes ferrous metals. Any system components made from …

read more...


SupplyHouse.com Logo