SupplyHouse Blog Banner 2




Steam Boiler is Over 50 Years Old, High School Considers Replacing Artifact

Gregory

A high school in Geneseo is still using Kewanee steam boilers originally installed in 1952 and 1963. These systems, over 60 years old, are in desperate need of repairs, which is causing the school to debate replacing them altogether.   The original steam boiler was installed in 1952 to ac…

read more...

Don’t Flush Your Contacts!

Nick B

Pop quiz: you just took out your contact lenses and are ready to dispose of them.  Where do you put them, in the nice little trash can, or the toilet?  If you said toilet then you need to stop.  The toilet is not a trash can, so if it's trash, don't put it in there.  And yes, that includes cont…

read more...


SupplyHouse.com Logo