SupplyHouse Blog Banner 2




Give your Dryer a Boost

Tom

Does it seem like it takes forever for your clothes to dry? The solution may be easier than you think. With a Fantech Dryer Booster Exhaust Fan from SupplyHouse.com you can cut down on clothes drying times and slash your utility bills. Dryer Booster Fans are perfect for homes with long runs betwe…

read more...

Keep Your Home Cool, Dry, and Energy-Efficient With a Dehumidifier

Kristine

Sure it's uncomfortable outside, but if you are sensing damp, sticky conditions indoors, it's definitely time to consider the benefits of a dehumidification system. Hot and muggy summer weather outside can mean excess moisture inside. Mold and mildew, musty odors, condensation, warped wooden surf…

read more...

Hydraulic Expander Kit from Yellow Jacket

Adam

The Yellow Jacket Hydraulic Expander Kit helps save time by eliminating fittings as well as saving you money on soldering points and materials.  The lightweight, easy to use, one handed operation of the manual hydraulic mechanism expands tubing from 3/8” to 1-5/8”, replacing the need for additi…

read more...

PexTV Episode 7

Mark

Hey, here’s episode 7 of “PexTV” It's HOT out there, and Summer Sam wants you to STAYYYYYYYY COOOL.  Feel free to email us at pextv@supplyhouse.com with any thoughts or suggestions for future episodes. In this episode, you’ll see… Featured Product: LG Art Cool Picture Frame AC Unit …

read more...

Test Tools HVACR Pros Trust

Kristine

Live Readings for Full System HVAC Analysis with Fieldpiece Wireless! Now you can be faster, more accurate, and do more! Using Fieldpiece network of wireless tools you can get live readings in the palm of your hand! The Wireless HVAC Guide® System Analyzer, model HG3 turns any Fieldpiece Accesso…

read more...

Stay Cool With Art Cool

Mark

A little while back, Tim from receiving and I put together a video on LG's "Art Cool" mini-split air conditioning systems.  These units can help you stay cool in this current heat, and they also look awesome. With LG's Art Cool systems, you can transform your air conditioner into a piece of art.…

read more...

“Which Line Set Do I Need?”

Mark

I recently spoke with Nicole from customer service and she told me that a number of people call and ask about Line Set sizing. A line set is used to connect an indoor evaporator unit to the outdoor condenser in a ductless mini-split air conditioning system.  A line set includes a supply and ret…

read more...

QuikSEER+ WattSaver

Adam

With summer upon us, the QuikSEER+ Wattsaver from Mainstream Engineering is an innovative and cost-saving electronic control that operates in the cooling mode of an existing air conditioner or heat pump.  By varying the airflow of the blower motor, this technology optimizes the airflow of the air c…

read more...

The Mini-Split Air Conditioner: Today’s Smart Cooling Option

Kristine

If you live in an older home without ductwork, or if you've added a new room to your house, consider the benefits and convenience of a mini-split air conditioner. Now that summer has arrived, it’s definitely time to focus on home cooling. If your house does not have central air conditioning—a…

read more...

Fantech Dehumidifiers

Adam

Dehumidifiers are primarily used to remove excess moisture from the air.  Some homes or residences can have moisture problems only at specific times of the year, such as in spring, whilst others may have problems all year round.  There can be certain areas or rooms that need specific attention.  …

read more...

Save 5% on Spirotherm Air Eliminators! Use code: SPIRO5 (Exp. 6/19/13)

Kristine

Spirotherm Air Eliminators are designed for use in hydronic heating systems. In heating applications, air in the system water can cause corrosion, reduce efficiency and can result in poorly heated rooms. Stock up and save today! Spirotherm Air Eliminators Feature:     Solid Brass Constr…

read more...

New Product: Line Set Covers

Adam

Line Set Covers are a great way to tidy up the installation of mini-split air conditioning and heat pump systems where the line sets are travelling on the outside of the house.  This is especially useful when the air handler is up high on the wall with mini-split systems, or when the air handler fu…

read more...


SupplyHouse.com Logo