SupplyHouse Blog Banner 2




Hot Water Made Easy, Thanks to Tankless

Gregory

We all love hot water; it’s great for a hot shower or a nice cup of tea. And the only way we can consistently and reliably get hot water in our homes is through our hot water heaters. But not all water heaters are created equally. So let’s talk about tankless water heaters.   What mak…

read more...

How to Double the Lifespan of your Water Heater

Gregory

To many, water heaters are a one-and done item, meaning once you install it, that's it. But think again. The way to doubling the lifespan of a water heater lies in a yearly check-up of one simple part: the anode rod. To get to the anode rod, let's first work our way through the water heater itself.…

read more...

Steam Boiler is Over 50 Years Old, High School Considers Replacing Artifact

Gregory

A high school in Geneseo is still using Kewanee steam boilers originally installed in 1952 and 1963. These systems, over 60 years old, are in desperate need of repairs, which is causing the school to debate replacing them altogether.   The original steam boiler was installed in 1952 to ac…

read more...

Amtrol BoilerMate Indirect Water Heaters

Mark

When it comes to saving fuel without sacrificing hot water performance, few brands stack up to Amtrol's BoilerMate's line of indirect water heaters.  Perfect for homes the utilize hydronic heating systems, the BoilerMate line utilizes the heat generated from the hydronic system's boiler to create u…

read more...


SupplyHouse.com Logo