SupplyHouse Blog Banner 2




ZoomLock, a.k.a. the New Best Friend of Refrigerant Lines

Shyene

Several recent blogs revolved around SharkBite and its ability to provide an alternative to soldering. While the product I’m about to discuss is not tool-free, it allows those without much copper installation experience to make a solid connection. Parker Hannifin came out with a new method for…

read more...

What’s Up with Uponor? A Refresher on the Brand

Shyene

What’s up with Uponor – get it? Yes, no, maybe so. In this post, we’re revisiting the leader in PEX supplies, Uponor (formerly known as Wirsbo in case you’re one of those homeowners with the older manifold/actuator set-up). There is a major update with Uponor’s product line as well. Keep r…

read more...

Viega’s Fresh off the Press

Shyene

Our “Fittings” tab has a lot to choose from, including a dozen different brands and just as many connection methods. So you're probably asking yourself "Where do you start? Which brands can you trust with a secure hold for potable water, fire sprinkler systems, fuels, gases, and lubricants?" Don…

read more...

Bluefin PEX Fittings

Emily

  These lead-free barbed fittings work for PEX connections and may be used with the copper crimp ring system or the stainless steel clamp system.   Bluefin PEX fittings come in poly and brass material.  They come in different styles of fittings such as elbows, tees, couplings, ad…

read more...

How To: Connect PEX to Copper or PVC

Guest

Today, with the help of cross-linked polyethylene (PEX) pipe, plumbing work has become more efficient for professionals and much more accessible for do-it-yourselfers.  These flexible red and blue pipes can bend in nearly any direction to funnel hot and cold water, respectively, where it needs to g…

read more...


SupplyHouse.com Logo