SupplyHouse Blog Banner 2





Sump Pumps: The Basics

Guest

In order to maintain the drainage systems of your residential, as well as commercial, buildings installation of sump pumps is very crucial.  They are made efficient to pump out the extra water accumulated in the basement of your buildings.  Sump pumps keep the basement dry and procure a smooth drainage flow in the system.

 

There are a number of different types of sump pumps that are available in the market.  Each type of sump pump is used for a specific purpose in the advent of managing the draining system of the building.  Therefore, in order to find out the most appropriate sump pump that would suit your purpose, you would first need to make sure that you know about these types and their specific functionalities.

 

 

What Are Primary Sump Pumps?

Primary sump pumps are the most basic and standard pumps that are usually found in residential buildings.  They are specifically designed to pump out the seepage water from the basement and prevent waterlogging.  They are preferably the best choice for residential purposes where they can efficiently pump out up to more than a thousand gallons per hour, just to keep your house dry and safe.

 

Now, these primary sump pumps are further subdivided into submersible pumps and pedestal pumps.  Where submersible sump pumps are strategically placed under the water in the basin of the pump, pedestal pumps are positioned with the pump motor outside the water, which is above the sump basin.  In case of small basins, pedestal pumps are the best choice as the pump base is technically submerged but the motor of the pump is not.

 

Battery Backup Pumps And Combination Pumps

In case of a power failure or an event where the main pump somehow fails, these battery backup sump pumps would make sure that the motor does not stop working.  Ultimately the battery on the unit of the backup would come in to provide the main pump with sufficient power to continue working even without the presence of the electric power.

 

Moreover, a combination sump pump is simply a combined machine of a battery backup pump and a primary pump in one whole package.  This pump would keep your drainage system safe and smooth in normal conditions as well as in the onset of a power failure.  It works best as a flood protection measure in residences.

 

The Final Blow

Another important type of sump pump is the sewage pump.  These types of pumps are rather used to pump out the sewage from the drainage system with an automatic mechanism.  They are efficient as well as widely used in residential buildings.

 

Now that you know all the different types of sump pumps available in the market, it will be easier for you to make your pick.  Whichever type of pump you choose, you need to be sure that your choice of the sump pump is efficient in fulfilling the purpose you are purchasing it for.

 

-Written by guest contributor, sumppumpguides

 

Posted in All Posts, Products | Tagged , , , , , , , , ,

4 Responses to Sump Pumps: The Basics

  1. Grage says:

    great stuff is this really appreciated to you guys have a best information i got..

  2. billy says:

    Nice post about sump pump.. it has best ideas to know about the basics things.. l was going to buy sump pump for my home but i had not right information before reading this post.. but now i really thank you guys for sharing best information..

  3. Highly appreciative information on sump pump . not only it guides about what sump pump to prefer but also what is appropriate.

Leave a Reply to thesumppumpguides Cancel reply

Your email address will not be published.


Logo

Join Our Mailing List - Sign up and receive special offers and coupons