SupplyHouse Blog Banner 2





SharkBite Swings for the Fences with their Home Run Manifold

Gregory

When SharkBite comes to bat, they never fail! They’ve made manifolds even easier with what’s called a home run manifold!

 

So what is a home run manifold, you ask? Well, it’s a system that you run your water on a large—typically ¾”—supply line that feeds into a central manifold. Then, the manifold branches off into smaller port piping for each individual fixture. Even though it requires a lot of pipe to operate a system like this, it will ultimately save customers from using large amounts of water. The key to it all? The port piping requires a smaller, over-all piping, typically ½” or 3/8”.

 

SharkBite Home Run Systems make our lives easier in so many ways. First off, they are incredibly easy to install. It also uses the signature ½” push to fit connections on the ports and ¾” MNPT threaded supplies. Plus, for those of you who use PEX, CPVC, or copper, you’re able to simply insert your tubing into their respective ports for a quick and water-tight connection. Even if you use Uponor’s expansion method, you can easily use the Home Run manifolds!

 

Like all of SharkBite, this manifold is made to last! It’s constructed of a durable poly-alloy that has options for brass ball valve ports or poly-alloy ball valve ports. In addition, the brackets are already attached, making your installation work as minimal as installing a few screws.

 

The SharkBite Home Run Manifold is currently offered in either 12 or 24-port configurations, for use with either brass or poly-alloy connections.

 

You can find the SharkBite Home Run manifolds at SupplyHouse.com along with all other SharkBite products and everything else you for your plumbing needs!

 

Posted in All Posts, Products | Tagged , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , , ,

Leave a Reply

Your email address will not be published.


Logo

Join Our Mailing List - Sign up and receive special offers and coupons