Home Radiant Heat

Category: Radiant Heat


Radiant Heat Insulation Saves Money

Steffy

Envious of your neighbor with the tulip-filled lawn in January? Think again.  According to Daniel O’Brian, a technical expert here at SupplyHouse.com, warm soil mid winter comes at a huge cost to the home owner.  Instead of warming the house, … Continue reading

Posted in Heating Supplies, Radiant Heat | Tagged , ,

AquaMotion

Adam

Here at SupplyHouse.com, we sell 8 AquaMotion pumps available in cast iron and stainless steel models, featuring the Green ECO-Cartridge design. The innovative design is incredibly efficient and will consume much less power in comparison with the market leader. AquaMotion … Continue reading

Posted in All Posts, Heating Supplies, New Products, Radiant Heat | Tagged

Sizing a Gas Regulator

Tom

Gas regulators control the flow of natural gas (NG) and liquid propane (LP) to appliances and equipment that use them as fuel. The pressure of incoming gas is often unstable and excessively high. Regulators ensure that sufficiently-low constant pressure is … Continue reading

Posted in All Posts, Heating Supplies, Radiant Heat | Tagged

Honeywell’s New Lyric Thermostat

Tom

A thermostat is nothing more than an on/off switch, activated automatically based on temperature settings, for a heating and/or cooling zone. Nevertheless, thermostats have evolved significantly over the years, including two relatively recent advances: programmability and internet connectivity. Honeywell’s new … Continue reading

Posted in All Posts, Heating Supplies, New Products, Radiant Heat | Tagged

Watts Onix Tubing

Tom

Onix Tubing from Watts Radiant provides several key advantages in radiant heat installations. Onix tubing is composed of two layers of cross-linked Durel EPDM around an “AlumaShield” aluminum oxygen barrier. The AlumaShield adds durability and reduces the risk of worksite … Continue reading

Posted in All Posts, Radiant Heat | Tagged

Cadet Heaters

Adam

We are pleased to announce that SupplyHouse.com now stocks a variety of heaters manufactured by Cadet, including Electric Baseboard, Garage Unit and Wall Heaters. Cadet is based in Vancouver, Washington, where every one of their electric baseboards, wall fans and … Continue reading

Posted in All Posts, Heating Supplies, New Products, Radiant Heat | Tagged

The New White Rodgers Sensi Wi-Fi Thermostat

Tom

Due to their basic functionality, traditional low-voltage mercury or mechanical thermostats require no outside source of power. Digital thermostats need energy in order to power their displays, but batteries can generally serve as the power source in the absence of … Continue reading

Posted in All Posts, Heating Supplies, Radiant Heat | Tagged

Axiom Pressure Pal System Feeders

Tom

Hot water heating systems generally operate on a closed loop (i.e. under pressure with the same fluid continually being reheated). This allows water in such systems to oxidize so that it cannot cause ferrous metal system components to corrode, but … Continue reading

Posted in All Posts, Radiant Heat | Tagged

Basic Baseboarders: A New Option for DIY Renovation

Tom

Baseboarders do-it-yourself baseboard heater covers changed the face of baseboard radiation. The original Premium design features covers filled with small perforations. This prevents small children from being able to touch hot elements, while allowing better airflow to and from a … Continue reading

Posted in All Posts, Heating Supplies, Radiant Heat | Tagged

Hydronic Kickspace Heaters

Tom

Kickspace heaters can serve as a space-saving solution in hot water heating systems. They take up a fraction of the space of baseboards or panel radiators, making them ideal for kitchens and bathrooms (or any other area in which baseboard … Continue reading

Posted in All Posts, Heating Supplies, Radiant Heat | Tagged ,

Logo

Join Our Mailing List - Sign up and receive special offers and coupons