SupplyHouse Blog Banner 2




How to Replace an Anode Rod

Mark

Anode Rods Steel rusts and corrodes when exposed to water for extended periods of time.  This, along with the acidity of water, leaves water heaters vulnerable to a more rapid corrosion process and bad smelling water.   By installing an anode rod you can delay this process and extend …

read more...

The One Tool Your Workshop Is Probably Missing

Guest

Even if you pride yourself on your well-equipped workshop with every state-of-the-art tool you need for construction projects or car repairs, there’s one piece of equipment that’s easy to overlook: the work light.  Because a dedicated work light doesn’t perform a specific task like…

read more...

AC SmartSeal Quick Shot

Emily

  AC SmartSeal Quick Shot is the newest technology from Cool Air Products.  This eco-friendly solution does not require system pump down.  The re-usable injection hose will last for multiple doses and is operator friendly.  This product is ideal for direct pinhole repairs and the prevention…

read more...

Pump It Up: Moving Water The Right Way

Nick B

Pumps, or circulators, are used in hydronic systems to move water through the system at a desired rate.  There are many important factors to consider when purchasing a pump, such as GPM, head range, voltage, and horsepower.   Two Quick Terms -GPM - An acronym for “gallons per minute,…

read more...

SupplyHouse Stress Test: Milwaukee M12 Airsnake

Nick B

Ever wanted to take your tools and really see what they can do?  Well recently I got to do just that with the Milwaukee M12 Airsnake.  This innovative tool uses compressed air to blast tough clogs out of pipes without having to take anything apart or run a traditional drain snake.  The Airsnake …

read more...

Panasonic FV-05-11VK1/FV-0511VK2 WhisperGreen Select Ventilation Fan

Emily

  Thanks to an impressive array of advanced options, the new WhisperGreen Select is the ideal all-purpose IAQ Solution.  Pick-A-Flow technology gives users the ability to select required air flow with just the flip of a switch.   WhisperGreen Select offers a unique set of four patented m…

read more...

3 Useful Sump Pump Maintenance Tips

Guest

The sump pump acts as a protective barrier between the foundation of your house and the water from the municipal sewage system.  The groundwater in the foundation is rerouted into a drain system (which is also located at the foundation), goes through a system of pipes, and finally reaches the s…

read more...

5 Signs Your Home Needs a Dehumidifier—and How to Select the Right One

Guest

Does your bread seem to go stale after a day or two?  Do your crackers and cookies lose their crispness soon after you open the box?  These aren’t just minor quirks that homeowners learn to live with, they are also signs that you may have a problem with high humidity in your home.   W…

read more...

Mini-Split Air Conditioning Systems

Emily

  A ductless mini-split air conditioning system includes an indoor evaporator unit connected to an outdoor condenser by a refrigerant line set.  These systems eliminate noise, wiring, and ductwork from the living space and present an alternative to window-mounted units and ducted central ai…

read more...

Sump Pumps: The Basics

Guest

In order to maintain the drainage systems of your residential, as well as commercial, buildings installation of sump pumps is very crucial.  They are made efficient to pump out the extra water accumulated in the basement of your buildings.  Sump pumps keep the basement dry and procure a smooth dr…

read more...

Bluefin PEX Fittings

Emily

  These lead-free barbed fittings work for PEX connections and may be used with the copper crimp ring system or the stainless steel clamp system.   Bluefin PEX fittings come in poly and brass material.  They come in different styles of fittings such as elbows, tees, couplings, ad…

read more...

Finding the Right Gas Valve for You!

Nick B

Gas valves are a critical component of many heating systems (If you are using a classic fireplace then you don't have to worry about them).  They are used to regulate the natural gas or liquid propane needed in the systems.  With their varied applications it's important to get the right one for yo…

read more...


SupplyHouse.com Logo