Home Plumbing Supplies

Category: Plumbing Supplies


How to Size a Tankless Water Heater

Tom

Tankless water heaters only heat water on demand, eliminating the standby losses associated with traditional tank-style water heaters. A Tankless water heater can provide hot water indefinitely – as long as demand does not exceed the heater’s flow capacity. There … Continue reading

Posted in All Posts, Plumbing Supplies |

PVC Fittings

Adam

At SupplyHouse.com we have added two new types of PVC Fittings manufactured by Spears. PVC Barbed Insert Fittings are engineered to provide positive grip and ease during installation. The barbed fittings are ideal for when a tightly gripped seal is … Continue reading

Posted in All Posts, New Products, Plumbing Supplies | Tagged

Liberty’s SumpJet: The Ultimate Failsafe Sump Pump

Tom

Sump pumps remove excess water, generally from basement-level sump pits. Water levels tend to be at their highest during storms and periods of heavy rainfall — the times during which power outages are most likely to occur. Almost any sump … Continue reading

Posted in All Posts, PEX Products, Plumbing Supplies | Tagged

Gruvlok Grooved Fittings

Adam

Gruvlok Grooved Fittings have recently been added to SupplyHouse.com. You can find Grooved Elbows, Couplings, Tees, Flanges, Butterfly Valves, and more here.  Gruvlok Grooved Fittings by Anvil International, sets the industry standard for durability, efficiency and flexibility, and these fittings … Continue reading

Posted in All Posts, New Products, Plumbing Supplies | Tagged

How to Connect PEX to Faucets and Toilets

Tom

PEX tubing can simplify potable water plumbing installations, while providing added freeze resistance, hot/cold color coding, and a reduced risk of pinhole leaks. PEX’s flexibility reduces the need for fitting connections, which can greatly cut down on installation time. There … Continue reading

Posted in All Posts, PEX Products, Plumbing Supplies | Tagged

Intelligent Washing Machine Flow from Watts

Tom

Watts IntelliFlow Washing Machine Water Shut-off Valves automatically regulate hot and cold flow to washing machines. The valves sense increases in electrical current draw when a washing machine operates. This signals the valves to open in order to allow water … Continue reading

Posted in All Posts, Plumbing Supplies | Tagged

Noritz Tankless Water Heaters

Adam

We’ve added a range of Noritz Tankless Water Heaters to the site.  Noritz has been an innovator of the water heating industry for over 60 years. Having introduced the first modern, electronically controlled tankless hot water heater in 1981 they … Continue reading

Posted in All Posts, New Products, Plumbing Supplies | Tagged

Lead-Free Plumbing Law

Tom

The Reduction of Lead in Drinking Water Act in the United States went into effect earlier this year, on January 4. The act imposes standards that were already enforced in several states. It defines “lead-free” as less than .25% lead … Continue reading

Posted in All Posts, Plumbing Supplies |

Frozen Pipes

Tom

Frozen pipes are a common occurrence during the cold season. To thaw a frozen pipe in your home, try turning on each faucet. If the water is flowing, run warm water through the pipes to help thaw the frozen spot. … Continue reading

Posted in All Posts, Plumbing Supplies |

Blue Monster Compression Seal Tape

Adam

Blue Monster Compression Seal Tape is perfect as a quick and cost-effective solution to help stop leakage under pressure without turning off the water source. This makes it the ideal solution equally for crisis and long-term applications, and has been … Continue reading

Posted in All Posts, New Products, Plumbing Supplies |

Venting Options for Boilers and Water Heaters

Mark

For gas and oil-powered boilers and water heaters, you need to select a venting system that will work in your home.  Chimney vented units vent exhaust naturally through a chimney.  Power vent and direct vent use fans to push exhaust … Continue reading

Posted in All Posts, Boilers, Plumbing Supplies | Tagged , ,

SALE: 5% Off All Grease Traps – Use Code: TRAPS (Exp. 5/29/13)

Kristine

SALE: 5% Off All Grease Traps – Use Code: TRAPS (Exp. 5/29/13) Grease traps are frequently found in restaurants, and it’s often required that a grease trap be installed in any location where food is being prepared. Small amounts of … Continue reading

Posted in All Posts, Plumbing Supplies, Sales |

Logo

Join Our Mailing List - Sign up and receive special offers and coupons