SupplyHouse Blog Banner 2



All Posts


ClearVue Condensate Pump

Tom

DiversiTech’s ClearVue condensate pump comes at a price similar to those of comparable condensate pumps, but it offers several unique features. Its clear body allows you to see inside the pump in order to monitor operation and diagnose problems. The pump can clean itself at the push of a button, w…

read more...

What a Dehumidifier Does…

Mark

Have you ever wondered what actually goes on inside of a dehumidifier?  Recently I did a video with Nicole from customer service about the dehumidifiers sold on our website. We created a pretty cool image that shows the basic functions inside a dehumidifier. When an excess amount of moisture is …

read more...

Hot Water in an Instant

Tom

Are you tired of waiting for hot water to reach your shower every day? Do you shake your head as wasted cold water flows down the drain? SupplyHouse may have the solution: a hot water recirculation pump. These pumps allow you to get instant hot water at the turn of the faucet and can result in big s…

read more...

KS1 Kickstart Compressor

Adam

The KS1 Kickstart Compressor from Rectorseal is the only two-wire, pre-assembled starting component Hard Start Kit on the market that uses a high-quality mechanical potential relay in a unique design. There is absolutely no use of circuit boards, timers or PTCR devices. The KS1 is used for single ph…

read more...

Direct Burial of PEX Tubing

Tom

PEX tubing is approved for direct burial outdoors, a practice most often necessary when running a water supply line to a house. PEX, since it can expand, resists freezing more effectively than rigid pipe, but PEX can still burst if water freezes in a line. As a result, it’s a must to bury the tubi…

read more...

How to Become a Better Troubleshooter

Kristine

Avoid "Auto" Conclusions Don't try to solve the problem while you're still in your truck. Some technicians make up their minds before looking around, and then they set out to prove that they're right - even if they're not! Comprehend the components If you don't understand how the parts work…

read more...

Bath Fans Do More Than Clear Odors

Kristine

Since the bathroom is the most humid room in any house, a ventilation fan is the best defense against moisture-related problems—namely, mold and mildew. Humidity is not only uncomfortable, it is damaging to your home, particularly indoors where it can lead to peeling paint, warped wooden doors …

read more...

Sioux Chief Copper Manifolds

Adam

Brand new to SupplyHouse.com are a range of Sioux Chief Copper Manifolds with Crimp or Compression Balancing Valves. Both of these styles are available with 2, 3, and 4 loops, and have brazed branches which are perfect for hydronic applications. These economic PEX manifolds will be useful for anyone…

read more...

When to use Supply End Caps on Viega Manablocs

Tom

Viega Manablocs have three “supply port” connections: one hot and one cold at the top, and one cold at the bottom. Since the Manabloc is partitioned internally into hot and cold sections, hot water from the water heater must enter through the hot port. Incoming cold water can enter through eithe…

read more...

UV Air Purifier

Adam

New from Honeywell, the Ultraviolet Air Purifier with AirBRIGHT Odor Absorption uses ultraviolet light to help keep your air clean.  The system can eliminate up to 99 percent of mold spores on the air conditioning coil, which will help to maintain system efficiency and airflow.  Similar to what is…

read more...

PexTV Episode 9

Mark

Hey, here's episode 9 of "PexTV" but its also kind of like episode 467...This weeks episode gets a visit from a special guest. You won't want to miss who it is... In this episode, you'll see... Featured Product: Honeywell RedLINK Internet Gateway Tip of the Week: Energy Star qualified products …

read more...

Connecting PEX to PB

Tom

Polybutylene (PB) piping was commonly used for domestic water piping in the United States during parts of the 1970s and 1980s. Polybutylene can be identified by its gray color. Lawsuits related to fitting assembly failures caused the production of PB to stop, but the plastic tubing is still present …

read more...


SupplyHouse.com Logo