Research by Uponor further proves our inclination that the Plumbing and Heating industries are where it's at. 90 percent of installers are enthusiastic about the year ahead. Here's why (according to a survey of Uponor's supplier network): 45 percent of survey respondents think the biggest fac…

New Residential Water Heating Guidelines In 2015
A new standard for residential water heaters is set to take effect on April 16, 2015. This new standard is expected to conserve 3.3 quads of energy and result in $63 billion in energy savings between 2015 and 2044. What Does This Mean For You? Affects water heaters manufactured on or…

The SMAN Digital Manifold makes HVACR Jobs Easier
[caption id="attachment_213126" align="alignright" width="443"] Source: Fieldpiece.com[/caption] The new SMAN Digital Manifolds range from Fieldpiece is manufactured to show you everything you need to check, evaluate and charge sys…

39 SupplyHouse.com Employees Accept the Ice Bucket Challenge
When Eileen from the customer service department nominated the team to take the ALS Ice Bucket Challenge, we were up for the challenge. 39 of us lined up with buckets of ice water behind us, and Justin and Al went down the line dumping water. Nobody left dry, and everybody left in a bett…

Access Doors by Acudor
Acudor manufacture ducts and access doors for walls, ceilings, or floors. Access doors can be installed in drywall, plaster, masonry, tile or any flush surface. Here at SupplyHouse.com, we offer a wide variety of access doors in many different sizes for specific uses such as Fire Rated, which ar…

AquaMotion
Here at SupplyHouse.com, we sell 8 AquaMotion pumps available in cast iron and stainless steel models, featuring the Green ECO-Cartridge design. The innovative design is incredibly efficient and will consume much less power in comparison with the market leader. AquaMotion brings decades of experienc…

PEX-A, PEX-B, & PEX-C
All PEX tubing carries one of three grades: PEX-A, PEX-B, or PEX-C. PEX stands for polyethylene (PE) cross-linked (X), and the grades are based on the various methods that manufacturers use to cross-link polyethylene molecules. PEX-A represents the highest grade. Cross-linking occurs while the po…

IW25-1 In-Wall Dehumidifiers
New to SupplyHouse.com is the award winning IW25-1 In-Wall Dehumidifier manufactured by Innovative Dehumidifiers. It’s designed with the user in mind with its lock out control system, making it ideal for landlords to keep control away from tenants and other occupants, which in turn will help to av…

Sizing a Gas Regulator
Gas regulators control the flow of natural gas (NG) and liquid propane (LP) to appliances and equipment that use them as fuel. The pressure of incoming gas is often unstable and excessively high. Regulators ensure that sufficiently-low constant pressure is maintained and sent to appliances. Proper s…

How to Size a Tankless Water Heater
Tankless water heaters only heat water on demand, eliminating the standby losses associated with traditional tank-style water heaters. A Tankless water heater can provide hot water indefinitely – as long as demand does not exceed the heater’s flow capacity. There is a limit to the amount of hot …

PVC Fittings
At SupplyHouse.com we have added two new types of PVC Fittings manufactured by Spears. PVC Barbed Insert Fittings are engineered to provide positive grip and ease during installation. The barbed fittings are ideal for when a tightly gripped seal is needed, and means that adhesive isn’t necessary. …
Honeywell’s New Lyric Thermostat
A thermostat is nothing more than an on/off switch, activated automatically based on temperature settings, for a heating and/or cooling zone. Nevertheless, thermostats have evolved significantly over the years, including two relatively recent advances: programmability and internet connectivity. Hone…