SupplyHouse Blog Banner 2




Watch the Tailpipe

Kristine

Start your car on a cold morning and walk around to the tailpipe. See that water dripping? That's the way a high-efficiency, condensing boiler works. It removes so much of the heat from the flue gases that the gases turn to liquid and drip out. That liquid is acidic so we use neutralizers to deal wi…

read more...

Tank vs. Tankless Water Heaters

Tom

Tankless water heaters present an alternative to conventional tank water heaters. Tankless units generally take up less space, can be mounted on a wall, and only heat water on demand. Although tank-style water heaters expend extra energy to keep the contents of their storage tanks warm at all times,…

read more...

Spruce Up Old Baseboard Heaters With Stylish DIY Replacement Covers

Kristine

Looking for a way to retrofit your old baseboard heaters? Do-it-yourself with the versatile and easy to install Baseboarders replacement covers. Baseboard heaters have been an extremely popular choice for many homes since the mid-1950s—and unfortunately, many of these units are showing their ag…

read more...

Eliminate Drafts this Winter

Tom

During heating season, homes and buildings inevitably lose heat through ceilings, floors, windows, and doors. One major source of heat-loss is often overlooked: ducts. Unless a structure has a forced-air heating system, ducts used for central air conditioning are inactive during the winter. Ducts us…

read more...

Grocery Store Radiant

Kristine

A great place to understand radiant heating (or to explain it to your customer) is your local grocery store. Stop first in the gadget aisle and pick up a thermometer. It will probably read 70 degrees, a nice comfortable temperature. Walk up and down the aisles and keep your eye on the temperatur…

read more...

Expansion Tank Mounting Positions

Tom

Expansion tanks can be installed in any direction. Whether oriented uprightly, horizontally, or even upside down, the expansion tank will function properly without any adverse effects. When putting an expansion in an abnormal position (specifically sideways or horizontally), make sure to support the…

read more...

Rotten Egg Smell in Hot Water

Tom

Anode rods protect the lining of water heater tanks from corrosion. In rare instances, anode rods can contribute to foul-smelling hot water that has the odor of rotten eggs. This may occur when there are high sulfur and low oxygen concentrations in supply water. The anode rod promotes the generation…

read more...

Why closely spaced tees?

Kristine

Primary-secondary piping systems call for the tees that go off to the secondary circuit to be close together, ideally not more than six inches apart. Think like water and you'll see why this is. Flow down the primary main and imagine you're entering that first tee. You have two choices: You can stay…

read more...

PexTV Episode 11

Mark

Hey everyone, this is PexTV episode 11. It's all about some tips and tricks that we can help you with as you think about winterizing your home. In this episode you will see... Product Spotlight: Frost Proof Sill Cock Tip of The Week: Get your heating system serviced Customer Review: Easy Hea…

read more...

The Top 10 Things to Check if that Steam System is Hammering

Kristine

1. The near-boiler piping doesn't meet the manufacturer's specs 2. The steam quality is bad (wet steam causes hammering) 3. The boiler is oversized or overtired. 4. The insulation is missing from the piping. 5. The Hartford Loop connection is too close to the waterline, or has a nipple that's…

read more...

The Pros and Cons of PEX-AL-PEX

Tom

PEX-Aluminum-PEX (PEX-AL-PEX) tubing contains a layer of aluminum embedded between two layers of PEX. SupplyHouse.com carries standard PEX-AL-PEX made by Rifeng and Uponor. The aluminum serves as an oxygen barrier and makes the tubing more rigid. See the chart below for some of the the advantages an…

read more...

Fix Kinks in PEX

Tom

It’s possible to kink PEX tubing if you bend it too tightly.  When using PEX-B or PEX-C grade pipe you will normally want to cut the affected piece of tubing out of the line and replace it with a coupling, depending on the severity of the kink. With PEX-A, heat can be used to fix the kink (watch …

read more...


SupplyHouse.com Logo