The Honeywell T4 Pro Programmable Thermostat has several programmable and non-programmable options that can be fine tuned to your schedule. But how do you get it to do what you need? Read the instructions below or watch the video at the end of this post to learn how. Or do both if you really want to be sure.
1) Power up the Unit
Once on, press the Select button to awaken the screen.
2) Setting the Year
Press the Plus or Minus buttons to choose the year you want and press the Select button to finalize. (I suggest choosing the current year)
3) Setting the Month
Once the year is selected it will automatically ask you for the month. Again, use the Plus and Minus buttons to navigate the months and hit Select to finalize.
4) Setting the Day
Just like with the month, you will be automatically asked to select the day, use the Plus and Minus buttons to navigate, and hit Select when the right one is on the screen.
5) Choosing Clock Format
Next, you will be asked to choose between a 12 and 24 hour clock. Use the Plus, Minus, and Select buttons to make you decision.
6) Setting the Time
As you have been doing, use the Plus, Minus, and Select buttons to choose the time, but here you can press and hold either Plus or Minus to cycle through the numbers faster. (While it might seem like a fun prank to set the time wrong and confuse people, it is important to set the time correctly for the rest of the programming to work properly.)
After selecting your time your base settings will be saved!
1) Get to the Home Screen
This is an easy one, press the Home button and you’re there. This will be your hub to navigate the rest of your options.
2) Select your System Mode
Press the Mode button to cycle through the Heat, Cool, and Off modes until the one you want is displayed.
3) Advanced Menu
To access the Advanced Menu press the Menu button from the Home screen. From here you will be able to adjust the thermostat settings like Program Schedule and the Base Settings. Navigate them with the Plus and Minus buttons.
4) Turning Programming On or Off
Through the Advance Menu cycle through until “PROG” is displayed on the screen then press Select. From here you will be presented with On or Off options which you can navigate and choose via the Plus, Minus, and Select buttons.
5) Program Schedules
From the end of step 4 select On. Once there you will be able to navigate and select the desired program schedule with the Plus, Minus, and Select buttons. For each schedule you will be able to program up to four time periods each day, with different settings for weekdays and weekends. The times periods are;
- Wake: When you wake up.
- Away: When you leave the house for the day.
- Home: When you return home for the evening.
- Sleep: When you go to bed at night.
6) Setting and Editing Program Schedules
After selecting the time period to edit the system will have you set the Heating Schedule. Using the Plus, Minus, and Select buttons choose the exact Time you want. After that you will be prompted to select the Temperature you want. After that you will move onto the Cooling schedule for that time period. Follow the same steps as for Heating to complete this Schedule.
7) Turning Off Certain Time Periods
If you do not want to have one or more of the Time Periods (Wake, Away, Home, Sleep) active navigate the menu and select the one you do not want. From here use the Plus or Minus buttons to switch from On to Off and then press Select.
8) Finalize Changes
Once everything is set just how you want, press the Home button and return to the home screen. There will be a screen that reads “Save” before the home screen appears. Don’t worry, you can always return to your settings and make any adjustments you want.
9) Overriding the Programmed Schedule
If you need to make a temporary or permanent change to the currently set temperature, press the Plus button on the Home screen. Then the small temperature will begin flashing. Adjust this to the temperature you want it to be and press the the Hold button to temporarily or permanently change the temperature.
10) Fan Options
There are two options here. Fan Auto which only runs when the system is on and Fan On which runs continuously. Press the Fan button on the Home screen to choose between the two.
Now you are all programmed! When you need a T4 Pro or any other HVAC, heating, or plumbing products SupplyHouse.com will have what you need. Stop by today and see our entire selection.
I have a T4 pro I can’t change the program only unlock showing in center of button why?
Hi Toan,
Check these manuals for more details on unlocking the unit.
https://forwardthinking.honeywell.com/assets/tseries/resources/install/T4%20Pro%20User%20Guide%20-%2033-00188EFS.pdf
.
https://forwardthinking.honeywell.com/assets/tseries/resources/install/T4%20Pro%20Install%20Instructions%20-%2033-00187EFS.pdf
I’ve got this manual and I can find absolutely nothing about “unlocking” the unit, which I accidentally did. The installer went thru the programming so fast and was in such a hurry, I could hardly keep-up so now I’ve got one unit locked and cannot determine how to unlock it. Please identify the section that deals with this.
Hi Debbie,
.
Give page 5 of this manual a look for help unlocking.
https://forwardthinking.honeywell.com/assets/tseries/resources/install/T4%20Pro%20User%20Guide%20-%2033-00188EFS.pdf
Why does my Honeywell not turn on for wake when I have turned it off to go to bed the night before. Does it need to be on all the time to follow the schedule? Also the sleep function, does that turn the heater off through the night?
Hi Elly,
So once you have programmed your thermostat you can just leave it and it will maintain the heat/cool levels you set it to. Go through the programming process, setting the times you want your home be certain temperatures, and then the thermostat will do the rest for you. The wake and sleep settings will be handled through that process, setting the temperature for the morning and night respectively.
My hold button disappeared. How do I get it back?
Hi Kong,
You may be locked out of the programming. Check out the link below for more info about working with that.
https://forwardthinking.honeywell.com/assets/tseries/resources/install/T4%20Pro%20User%20Guide%20-%2033-00188EFS.pdf
.
If that isn’t working then you should reach out to Honeywell directly for specific troubleshooting. I included a link below here to get you connected to them.
https://www.honeywell.com/contact-us
Good day, I had a T4 Pro installed. The technician advised me not to put batteries in the thermostat, as it would cause corrosion. Can you please confirm or advise if this is true. And if I choose not to utilize batteries, does this create any issues for the function of the thermostat, other than as a backup in the event of a power failure.
Hi Trish,
.
While there is a small risk of corrosion with any battery, that should not stop you from using one. The thermostat has a low battery warning that will alert you that the battery needs changing.
.
In regards to the backup question, the battery is the backup in case of power failure. So if your power goes out and you do not have a battery you will lose all of your programming and functionality until power returns and you reprogram it.
my T4 is programmed to cool to a temperature of 72 for the “home” time period, but the thermostat goes to 68 on its own. i check the program, it’s correct, its set at the 72, i check the time and date, its correct, I save everything, go back to the home screen, thermostat says its going to cool to 68 still. why????
Hey Peter,
.
Your best bet to getting this specific issue solved quickly and accurately is to reach out Honeywell directly following this link: https://www.honeywell.com/contact-us
.
Another option would be to bring in a service tech to take a look at it, but that would cost money so I suggest reaching out to Honeywell first.
My fan does not ever turn off. I have Program set to “off” as well as the heat/cool system set to “off” but the fan is continuously running. How do I fix this issue?
Hi Christina,
.
Have you looked into specifically your fan settings? It can be set either “on” or “auto” so if it is “on” then that explains it. If it is on “auto” then there are other issues.
.
If this doesn’t solve your issue I suggest reaching out to Honeywell directly by following this link: https://www.honeywell.com/contact-us
Thanks for the quick reply, Nick. The fan is set to “auto” but still runs when system is off.
Yeah, I’m not sure at this point. I would recommend reaching out to Honeywell directly with the link in my comment above. They have a phone number to call or a form to fill out depending on what you want to do.
hi i have a t4pro and program doesnt show up in the advanced menu
Hey Scott,
.
You may be locked out of the programming. Give the link below a look for more info about that.
https://forwardthinking.honeywell.com/assets/tseries/resources/install/T4%20Pro%20User%20Guide%20-%2033-00188EFS.pdf
.
If that isn’t what you need then I would recommend reaching out to Honeywell directly with the link I put below here.
https://www.honeywell.com/contact-us
I was able to set the date, time, function. But when I press menu, I do not see PROG, thus I can’t set a program. Any tips?
Hi David,
.
What comes to mind first is that you may be locked out of PROG. Give the link below a look for more info about fixing that.
https://forwardthinking.honeywell.com/assets/tseries/resources/install/T4%20Pro%20Install%20Instructions%20-%2033-00187EFS.pdf
.
If that isn’t what you need to fix what’s happening I would recommend reaching out to Honeywell directly for more specific help. Check out this link to do that.
https://www.honeywell.com/contact-us
Hi There is a warning triangle on top of Fan Auto. What does it mean?
Thanks
Amanda
Hi Amanda,
.
I am not sure what that warning is referencing to in your situation. For specific help I would suggest reaching out to Honeywell directly, they’ll be able to help you better. I attached a link that will get you where you need to go.
https://www.honeywell.com/contact-us
Hi, I moved to a new home and am trying to reset the schedule. I can’t figure out how to reset whether it is on heat or cool. So for example, it’s summer time, and if I set one of the time periods to 77 degrees, it still shows heat. Other time periods show cool when set at the same temperature. Thanks in advance!
Hey,
.
So there are a couple of things you can try.
1) Change the Mode: From the home screen press the Mode button and cycle through Heat, Cool, and Off modes until you have the one that makes sense for you.
2) Change the Program settings: From the home screen press the Menu button and navigate until “PROG” is displayed. Select that and change the programming settings until it’s all set how you want.
.
Check out our video I am linking for a visual on how to do that -> https://youtu.be/ZkGfslseYWA?t=1m10s
.
If none of that helps I would suggest reaching out to Honeywell directly for specific guidance. You can get to them with the link here -> https://www.honeywell.com/contact-us
Can I put a lock it so nobody can turn the system off
Hi Jessica,
.
The T4 does have a lock feature. From the Home screen select Menu then go all the way to the end of that list. You will see “LOCK” and that’s what you’ll want to select. Once selected you will want to navigate to and select “ON” and you should be all set!
.
Find more information about the lock and how to change the code here -> https://forwardthinking.honeywell.com/assets/tseries/resources/install/T4%20Pro%20User%20Guide%20-%2033-00188EFS.pdf
How do I programe the thermostat to say 70 degrees when the room temp is really 68 degrees?
Hey Brady,
.
I’m not sure if this unit can do that. Your best bet is to reach out to Honeywell directly. You can reach them here -> https://www.honeywell.com/contact-us
My oil company recently installed a T4 Pro thermostat. It is my understanding that this unit is a 5-2 or 5 1-1. When I attemp to program it, it forces me to program all 7 day individually, instead of programing Monday thru Friday as a block. Is this a defective unit, or am I doing something incorrectly. I have read the owner manual multiple times, plus watch multiple YouTube vids, but can’t figure what I’m doing wrong.
Hi Robert,
.
You should be seeing Monday through Friday in a block for programming. From the Home screen go to Menu, then select PROG, and then ON. From there at the top of the screen you should see “Mon Tue Wed Thu Fri” flashing to be edited.
.
I am not sure why it is forcing you to program each day individually. For help on this specific issue I recommend reaching out to Honeywell directly. Use the link below to do so.
https://www.honeywell.com/contact-us
Nick, thanks for the reply. I followed the steps you described, the only thing that is flashing is Monday, I will get in touch with Honeywell, hopefully they can walk me thru this issue.
No problem, they’ll be able to get to the bottom of this.
Saw a tech from oil company today. Apparently the tech who installed my thermostat was new, unfamiliar with this unit and did something incorrectly when setting it up. The techie today used what he decried as a BACK DOOR FIX to correct my issue. Everything is fine now.
Great! I’m glad you got it working.
Thermostat will not let me go below 70 in cool mode. How can i override this? I’ve seen other videos about other models featuring a range stop function, but I am unable to figure this out for the T4 pro.
Hi Klayton,
That can be changed by following the instructions on page 6 and 7 here! https://forwardthinking.honeywellhome.com/assets/tseries/resources/install/T4%20Pro%20Install%20Instructions%20-%2033-00187EFS.pdf
Hope this helps!
Hello,
My unit will not display a model button or a fan button. The only options that ever displays is “unlock” , once you press unlock, it takes you to a screen where you can plus or minus up to four numbers, on this screen the only “button” option it displays is “back”. The tech did not provide any instructions on the process of generating the “mode” or “fan” button to display. I am unable to enter into advanced mode or change any other settings. The temperature remains at a constant 71.
Hello! Thank you for your question. You may be able to resolve this by unlocking your thermostat. Here are instructions on how to do so.
What would cause the thermostat not to give me heat as an option? While cycling through the settings I only have cool/off as options.
Hello Eddie. Thank you for your question.
Is it possible that you have the thermostat set up as having no heating system? ISU #200 may be set to cool only. Please refer to page 6 here for further info – https://customer.resideo.com/resources/Techlit/TechLitDocuments/33-00000s/33-00187EFS.pdf
I have the fan set to on but it won’t come on… any ideas?
Hello Linda.
It may possible that there is something wrong with the fan itself. Is this something you already looked into?
How do I change the lock code? I didn’t find the instructions in the install resources linked at https://forwardthinking.honeywellhome.com/assets/tseries/resources/install/T4%20Pro%20User%20Guide%20-%2033-00188EFS.pdf
Thanks
Ryan
Hello Ryan.
Unfortunately it is not possible to change the lock code. We’re sorry for the inconvenience!
Hi,
Is there any way to have the fan completely off the entire time? Do I have to put it at a certain temp for it not to turn on..? Moved to new house but they forgot to leave manual & no verbal instructions on how to use it.
Thanks in advance,
Joyce
Joyce
There are two fan modes for this thermostat. In “On” mode, the fan operates continuously. In “Auto,” the fan only runs when the heating or cooling system is running. The fan will only cease running if the heating or cooling systems are not running.
I have a Honeywell t4 and when the temp.in my house is at 64 AND I WHAT IT TO BE WARMER WHY IS IT THAT WHEN I SET IT AT A SET TEMP. ITGOES PASS THAT AND GET`S SO HOT THAT I HAVE TO TURN ON THE AC TO COOL.
We’d advise that you take a look at your program settings. It’s possible that the thermostat has programmed schedules causing the setpoint to go beyond your desired temperatures. It’s also possible that the thermostat is positioned in an area of the house much cooler than the spaces you generally occupy, which could cause it to run for a length of time that causes other areas of the house to get uncomfortably warm
Good afternoon.
I have two T4 thermostats in my home and neither have an auto selection for the temperature. I have heat, cool, e-heat and off.
So my question is do I need to have the auto option when the thermostat is following a schedule? If so how do I get the “auto” option?
Hi Jason,
As long as your particular T4 model has an Auto option, you should be able to activate it in the Installer Setup Settings. On T4 Pro models, this can be done by changing Advanced Setup Option 300 from “0” to “1” by following the instructions on pages 6 & 7 of the manual linked below. “Auto” simply allows the thermostat to alternate between heating and cooling modes automatically. While this can be a helpful feature (especially in certain climates and certain parts of the year), it’s not something critical to system operation.
https://forwardthinking.honeywellhome.com/assets/tseries/resources/install/T4%20Pro%20Install%20Instructions%20-%2033-00187EFS.pdf
Is there a way where I can turn off the programming, and just use this as a regular thermostat? When this was installed we were able to keep it going without a schedule, but a couple nights this week its defaulted to the default schedule.
Hi Nick,
Yes, you can turn off the programming feature. To do this, please use the Advanced Menu setting. To access this, press the Menu button from the Home screen. From here you will be able to adjust the thermostat settings like Program schedule and Base Settings. Navigate these with the Plus and Minus Buttons.To turn the Programming On or Off, go through the Advanced Menu cycle until “PROG” is displayed on the screen then press Select. From here you will be presented with On or Off options which you can navigate and choose via the Plus, Minus, and Select buttons.
Thank you!
Greg
Hello I just had a T4 Pro installed with the cool and heat programmed I just only see a auto for the fan does the system changes automatically I have it on cool now but would like for it to turn to heat if the temperature drops when I’m not home
Hi Vic,
You should be able to enable the ability to select automatic system changeover by changing Advanced Setup Option #300 from 0 (Manual) to 1 (Automatic) by following the instructions on page 6 and 7 of the manual linked below:
https://forwardthinking.honeywellhome.com/assets/tseries/resources/install/T4%20Pro%20Install%20Instructions%20-%2033-00187EFS.pdf
I had my brand new thermostat moved from one side of the house to the other & since the moved I keep having a Battery Low reading on the screen. If I unplug it & put it back in it goes off for 45 minutes then comes back on. Our Tech has no idea – brand new & brand new batteries tested fully charged. How can I turn the Low Batter wording off my screen?
Hi Stan,
It would seem to us that your thermostat is defective. We’d advise trying to replace it under the warranty, which we can assist with if you purchased it from SupplyHouse.com
i use it for commercial.if i want to set up: “away”—for the night time. “home”—for the daytime.is it the same setting?
Hi Michael,
The thermostat cannot internally have the “Home” and “Away” wording reversed unfortunately. However, setting the “Home” at a lower/higher temperature set point than the “Away” will not cause an functionality issues.
I’m trying to increase the temperature in heat mode and does not go beyond 70 degrees.
Hi Mario,
It is likely that your landlord has put in a range limitation, which is why it is not going above 70°. Page 5 shows how to get into the installer set up and page 7 #431 shows how you can adjust the maximum heat set point.
https://forwardthinking.honeywellhome.com/assets/tseries/resources/install/T4%20Pro%20Install%20Instructions%20-%2033-00187EFS.pdf
Hello,
Just curious is anyone has reported an issue where the schedule cycles on exactly one-hour before the programmed time. Example–my unit is programmed to increase the heat setting from 62 to 66 at 5:00PM. Clock is set to the correct time. Unit comes on at 4:00PM. I have reset the clock a couple of times. I have reset my schedule a couple of times. Have not seen any “daylight saving time” setting. It’s odd. Not something that cannot be worked around.
Thanks.
Tim
Hi Tim,
We have not heard of any reports of this issue. Since you have covered the bases regarding potential issues an incorrect time setting or daylight saving time, we would be inclined to believe that there could be some kind of glitch or defect with your thermostat. One thing to confirm on daylight saving time would be to check Advanced Setup Option #1415 (see pages 6 and 9 of the manual linked here — https://forwardthinking.honeywellhome.com/assets/tseries/resources/install/T4%20Pro%20Install%20Instructions%20-%2033-00187EFS.pdf)
Thanks for taking the time to respond. Much appreciated.
My pleasure. Please do let us know if this solves your issue, and if not, we will working on looking for an alternative solution! Have a nice day.
I am also having this problem. I have it set for sleep at 10:00 pm (16 degrees) and wake at 6:30 am (19 degrees). At some point in the night it is increasing itself to 19 degrees. Very frustrating!
Hi Lisa,
I’m sorry that you are having this problem as well. Have you tried the steps that we recommended for Tim to see if that solves the issue?
Thank you,